<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config ToolsのトピックRe: Can build project, but cannot update pin changes</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937571#M735</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had 2 warnings about an Include path not found.&amp;nbsp; They were part of the Assembler settings under Project Properties -&amp;gt; C/C++ Build -&amp;gt; Settings -&amp;gt;MCU Assembler -&amp;gt; General.&amp;nbsp; They weren't needed so I removed them from the project, which removed the two warnings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88247i588F8C9700FF64C6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a clean build of the project and "Update Project" is still grayed out with the same error message in the Pins configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Sep 2019 13:40:15 GMT</pubDate>
    <dc:creator>curtis_hendrix</dc:creator>
    <dc:date>2019-09-18T13:40:15Z</dc:date>
    <item>
      <title>Can build project, but cannot update pin changes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937569#M733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on code that was created by another team.&amp;nbsp; I can successfully build the project, but I cannot update any changes made with the Pin Config utility.&amp;nbsp; The "Update Project" button is grayed out with the message "Action is not available, because no toolchain project was detected in the configuration directory".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How do I fix this?&lt;BR /&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87679i70B16ACF735BA2E7/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Sep 2019 15:04:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937569#M733</guid>
      <dc:creator>curtis_hendrix</dc:creator>
      <dc:date>2019-09-17T15:04:51Z</dc:date>
    </item>
    <item>
      <title>Re: Can build project, but cannot update pin changes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937570#M734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Curtis,&lt;/P&gt;&lt;P&gt;switch to `Develop` perspective and check the project - look into Problems view and Error Log view to find&amp;nbsp;what issues are reported for the project. The typical root-cause is that you do not have SDK package assigned to the project, so SDK project cannot be loaded.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 12:16:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937570#M734</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2019-09-18T12:16:48Z</dc:date>
    </item>
    <item>
      <title>Re: Can build project, but cannot update pin changes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937571#M735</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I had 2 warnings about an Include path not found.&amp;nbsp; They were part of the Assembler settings under Project Properties -&amp;gt; C/C++ Build -&amp;gt; Settings -&amp;gt;MCU Assembler -&amp;gt; General.&amp;nbsp; They weren't needed so I removed them from the project, which removed the two warnings.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88247i588F8C9700FF64C6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I did a clean build of the project and "Update Project" is still grayed out with the same error message in the Pins configuration.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 13:40:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937571#M735</guid>
      <dc:creator>curtis_hendrix</dc:creator>
      <dc:date>2019-09-18T13:40:15Z</dc:date>
    </item>
    <item>
      <title>Re: Can build project, but cannot update pin changes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937572#M736</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;And Error Log?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 13:46:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937572#M736</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2019-09-18T13:46:50Z</dc:date>
    </item>
    <item>
      <title>Re: Can build project, but cannot update pin changes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937573#M737</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 14:25:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937573#M737</guid>
      <dc:creator>curtis_hendrix</dc:creator>
      <dc:date>2019-09-18T14:25:46Z</dc:date>
    </item>
    <item>
      <title>Re: Can build project, but cannot update pin changes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937574#M738</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Curtis,&lt;/P&gt;&lt;P&gt;I can see the following exception in your log:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;java.lang.Exception: org.eclipse.core.runtime.CoreException: The project 'Project_Name' has no nature com.nxp.mcuxpresso.core.datamodels.sdkNature&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;This means the SDK project nature was not initialized properly and this is the root cause why you cannot use SDK specific features in Pins/Clocks/Peripherals. Please follow your project with MCU IDE team, to get help on this problem: &lt;A _jive_internal="true" href="https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide"&gt;https://community.nxp.com/community/mcuxpresso/mcuxpresso-ide&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 14:39:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Can-build-project-but-cannot-update-pin-changes/m-p/937574#M738</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2019-09-18T14:39:45Z</dc:date>
    </item>
  </channel>
</rss>