<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config Tools中的主题 Re: Unable to create new configuration for processor</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790709#M461</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;it is sufficient to go to C:\ProgramData\ and there&lt;/P&gt;&lt;P&gt;a) delete the whole NXP folder&amp;nbsp; (which also might have incorrect security settings - not only mcu_data_v4.1 folder) -&lt;STRONG&gt; you have to re-start the application again&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;b) or click right mouse on the folder, select Properties, dialog will appear. Go to "Security" tab and make sure the group "Users" has write permission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you tried the a) , is that folder "mcu_data_v4.1"&lt;/P&gt;&lt;P&gt;1. re-created yes/no ?&lt;/P&gt;&lt;P&gt;2. writable by the tool yes/no ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: running the tool as an Administrator is a last resort which might help, but from that time it is needed to run it everytime as an Admin, otherwise the files/folders will not be writable when running as regular user.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Jul 2018 15:35:13 GMT</pubDate>
    <dc:creator>liborukropec</dc:creator>
    <dc:date>2018-07-30T15:35:13Z</dc:date>
    <item>
      <title>Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790706#M458</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am having great difficulties creating a new configuration for my uC.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I go to new - &amp;gt; Create new configuration for processor, board or kit, originally, I was selecting the processor config I need, which is the&amp;nbsp;MK22FN1M0Axxx12.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However; upon clicking Finish, I get this error message:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"Disk operation error. Check disk space and write permissions for the data folder:&lt;/P&gt;&lt;P&gt;C:\ProgramData\Application Data\NXP\mcu_data_v4.1"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've checked this folder's permissions, and I have plenty of disk space (101GB free). Also, having admin rights to the computer / use Run As Administrator option, same error message.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am running Windows 10 Pro 64 bit (potentially the root cause)&lt;/P&gt;&lt;P&gt;and I am running MCUXpresso Config Tools 4.1&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Jul 2018 19:36:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790706#M458</guid>
      <dc:creator>jturner</dc:creator>
      <dc:date>2018-07-27T19:36:48Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790707#M459</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jahmai Turner,&lt;/P&gt;&lt;P&gt;sometimes there is a problem with access rights to the data folder. Please remove folder from your disk and restart the tool. The tool will re-create folder and the problem should be fixed.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 07:02:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790707#M459</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2018-07-30T07:02:17Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790708#M460</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Marek for the reply..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, even after removing the NXP\mcu_data_v4.1 folder, the application still presents the same error message. I was not able to go directly to C:\ProgramData\Application Data\&amp;nbsp; (in order to remove the NXP folder)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, I tried removing the tool via add/remove programs, and reinstalling the application. Same problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 13:35:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790708#M460</guid>
      <dc:creator>jturner</dc:creator>
      <dc:date>2018-07-30T13:35:52Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790709#M461</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;it is sufficient to go to C:\ProgramData\ and there&lt;/P&gt;&lt;P&gt;a) delete the whole NXP folder&amp;nbsp; (which also might have incorrect security settings - not only mcu_data_v4.1 folder) -&lt;STRONG&gt; you have to re-start the application again&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;b) or click right mouse on the folder, select Properties, dialog will appear. Go to "Security" tab and make sure the group "Users" has write permission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you tried the a) , is that folder "mcu_data_v4.1"&lt;/P&gt;&lt;P&gt;1. re-created yes/no ?&lt;/P&gt;&lt;P&gt;2. writable by the tool yes/no ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note: running the tool as an Administrator is a last resort which might help, but from that time it is needed to run it everytime as an Admin, otherwise the files/folders will not be writable when running as regular user.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 15:35:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790709#M461</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2018-07-30T15:35:13Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790710#M462</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Libor,&lt;/P&gt;&lt;P&gt;I've removed /ProgramData/NXP from the system, and rebooted my machine after removing the folder&lt;/P&gt;&lt;P&gt;Still, haven't had any luck getting it to work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am an administrator on my local machine. I (should) have read/write rights to the folder inherently. However&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried the following:&lt;/P&gt;&lt;P&gt;1) Deleting the /ProgramData/NXP folder&lt;/P&gt;&lt;P&gt;2) Running MCUXpresso Config Tools v4.1 as an administrator (Right Click Shortcut -&amp;gt; run as administrator).&lt;/P&gt;&lt;P&gt;Similarly, I get the same error as the original post.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll try to have my co-worker install the tool on his PC to see if he can get the software to function properly.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jul 2018 17:42:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790710#M462</guid>
      <dc:creator>jturner</dc:creator>
      <dc:date>2018-07-30T17:42:43Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790711#M463</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jahmai Turner,&lt;/P&gt;&lt;P&gt;if you delete the folder and restart the tool, is the folder re-created?&lt;/P&gt;&lt;P&gt;Can you try to create the folder manually - using another application - e.g. Windows Explorer?&lt;/P&gt;&lt;P&gt;Config Tools uses standard access to the file on the disk.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Win10 64bit too, and on my computer, path is "c:\ProgramData\NXP\mcu_data_v4.1"&lt;A&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 05:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790711#M463</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2018-07-31T05:55:08Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790712#M464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marek,&lt;/P&gt;&lt;P&gt;To answer your question about deleting the ProgramData/mcu_data_v4.1 folder, yes, the program appears to recreate the folder, if deleted. It looks like it also places several folders and an xml document inside of the folder as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also tried to recreate the folder and I gave myself "Full Control" through the Security Tab of the mcu_data_v4.1 folder.&lt;/P&gt;&lt;P&gt;Still getting the same error. Additionally I am administrator to the local PC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 12:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790712#M464</guid>
      <dc:creator>jturner</dc:creator>
      <dc:date>2018-07-31T12:02:04Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790713#M465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK, I had my co-worker try to install MCUXpresso Config Tools on his computer as well, he is also getting the same error message. He essentially has the same setup as I do (local admin rights)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 12:04:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790713#M465</guid>
      <dc:creator>jturner</dc:creator>
      <dc:date>2018-07-31T12:04:16Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790714#M466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is strange that some files/folders are created and then it is complaining. Could you please ZIP the content of the folder and upload here so I we see if some files are missing and which. I have a tip that it could be caused by antivirus - could you disable the antivirus before the tool downloads the data? The data contains javascript files, they might be blocked (just guessing).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please also attach log file located here? c:\Users\&lt;STRONG&gt;&amp;lt;yourusername&amp;gt;&lt;/STRONG&gt;\.nxp\swtools.log&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 14:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790714#M466</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2018-07-31T14:37:47Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790715#M467</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Libor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see the attached.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ill try disabling the anti virus software to see if it makes a difference.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 31 Jul 2018 14:46:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790715#M467</guid>
      <dc:creator>jturner</dc:creator>
      <dc:date>2018-07-31T14:46:41Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to create new configuration for processor</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790716#M468</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello,&lt;/P&gt;&lt;P&gt;it helped, it seems that some process (?Antivirus?) is holding the temporary directory which can't be cleaned.&lt;/P&gt;&lt;P&gt;Please do these steps:&lt;/P&gt;&lt;P&gt;1) close the tool&lt;/P&gt;&lt;P&gt;2) make a backup of c:\nxp\MCUX_CFG_v4_1\bin\plugins\com.nxp.kex.standalone_1.0.0.201805101316.jar&lt;/P&gt;&lt;P&gt;3) replace file from point 2) with the attached file&lt;/P&gt;&lt;P&gt;4) start the tool, try to create new configuration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if it resolves the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Aug 2018 12:29:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Unable-to-create-new-configuration-for-processor/m-p/790716#M468</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2018-08-01T12:29:53Z</dc:date>
    </item>
  </channel>
</rss>