<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config Tools中的主题 Where is the driver selection in Config Tools v4?</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777812#M441</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I choose to create a new configuration based on the Hello World example, and then try to configure the SPI1 peripheral it show an error saying the driver is not found. Ok, well, why doesn't it let me import it? The config tools know which SDK I am using, it should be able to import the necessary driver files.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 10 Dec 2017 17:34:54 GMT</pubDate>
    <dc:creator>benjaminnoack</dc:creator>
    <dc:date>2017-12-10T17:34:54Z</dc:date>
    <item>
      <title>Where is the driver selection in Config Tools v4?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777812#M441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I choose to create a new configuration based on the Hello World example, and then try to configure the SPI1 peripheral it show an error saying the driver is not found. Ok, well, why doesn't it let me import it? The config tools know which SDK I am using, it should be able to import the necessary driver files.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Dec 2017 17:34:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777812#M441</guid>
      <dc:creator>benjaminnoack</dc:creator>
      <dc:date>2017-12-10T17:34:54Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the driver selection in Config Tools v4?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777813#M442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Benjamin,&lt;/P&gt;&lt;P&gt;if you are using MCUXpresso IDE, just click on the problem in Problems view and select "Add component". Several problems allows to be fixed this way.&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 07:06:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777813#M442</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2017-12-11T07:06:36Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the driver selection in Config Tools v4?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777814#M443</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-userid="309118" data-username="benjaminnoack" href="https://community.nxp.com/people/benjaminnoack"&gt;Benjamin Noack&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When using the MCUXpresso Config tool to config peripherals, it generate two files "peripherals.c" and "peripherals.h",&lt;/P&gt;&lt;P&gt;it only includes the initialize information code, the drivers are in driver&amp;nbsp; files, when you create project, you need choose&lt;/P&gt;&lt;P&gt;peripherals driver that you need. Please ignore the error , in fact, the initialize code has generate in the peripherals .c file,&lt;/P&gt;&lt;P&gt;just export them , then add them into your project 。&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/4449i1DD265FC052271B7/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also if you need MCUXpresso IDE, you can refer to Marek's said righting&amp;nbsp; click the error&lt;/P&gt;&lt;P&gt;reminder, then choose Add component .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 08:25:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777814#M443</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2017-12-11T08:25:53Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the driver selection in Config Tools v4?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777815#M444</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;error "XXX Driver is missing" means, that the driver is not included&amp;nbsp;in the toolchain project. This does not cause any problem for Config Tools, e.g. you can ignore the error continue working in&amp;nbsp;Config Tools, but when you switch back to&amp;nbsp;IDE (MDK, IAR or MCUXpresso IDE), the project will not be compilable until you add the SDK driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Marek&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Dec 2017 09:36:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777815#M444</guid>
      <dc:creator>marek-trmac</dc:creator>
      <dc:date>2017-12-11T09:36:06Z</dc:date>
    </item>
    <item>
      <title>Re: Where is the driver selection in Config Tools v4?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777816#M445</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, so it seems the config tools no longer support the automatic inclusion of drivers during project creation. That is disappointing. The screenshot I attached is from v3 and it was a nice feature. Thank you for the reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Dec 2017 01:52:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Where-is-the-driver-selection-in-Config-Tools-v4/m-p/777816#M445</guid>
      <dc:creator>benjaminnoack</dc:creator>
      <dc:date>2017-12-13T01:52:55Z</dc:date>
    </item>
  </channel>
</rss>