<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config Tools中的主题 Using clock tool code to switch between RUN and HSRUN</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-clock-tool-code-to-switch-between-RUN-and-HSRUN/m-p/767574#M416</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use the clock config tool to generate 2 clock configurations, a "HighPower" mode (run mode = HSRUN) and a "LowPower" mode (run mode = RUN).&amp;nbsp; My intent is to save power by switching back and forth between these two clock configurations depending on the processing needs. I have the 2 configurations set up in the MCUXpresso Config Tools, but when I observe the generated C source, the "LowPower" mode lacks code to switch the run mode back to RUN.&amp;nbsp; There is code in the "HighPower" mode to change the run mode to HSRUN, but if I switch back to "LowPower" the device will not be switched back to RUN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a bug in the tool?&amp;nbsp; A configuration error on my part?&amp;nbsp;&amp;nbsp;A misuse of the tool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MCUXpress config tools v4.&amp;nbsp; Thanks for any insight.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Mar 2018 17:35:23 GMT</pubDate>
    <dc:creator>chriskeeser</dc:creator>
    <dc:date>2018-03-16T17:35:23Z</dc:date>
    <item>
      <title>Using clock tool code to switch between RUN and HSRUN</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-clock-tool-code-to-switch-between-RUN-and-HSRUN/m-p/767574#M416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to use the clock config tool to generate 2 clock configurations, a "HighPower" mode (run mode = HSRUN) and a "LowPower" mode (run mode = RUN).&amp;nbsp; My intent is to save power by switching back and forth between these two clock configurations depending on the processing needs. I have the 2 configurations set up in the MCUXpresso Config Tools, but when I observe the generated C source, the "LowPower" mode lacks code to switch the run mode back to RUN.&amp;nbsp; There is code in the "HighPower" mode to change the run mode to HSRUN, but if I switch back to "LowPower" the device will not be switched back to RUN.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this a bug in the tool?&amp;nbsp; A configuration error on my part?&amp;nbsp;&amp;nbsp;A misuse of the tool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MCUXpress config tools v4.&amp;nbsp; Thanks for any insight.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Mar 2018 17:35:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-clock-tool-code-to-switch-between-RUN-and-HSRUN/m-p/767574#M416</guid>
      <dc:creator>chriskeeser</dc:creator>
      <dc:date>2018-03-16T17:35:23Z</dc:date>
    </item>
    <item>
      <title>Re: Using clock tool code to switch between RUN and HSRUN</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-clock-tool-code-to-switch-between-RUN-and-HSRUN/m-p/767575#M417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="292518" data-username="chriskeeser" href="https://community.nxp.com/people/chriskeeser"&gt;Chris Keeser&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;In my&amp;nbsp; opinion, the MCUXpresso Config tools for clock just configure&lt;/P&gt;&lt;P&gt;the run mode and clock mode , so it doesn't include the switch function from one mode to another,&lt;/P&gt;&lt;P&gt;we need change by our own code.&lt;/P&gt;&lt;P&gt;And about there is no configure in RUN mode(normal run state) on "LowPower",&amp;nbsp; because the default mode&lt;/P&gt;&lt;P&gt;after any reset is normal run state .&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Mar 2018 04:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-clock-tool-code-to-switch-between-RUN-and-HSRUN/m-p/767575#M417</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-03-22T04:01:04Z</dc:date>
    </item>
  </channel>
</rss>