<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config ToolsのトピックRe: Using MCUXpresso Config Tools to specify pin direction</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-MCUXpresso-Config-Tools-to-specify-pin-direction/m-p/767006#M415</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andy,&lt;/P&gt;&lt;P&gt;today is available Config Tools v4.1 which generates the&amp;nbsp;code for the direction, when configured in the tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 May 2018 07:04:10 GMT</pubDate>
    <dc:creator>liborukropec</dc:creator>
    <dc:date>2018-05-18T07:04:10Z</dc:date>
    <item>
      <title>Using MCUXpresso Config Tools to specify pin direction</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-MCUXpresso-Config-Tools-to-specify-pin-direction/m-p/767005#M414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using MCUXpresso Config Tools to generate the BOARD_InitPins() function. I am trying to initialize a couple of pins as GPIO (some as input, others as output).&amp;nbsp;I am able to set the routed pin direction on the "Routed Pins" tab, but it seems that there is no code generated that actually sets the port direction register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is Config Tools able to generate C code to configure the port data direction?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 May 2018 18:31:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-MCUXpresso-Config-Tools-to-specify-pin-direction/m-p/767005#M414</guid>
      <dc:creator>aberger</dc:creator>
      <dc:date>2018-05-17T18:31:41Z</dc:date>
    </item>
    <item>
      <title>Re: Using MCUXpresso Config Tools to specify pin direction</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-MCUXpresso-Config-Tools-to-specify-pin-direction/m-p/767006#M415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Andy,&lt;/P&gt;&lt;P&gt;today is available Config Tools v4.1 which generates the&amp;nbsp;code for the direction, when configured in the tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 May 2018 07:04:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Using-MCUXpresso-Config-Tools-to-specify-pin-direction/m-p/767006#M415</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2018-05-18T07:04:10Z</dc:date>
    </item>
  </channel>
</rss>