<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config Tools中的主题 Re: Config Tools Error from version 10 to version 15 for i.MX RT 1175</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Config-Tools-Error-from-version-10-to-version-15-for-i-MX-RT/m-p/1816491#M1812</link>
    <description>&lt;P&gt;Hello Michael,&lt;/P&gt;
&lt;P&gt;sorry for inconvenience.&lt;BR /&gt;&lt;BR /&gt;There has been added new conflict check in the pin routing set by SELECT_INPUT registers in IOMUXC peripheral. This check was missing in the data for the tool version 10.&lt;/P&gt;
&lt;P&gt;ENET_QOS peripheral is available only on i.MX RT1176, it was removed from the tools data for i.MX RT1175 &lt;SPAN&gt;intentionally.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jan Kucera&lt;/P&gt;</description>
    <pubDate>Tue, 27 Feb 2024 10:21:36 GMT</pubDate>
    <dc:creator>Jan_Kucera</dc:creator>
    <dc:date>2024-02-27T10:21:36Z</dc:date>
    <item>
      <title>Config Tools Error from version 10 to version 15 for i.MX RT 1175</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Config-Tools-Error-from-version-10-to-version-15-for-i-MX-RT/m-p/1815956#M1809</link>
      <description>&lt;P class=""&gt;Updated MCUXpresso Config Tools from version 10 to version 15, and had some errors suddenly pop up in the configuration for i.MX RT 1175.&amp;nbsp; The first ones we noticed were between L2 and C13, and A15 and M4.&amp;nbsp; These four pins are connected to ENC2-4 peripherals.&amp;nbsp; Where there was no error before, now the tool says “The selected value is in conflict with the ‘Routed pin/signal’ value in ‘#(Pin Name Here)’ setting, a conflict in the configuration of the DAISY bit-field of the IOMUXC_XBAR1-IN_SELECT_INPUT_34(or 35) register.”&lt;/P&gt;&lt;P class=""&gt;Is there a reason why this error wasn’t in the previous tools, but is showing up now?&amp;nbsp; Do you know if there is a way around it, or if it just wasn’t being checked in the old tool?&lt;/P&gt;&lt;P class=""&gt;The other concerning error that popped up was ENET_QOS was no longer allowed to be routed on an RT1175 configuration.&amp;nbsp; It was fine with the new tool when the configuration was set to an RT1176 but said not supported with RT1175.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Feb 2024 21:48:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Config-Tools-Error-from-version-10-to-version-15-for-i-MX-RT/m-p/1815956#M1809</guid>
      <dc:creator>MichaelC_Future</dc:creator>
      <dc:date>2024-02-26T21:48:20Z</dc:date>
    </item>
    <item>
      <title>Re: Config Tools Error from version 10 to version 15 for i.MX RT 1175</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Config-Tools-Error-from-version-10-to-version-15-for-i-MX-RT/m-p/1816491#M1812</link>
      <description>&lt;P&gt;Hello Michael,&lt;/P&gt;
&lt;P&gt;sorry for inconvenience.&lt;BR /&gt;&lt;BR /&gt;There has been added new conflict check in the pin routing set by SELECT_INPUT registers in IOMUXC peripheral. This check was missing in the data for the tool version 10.&lt;/P&gt;
&lt;P&gt;ENET_QOS peripheral is available only on i.MX RT1176, it was removed from the tools data for i.MX RT1175 &lt;SPAN&gt;intentionally.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards&lt;/P&gt;
&lt;P&gt;Jan Kucera&lt;/P&gt;</description>
      <pubDate>Tue, 27 Feb 2024 10:21:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Config-Tools-Error-from-version-10-to-version-15-for-i-MX-RT/m-p/1816491#M1812</guid>
      <dc:creator>Jan_Kucera</dc:creator>
      <dc:date>2024-02-27T10:21:36Z</dc:date>
    </item>
  </channel>
</rss>