<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imxrt1052 i2c transfer mode when using  LPI2C_MasterTransferNonBlocking API stuck in irq_callbac in MCUXpresso Config Tools</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/imxrt1052-i2c-transfer-mode-when-using-LPI2C/m-p/1625973#M1670</link>
    <description>Note: When I use polling mode,and using LPI2C_MasterTransferBlocking API is used as the actual transmission interface, the transfer process is correct. so I think the information in "lpi2c_master_transfer_t transfer" structure is correct.</description>
    <pubDate>Fri, 31 Mar 2023 09:41:26 GMT</pubDate>
    <dc:creator>Huxiwa</dc:creator>
    <dc:date>2023-03-31T09:41:26Z</dc:date>
    <item>
      <title>imxrt1052 i2c transfer mode when using  LPI2C_MasterTransferNonBlocking API stuck in irq_callback</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/imxrt1052-i2c-transfer-mode-when-using-LPI2C/m-p/1625963#M1668</link>
      <description>&lt;P&gt;hello， NXP developers，when i used the MCUXpresso Config Tools v12.1 to configure LPI2C as transfer mode, and then using LPI2C_MasterTransferNonBlocking API as actual&amp;nbsp; transmission interface, my code program stuck in irq_callback.Then, I used keil's call stack and obtained the following information.&lt;/P&gt;&lt;P&gt;I don't know where the problem is. Can you give me some help&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Huxiwa_1-1680255011502.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/217298i494B7FBA5FBBA120/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Huxiwa_1-1680255011502.png" alt="Huxiwa_1-1680255011502.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 31 Mar 2023 09:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/imxrt1052-i2c-transfer-mode-when-using-LPI2C/m-p/1625963#M1668</guid>
      <dc:creator>Huxiwa</dc:creator>
      <dc:date>2023-03-31T09:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: imxrt1052 i2c transfer mode when using  LPI2C_MasterTransferNonBlocking API stuck in irq_callbac</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/imxrt1052-i2c-transfer-mode-when-using-LPI2C/m-p/1625973#M1670</link>
      <description>Note: When I use polling mode,and using LPI2C_MasterTransferBlocking API is used as the actual transmission interface, the transfer process is correct. so I think the information in "lpi2c_master_transfer_t transfer" structure is correct.</description>
      <pubDate>Fri, 31 Mar 2023 09:41:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/imxrt1052-i2c-transfer-mode-when-using-LPI2C/m-p/1625973#M1670</guid>
      <dc:creator>Huxiwa</dc:creator>
      <dc:date>2023-03-31T09:41:26Z</dc:date>
    </item>
  </channel>
</rss>