<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config ToolsのトピックRe: processor data for MK10DN32VFM5 device</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1522169#M1491</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206354"&gt;@audinus&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I am sorry for the misunderstanding, but with "processor data" do you mean an SDK package?&lt;/P&gt;
&lt;P&gt;If so, please refer to&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;and search for the MK10. Then select and download the SDK for the TWR-K60, and since both share the same memory map, you could port the example into the MK10.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you have any doubts about the device or the peripherals, don't hestitate to ask! Hope you find this helpful.&lt;/P&gt;
&lt;P&gt;Best regards, Julian&lt;/P&gt;</description>
    <pubDate>Wed, 14 Sep 2022 18:06:07 GMT</pubDate>
    <dc:creator>Julián_AragónM</dc:creator>
    <dc:date>2022-09-14T18:06:07Z</dc:date>
    <item>
      <title>processor data for MK10DN32VFM5 device</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1521844#M1490</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am developing a board with&amp;nbsp;MK10DN32VFM5 device.&lt;/P&gt;&lt;P&gt;I tried to download processor data from MCUExpresso IDE or Config tool, but in vain;&lt;/P&gt;&lt;P&gt;&amp;nbsp; There is no data for the device !&lt;/P&gt;&lt;P&gt;Can I download the data for&amp;nbsp;MK10DN32VFM5 ?&lt;/P&gt;&lt;P&gt;Help needed.&lt;/P&gt;&lt;P&gt;Thanks ~&lt;/P&gt;&lt;P&gt;#MK10DN32VFM5&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 09:02:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1521844#M1490</guid>
      <dc:creator>audinus</dc:creator>
      <dc:date>2022-09-14T09:02:53Z</dc:date>
    </item>
    <item>
      <title>Re: processor data for MK10DN32VFM5 device</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1522169#M1491</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/206354"&gt;@audinus&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;I am sorry for the misunderstanding, but with "processor data" do you mean an SDK package?&lt;/P&gt;
&lt;P&gt;If so, please refer to&amp;nbsp;&lt;A href="https://mcuxpresso.nxp.com/en/select" target="_blank"&gt;https://mcuxpresso.nxp.com/en/select&lt;/A&gt;&amp;nbsp;and search for the MK10. Then select and download the SDK for the TWR-K60, and since both share the same memory map, you could port the example into the MK10.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;If you have any doubts about the device or the peripherals, don't hestitate to ask! Hope you find this helpful.&lt;/P&gt;
&lt;P&gt;Best regards, Julian&lt;/P&gt;</description>
      <pubDate>Wed, 14 Sep 2022 18:06:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1522169#M1491</guid>
      <dc:creator>Julián_AragónM</dc:creator>
      <dc:date>2022-09-14T18:06:07Z</dc:date>
    </item>
    <item>
      <title>Re: processor data for MK10DN32VFM5 device</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1522389#M1492</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/200831"&gt;@Julián_AragónM&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;Thanks for your answer.&lt;/P&gt;&lt;P&gt;I tried to switch processor in MCUXpresso Config Tool by using pull-down menu "File -&amp;gt; Switch Processor",&lt;/P&gt;&lt;P&gt;but is only shows - MK10DN512xxx10 which starts with "MK10DN".&lt;/P&gt;&lt;P&gt;Moreover the&amp;nbsp;MK10DN512xxx10 processor does not have 32pin package in the tool.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, I understood that I can use the SDK which follows&amp;nbsp;MK10DN512xxx10 device.&lt;/P&gt;&lt;P&gt;My question is if I could use the MCUXpresso Config Tool for MK10DN32VFN5 device&lt;/P&gt;&lt;P&gt;&amp;nbsp; &amp;nbsp; which, I guess, requires proper "processor data" .&lt;/P&gt;&lt;P&gt;If the answer is "No", I should start to build a platform code with the register maps and SDK&amp;nbsp;&lt;/P&gt;&lt;P&gt;modification.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 15 Sep 2022 00:28:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1522389#M1492</guid>
      <dc:creator>audinus</dc:creator>
      <dc:date>2022-09-15T00:28:33Z</dc:date>
    </item>
    <item>
      <title>Re: processor data for MK10DN32VFM5 device</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1522397#M1493</link>
      <description>From the "MCUXpresso Supported Devices Table (July 2022).xlsx" file, I just found that this device "MK10DN32VFM5" is not &amp;amp; will not be supported by MCUXpresso tools.&lt;BR /&gt;Thanks.</description>
      <pubDate>Thu, 15 Sep 2022 00:47:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/processor-data-for-MK10DN32VFM5-device/m-p/1522397#M1493</guid>
      <dc:creator>audinus</dc:creator>
      <dc:date>2022-09-15T00:47:46Z</dc:date>
    </item>
  </channel>
</rss>