<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config ToolsのトピックRe: How to configure OPWMCB to trigger ADC conversion using MCUXpresso</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-configure-OPWMCB-to-trigger-ADC-conversion-using/m-p/1509299#M1469</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;theoretically&lt;SPAN&gt;, in OPWMCB mode you need to select the timebase using Bus Select (Cn[BSL]). The timebase you select must be running in Up Count-Down Count mode and this timebase define PWM period. The channel generating this timebase can be then used to trigger ADC conversions at period boundary.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;See MCB mode description to know more about flag generation in MCB Up Count-Down Count mode.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can refer&amp;nbsp;to below example for BTCU ADC triggering. PIT is used to trigger BTCU but you can add eMIOS and modify TRGMUX module to use eMIOS instead&amp;nbsp;if PIT&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-ADC-DMA-DS3-4-RTD100/ta-p/1435324" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-ADC-DMA-DS3-4-RTD100/ta-p/1435324&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 22 Aug 2022 07:50:30 GMT</pubDate>
    <dc:creator>PetrS</dc:creator>
    <dc:date>2022-08-22T07:50:30Z</dc:date>
    <item>
      <title>How to configure OPWMCB to trigger ADC conversion using MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-configure-OPWMCB-to-trigger-ADC-conversion-using/m-p/1507048#M1468</link>
      <description>&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;I'm using S32K344 and S32K3 RTD AUTOSAR 4.4 2.0.1 D2207.&lt;/P&gt;&lt;P&gt;I would like to configure the PWM as OPWMCB (Center aligned Output PWM Buffered) using 6 aligned channels and notify via software or automatically trigger ADC conversion via hardware, occurring at the beginning of cycle as circled in the image below:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="MarcusVR_0-1660684448226.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/190421iD31BFF34AF0EA716/image-size/medium?v=v2&amp;amp;px=400" role="button" title="MarcusVR_0-1660684448226.png" alt="MarcusVR_0-1660684448226.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I would like to use BCTU for trigger ADC conversion (recommended in application note), how I can configure using the MCUXpresso Config Tools?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Tue, 16 Aug 2022 21:20:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-configure-OPWMCB-to-trigger-ADC-conversion-using/m-p/1507048#M1468</guid>
      <dc:creator>MVR</dc:creator>
      <dc:date>2022-08-16T21:20:08Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure OPWMCB to trigger ADC conversion using MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-configure-OPWMCB-to-trigger-ADC-conversion-using/m-p/1509299#M1469</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;theoretically&lt;SPAN&gt;, in OPWMCB mode you need to select the timebase using Bus Select (Cn[BSL]). The timebase you select must be running in Up Count-Down Count mode and this timebase define PWM period. The channel generating this timebase can be then used to trigger ADC conversions at period boundary.&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;See MCB mode description to know more about flag generation in MCB Up Count-Down Count mode.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can refer&amp;nbsp;to below example for BTCU ADC triggering. PIT is used to trigger BTCU but you can add eMIOS and modify TRGMUX module to use eMIOS instead&amp;nbsp;if PIT&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;A href="https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-ADC-DMA-DS3-4-RTD100/ta-p/1435324" target="_blank"&gt;https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-PIT-BTCU-ADC-DMA-DS3-4-RTD100/ta-p/1435324&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;BR, Petr&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 22 Aug 2022 07:50:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-configure-OPWMCB-to-trigger-ADC-conversion-using/m-p/1509299#M1469</guid>
      <dc:creator>PetrS</dc:creator>
      <dc:date>2022-08-22T07:50:30Z</dc:date>
    </item>
    <item>
      <title>Re: How to configure OPWMCB to trigger ADC conversion using MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-configure-OPWMCB-to-trigger-ADC-conversion-using/m-p/1511954#M1475</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/52961"&gt;@PetrS&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;I saw your example, I will test. If I define the timebase in EMIOS MCL being "Up Count-Down Count", is it enough to BCTU generate the trigger when I link with some EMIOS PWM channel?&lt;/P&gt;&lt;P&gt;I have read the document "AN13413 - ADC Guidelines Spec and Configuration" as well and I understand that there are two options for it:&lt;/P&gt;&lt;P&gt;1) EMIOS -&amp;gt; TRGMUX -&amp;gt; BCTU -&amp;gt; ADC&lt;/P&gt;&lt;P&gt;2) EMIOS -&amp;gt; BCTU -&amp;gt; ADC&lt;/P&gt;&lt;P&gt;Why we need of TRGMUX in this case? Really is it necessary?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;MVR&lt;/P&gt;</description>
      <pubDate>Thu, 25 Aug 2022 22:03:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/How-to-configure-OPWMCB-to-trigger-ADC-conversion-using/m-p/1511954#M1475</guid>
      <dc:creator>MVR</dc:creator>
      <dc:date>2022-08-25T22:03:31Z</dc:date>
    </item>
  </channel>
</rss>