<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config Tools中的主题 Re: Changing processor - doesn't work on desktop after, export/download/processor type</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Changing-processor-doesn-t-work-on-desktop-after-export-download/m-p/646281#M136</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Robert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure what exact steps you did. Could you please check&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) go to &lt;STRONG&gt;c:\ProgramData\NXP\mcu_data_v3\processors\&lt;/STRONG&gt; and delete (or move somewhere else) the folder &lt;STRONG&gt;MK20DX256xxx10&lt;/STRONG&gt; in case the data is somehow corrupted, so it will be downloaded again&lt;/P&gt;&lt;P&gt;2) start the tool and create a new configuration without SDK package(last option in the wizard)- are you able to create the configuration?&lt;/P&gt;&lt;P&gt;3) from what I can read I can see you are using the SDK - could you create a configuration with the SDk (first option in wizard) - are you able to create ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it's possible could you post here your MEX file that you cannot open? (or send me an PM message)&lt;/P&gt;&lt;P&gt;Also you can attach &lt;STRONG&gt;c:\users\&amp;lt;USER&amp;gt;\.nxp\swtools.log&lt;/STRONG&gt; which may be helpful to see if there's any problem reported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have exact steps how to reproduce your issue, please describe them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and regards,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 04 Apr 2017 06:46:02 GMT</pubDate>
    <dc:creator>liborukropec</dc:creator>
    <dc:date>2017-04-04T06:46:02Z</dc:date>
    <item>
      <title>Changing processor - doesn't work on desktop after, export/download/processor type</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Changing-processor-doesn-t-work-on-desktop-after-export-download/m-p/646280#M135</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to download V2.0 and configure an MK60DN512VLL10 processor without problem on my desktop pc. I downloaded V3.0 of the config tool, and built a V2.2 SDK for the MK20DX256VLL10 processor with the IAR toolset and some middleware. When I try to use the&amp;nbsp;&lt;SPAN&gt;MK20DX256VLL10 package nothing happens.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I successfully went to file /export/download/processor K type and the whole set downloaded. But when I try to use the above package again nothing happens. This works correctly on my Notebook computer but not the desktop. The first processor package I downloaded to the Notebook was the&amp;nbsp;MK20DX256VLL10 so maybe that is related, and the first package I downloaded on the desktop was the&amp;nbsp;MK60DN512VLL10 and that works.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I took the&amp;nbsp;MK20dx256VLL10.mex file from the notebook and loaded it into the desktop. It fails to load and says:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/17607i04BD15181870906F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;When I check the SDK version it says v2.0 even though I am using V2.2.... I put that down to sloppy versioning in the tool but that is an assumption. The config tool on the notebook is v3.0 and the sdk is definitely v2.2, so I don't know why the config tool can't read its own .mex file. Something is misaligned somewhere.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Is there somewhere that the paths can be checked or changed on the config tool? This has stopped the project until we can generate the pin mux code.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Thanks for any help offered.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Robert&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 04:20:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Changing-processor-doesn-t-work-on-desktop-after-export-download/m-p/646280#M135</guid>
      <dc:creator>Cdn_aye</dc:creator>
      <dc:date>2017-04-04T04:20:00Z</dc:date>
    </item>
    <item>
      <title>Re: Changing processor - doesn't work on desktop after, export/download/processor type</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Changing-processor-doesn-t-work-on-desktop-after-export-download/m-p/646281#M136</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Robert,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm not sure what exact steps you did. Could you please check&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1) go to &lt;STRONG&gt;c:\ProgramData\NXP\mcu_data_v3\processors\&lt;/STRONG&gt; and delete (or move somewhere else) the folder &lt;STRONG&gt;MK20DX256xxx10&lt;/STRONG&gt; in case the data is somehow corrupted, so it will be downloaded again&lt;/P&gt;&lt;P&gt;2) start the tool and create a new configuration without SDK package(last option in the wizard)- are you able to create the configuration?&lt;/P&gt;&lt;P&gt;3) from what I can read I can see you are using the SDK - could you create a configuration with the SDk (first option in wizard) - are you able to create ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If it's possible could you post here your MEX file that you cannot open? (or send me an PM message)&lt;/P&gt;&lt;P&gt;Also you can attach &lt;STRONG&gt;c:\users\&amp;lt;USER&amp;gt;\.nxp\swtools.log&lt;/STRONG&gt; which may be helpful to see if there's any problem reported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have exact steps how to reproduce your issue, please describe them.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and regards,&lt;/P&gt;&lt;P&gt;Libor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Apr 2017 06:46:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Changing-processor-doesn-t-work-on-desktop-after-export-download/m-p/646281#M136</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2017-04-04T06:46:02Z</dc:date>
    </item>
    <item>
      <title>Re: Changing processor - doesn't work on desktop after, export/download/processor type</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Changing-processor-doesn-t-work-on-desktop-after-export-download/m-p/646282#M137</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think there might have been an internet or server problem. I went back the next day and was able to export/download all the parts. Thanks for the help&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Robert&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Apr 2017 05:01:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/Changing-processor-doesn-t-work-on-desktop-after-export-download/m-p/646282#M137</guid>
      <dc:creator>Cdn_aye</dc:creator>
      <dc:date>2017-04-14T05:01:30Z</dc:date>
    </item>
  </channel>
</rss>