<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic BUG REPORT - Typo in MCUXpresso Config Tools generated file for LPADC in MCUXpresso Config Tools</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/BUG-REPORT-Typo-in-MCUXpresso-Config-Tools-generated-file-for/m-p/1414526#M1323</link>
    <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I recently ran into an error, where the file peripherals.c autogenerated with the MCUXpresso Config Tools had a typo, when I was trying to configure LPADC1 for a project on 1170-evk.&lt;/P&gt;&lt;P&gt;As seen in the linked image,&amp;nbsp;triggerPriorityPolicy has been misspelled as&amp;nbsp;triggerPrioirtyPolicy in the generated file, which in turn causes a failure to build the project (the "on disk" file is the one I fixed manually).&lt;/P&gt;&lt;P&gt;While it was relatively easy to fix manually, I figured that you would like to know it, so it can be fixed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Mathias&lt;/P&gt;</description>
    <pubDate>Wed, 16 Feb 2022 14:41:12 GMT</pubDate>
    <dc:creator>MathiasFriis</dc:creator>
    <dc:date>2022-02-16T14:41:12Z</dc:date>
    <item>
      <title>BUG REPORT - Typo in MCUXpresso Config Tools generated file for LPADC</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/BUG-REPORT-Typo-in-MCUXpresso-Config-Tools-generated-file-for/m-p/1414526#M1323</link>
      <description>&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I recently ran into an error, where the file peripherals.c autogenerated with the MCUXpresso Config Tools had a typo, when I was trying to configure LPADC1 for a project on 1170-evk.&lt;/P&gt;&lt;P&gt;As seen in the linked image,&amp;nbsp;triggerPriorityPolicy has been misspelled as&amp;nbsp;triggerPrioirtyPolicy in the generated file, which in turn causes a failure to build the project (the "on disk" file is the one I fixed manually).&lt;/P&gt;&lt;P&gt;While it was relatively easy to fix manually, I figured that you would like to know it, so it can be fixed.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Mathias&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 14:41:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/BUG-REPORT-Typo-in-MCUXpresso-Config-Tools-generated-file-for/m-p/1414526#M1323</guid>
      <dc:creator>MathiasFriis</dc:creator>
      <dc:date>2022-02-16T14:41:12Z</dc:date>
    </item>
    <item>
      <title>Re: BUG REPORT - Typo in MCUXpresso Config Tools generated file for LPADC</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/BUG-REPORT-Typo-in-MCUXpresso-Config-Tools-generated-file-for/m-p/1414615#M1324</link>
      <description>&lt;P&gt;Hi Mathias,&lt;/P&gt;
&lt;P&gt;there was this typo in the older SDK drivers and we have to have output code the same.&lt;/P&gt;
&lt;P&gt;It has been fixed since version 2.2.0 in driver as well as in component version 2.2.0 and newer.&lt;/P&gt;
&lt;P&gt;It seems like you have newer driver than component version.&lt;/P&gt;
&lt;P&gt;In latest release of Config tools v11, there is menu command for migration to other component version, see attached screenshot.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jch_0-1645032112257.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/170787i4BDA0A1F434459F5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jch_0-1645032112257.png" alt="jch_0-1645032112257.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 16 Feb 2022 17:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/BUG-REPORT-Typo-in-MCUXpresso-Config-Tools-generated-file-for/m-p/1414615#M1324</guid>
      <dc:creator>jch</dc:creator>
      <dc:date>2022-02-16T17:22:22Z</dc:date>
    </item>
  </channel>
</rss>