<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic can't add watchdog to KE02Z32VLC4 project in MCUXpresso Config Tools</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1396880#M1295</link>
    <description>&lt;P&gt;I'm trying to add the watchdog to my project and configure it with MCUXpresso IDE peripherals. &amp;nbsp;The watchdog does not show up in the Peripherals window.&lt;/P&gt;&lt;P&gt;Clicking the Open SDK components manager shows the checkbox selected in the Drivers. &amp;nbsp;Clicking the refresh SDK components doesn't seem to change anything.&lt;/P&gt;&lt;P&gt;How do you configure it?&lt;/P&gt;</description>
    <pubDate>Mon, 10 Jan 2022 19:35:53 GMT</pubDate>
    <dc:creator>dporada</dc:creator>
    <dc:date>2022-01-10T19:35:53Z</dc:date>
    <item>
      <title>can't add watchdog to KE02Z32VLC4 project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1396880#M1295</link>
      <description>&lt;P&gt;I'm trying to add the watchdog to my project and configure it with MCUXpresso IDE peripherals. &amp;nbsp;The watchdog does not show up in the Peripherals window.&lt;/P&gt;&lt;P&gt;Clicking the Open SDK components manager shows the checkbox selected in the Drivers. &amp;nbsp;Clicking the refresh SDK components doesn't seem to change anything.&lt;/P&gt;&lt;P&gt;How do you configure it?&lt;/P&gt;</description>
      <pubDate>Mon, 10 Jan 2022 19:35:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1396880#M1295</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2022-01-10T19:35:53Z</dc:date>
    </item>
    <item>
      <title>Re: can't add watchdog to KE02Z32VLC4 project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1398672#M1297</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;I have checked the availability of the wdog component on the MKE02Z32VLC4 MCU but this variant of the wdog driver (platform.drivers.wdog8 SDK component) is not supported in the Peripherals tool yet.&lt;/P&gt;
&lt;P&gt;I will create a request to support this component in the next release of MCUXpresso Config Tools.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Marek Neuzil&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 07:09:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1398672#M1297</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2022-01-13T07:09:12Z</dc:date>
    </item>
    <item>
      <title>Re: can't add watchdog to KE02Z32VLC4 project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1398999#M1300</link>
      <description>&lt;P&gt;Marek,&lt;/P&gt;&lt;P&gt;So I was using the tools correctly? &amp;nbsp;Is there tools that support this chip better?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Don&lt;/P&gt;</description>
      <pubDate>Thu, 13 Jan 2022 16:28:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1398999#M1300</guid>
      <dc:creator>dporada</dc:creator>
      <dc:date>2022-01-13T16:28:04Z</dc:date>
    </item>
    <item>
      <title>Re: can't add watchdog to KE02Z32VLC4 project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1399452#M1301</link>
      <description>&lt;P&gt;Hello Don,&lt;/P&gt;&lt;P&gt;The WDOG component cannot be added for MKE02Z32VLC4 MCU in the MCUXpresso Config Tools (Peripherals tool) but you can use the SDK drivers that supports the MCU in the MCUXpresso IDE. There are also SDK driver examples that demonstrate initialization and runtime API functionality of the drivers.&lt;/P&gt;&lt;P&gt;The MKE02Z332VLC4 MCU is also supported in&amp;nbsp;CodeWarrior for MCU, version: 11.1, in Processor Expert tool. This tool fully support the MCU but the drivers are generated. It also means that the generated code is not compatible with the SDK 2.x version (for example the SDK 2.11 for MKE02Z32).&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Marek Neuzil&lt;/P&gt;</description>
      <pubDate>Fri, 14 Jan 2022 11:29:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/can-t-add-watchdog-to-KE02Z32VLC4-project/m-p/1399452#M1301</guid>
      <dc:creator>marek_neuzil</dc:creator>
      <dc:date>2022-01-14T11:29:41Z</dc:date>
    </item>
  </channel>
</rss>