<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Config Tools中的主题 MCUXpresso Config Tools - Communication Error</title>
    <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/MCUXpresso-Config-Tools-Communication-Error/m-p/1352494#M1247</link>
    <description>&lt;P&gt;Just installed the MCUXpresso Config Tools v10, and tried opening one of my old .mex configurations, but it seems like there is something wrong with the connectivity for the program:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Communication error. Check the connectivity to the Internet and repeat again.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;A similar warning message is shown when trying to create a new configuration:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Network is not available or offline mode is on&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Previously, I used v9 of MCUXpresso Config Tools, but I was struggling with it crashing/not responding at startup, so I thought that upgrading to v10 could help.&lt;/P&gt;&lt;P&gt;I'm writing this post on the same computer, so I don't think network connectivity is the issue.&lt;/P&gt;</description>
    <pubDate>Fri, 08 Oct 2021 08:13:47 GMT</pubDate>
    <dc:creator>eam</dc:creator>
    <dc:date>2021-10-08T08:13:47Z</dc:date>
    <item>
      <title>MCUXpresso Config Tools - Communication Error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/MCUXpresso-Config-Tools-Communication-Error/m-p/1352494#M1247</link>
      <description>&lt;P&gt;Just installed the MCUXpresso Config Tools v10, and tried opening one of my old .mex configurations, but it seems like there is something wrong with the connectivity for the program:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Error&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Communication error. Check the connectivity to the Internet and repeat again.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;A similar warning message is shown when trying to create a new configuration:&lt;/P&gt;&lt;P&gt;&lt;EM&gt;Network is not available or offline mode is on&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;Previously, I used v9 of MCUXpresso Config Tools, but I was struggling with it crashing/not responding at startup, so I thought that upgrading to v10 could help.&lt;/P&gt;&lt;P&gt;I'm writing this post on the same computer, so I don't think network connectivity is the issue.&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 08:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/MCUXpresso-Config-Tools-Communication-Error/m-p/1352494#M1247</guid>
      <dc:creator>eam</dc:creator>
      <dc:date>2021-10-08T08:13:47Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso Config Tools - Communication Error</title>
      <link>https://community.nxp.com/t5/MCUXpresso-Config-Tools/MCUXpresso-Config-Tools-Communication-Error/m-p/1352731#M1248</link>
      <description>&lt;P&gt;Hello eam,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;could you please look to this post? &lt;A href="https://community.nxp.com/t5/MCUXpresso-Config-Tools/Why-config-tools-always-show-no-internet-link-and-cannot/m-p/1299059" target="_self"&gt;Why config tools always show no internet link, and cannot download more part number&lt;/A&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;There you can see my questions, that can be applied to you as well, including a workaround by downloading the data offline.&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Libor&lt;/P&gt;</description>
      <pubDate>Fri, 08 Oct 2021 13:47:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-Config-Tools/MCUXpresso-Config-Tools-Communication-Error/m-p/1352731#M1248</guid>
      <dc:creator>liborukropec</dc:creator>
      <dc:date>2021-10-08T13:47:10Z</dc:date>
    </item>
  </channel>
</rss>