<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: Is it possible to get access to the source of &amp;quot;MIMXRT1050-EVK_IS25WP064A.cfx&amp;quot; so it could be modified to work with two independent QSPI flashes</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828966#M987</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has this been done yet, and if so how do we get hold of it.&lt;/P&gt;&lt;P&gt;We have a RT1062 based board with the Hyperflash on it and need a means of programming it.&lt;/P&gt;&lt;P&gt;We do have IAR tools available also if its possible to do it with this instaed of McuXpresso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Oct 2018 09:53:40 GMT</pubDate>
    <dc:creator>martinhowell1</dc:creator>
    <dc:date>2018-10-24T09:53:40Z</dc:date>
    <item>
      <title>Is it possible to get access to the source of "MIMXRT1050-EVK_IS25WP064A.cfx" so it could be modified to work with two independent QSPI flashes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828964#M985</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We currently have two independent QSPI flash chips on our board and we can talk and XIP fine with the first chip, we can also access the second chip via our own driver we just cannot program it at debug time.&amp;nbsp; We have not tried the download tool yet and would rather not have to switch between different boot modes.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Jul 2018 21:48:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828964#M985</guid>
      <dc:creator>john_h_holste</dc:creator>
      <dc:date>2018-07-18T21:48:36Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to get access to the source of "MIMXRT1050-EVK_IS25WP064A.cfx" so it could be modified to work with two independent QSPI flashes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828965#M986</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;We expect to make an MCUXpresso IDE maintenance release around the end of this&amp;nbsp;month that will include updated i.MX RT LinkServer flash driver support. This will include i.MX RT example projects that can be used to create cfx files for programming other flash devices.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;MCUXpresso IDE Support&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Jul 2018 20:34:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828965#M986</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2018-07-20T20:34:32Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to get access to the source of "MIMXRT1050-EVK_IS25WP064A.cfx" so it could be modified to work with two independent QSPI flashes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828966#M987</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Has this been done yet, and if so how do we get hold of it.&lt;/P&gt;&lt;P&gt;We have a RT1062 based board with the Hyperflash on it and need a means of programming it.&lt;/P&gt;&lt;P&gt;We do have IAR tools available also if its possible to do it with this instaed of McuXpresso&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Oct 2018 09:53:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828966#M987</guid>
      <dc:creator>martinhowell1</dc:creator>
      <dc:date>2018-10-24T09:53:40Z</dc:date>
    </item>
    <item>
      <title>Re: Is it possible to get access to the source of "MIMXRT1050-EVK_IS25WP064A.cfx" so it could be modified to work with two independent QSPI flashes</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828967#M988</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to source code for the script to program QSPI on my own pcb. I use PEMicro multilink, and the flash programmation always failed. I think that's because I don't use signal DQS like rooted in the EVKB. I use FlexSPI A/B on 2 different chip (IS25LP064A). 'A' for XIP and 'B' for data storage. Is there somebody that can help me to find the right cfx file in my situation. The&amp;nbsp;MIMXRT1050-EVK_IS25WP064A.cfx doesn't work perfectly. It erase the chip, but got error during programming. Altough, If the code is compiled to execute in sram, the debugger work fine.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE class="" style="color: #000000; background: #f5f2f0; border: 0px; margin: 0.5em 0px; padding: 1em 1em 1em 3.8em;"&gt;&lt;CODE style="border: 0px; font-weight: inherit;"&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 22:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Is-it-possible-to-get-access-to-the-source-of-quot-MIMXRT1050/m-p/828967#M988</guid>
      <dc:creator>Lorac</dc:creator>
      <dc:date>2019-06-11T22:32:05Z</dc:date>
    </item>
  </channel>
</rss>