<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: How do I configure FlexBus with MCUXpresso Config Tools?</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-configure-FlexBus-with-MCUXpresso-Config-Tools/m-p/797810#M671</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Flexbus module is not supported in SDK Peripheral tool yet. I recommend you to use the Flexbus example from drivers example as a start point to create your application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Dec 2018 23:27:35 GMT</pubDate>
    <dc:creator>jorge_a_vazquez</dc:creator>
    <dc:date>2018-12-18T23:27:35Z</dc:date>
    <item>
      <title>How do I configure FlexBus with MCUXpresso Config Tools?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-configure-FlexBus-with-MCUXpresso-Config-Tools/m-p/797809#M670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to try driving an 8bit ILI9341 LCD on a FRDM-K64F board using the FlexBus. But for some reason I am unable to select the FlexBus peripheral or the FB component in the Peripherals tab of MCUXpresso Config Toools. Anyone know why that is?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my configuration/setup. I have MCUXpresso 10.2.1 with the latest SDK for MK64FN1M0xxx12 microcontrollers. My project is based on the FRDM-K64F board,&amp;nbsp;using FreeRTOS. I have the following drivers enabled: clock, common, flash, flexbus, gpio, port, sim, and smc; the project has semihosting enabled and using nanolib. I also have the FB_AD0 to FB_AD7 pins enabled for D0-D7 signals, FB_AD16 for D/C signal, FB_RW for R/W and FB_CS0 for LCD CS. The clocks are setup so that the system clock is 120 MHz and the FlexBus clock is 40 MHz.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I generate the code, the pinmux source file is showing correctly that all FB pins are being configured as FlexBus pins (alternate function 5) in the&amp;nbsp;BOARD_InitBootPins() function. But no matter what I do, I am not even able to see the FlexBus in the peripherals or components lists for selection... Isn't that possible at all?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Todor&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Dec 2018 03:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-configure-FlexBus-with-MCUXpresso-Config-Tools/m-p/797809#M670</guid>
      <dc:creator>tnt2</dc:creator>
      <dc:date>2018-12-14T03:02:51Z</dc:date>
    </item>
    <item>
      <title>Re: How do I configure FlexBus with MCUXpresso Config Tools?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-configure-FlexBus-with-MCUXpresso-Config-Tools/m-p/797810#M671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Flexbus module is not supported in SDK Peripheral tool yet. I recommend you to use the Flexbus example from drivers example as a start point to create your application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2018 23:27:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/How-do-I-configure-FlexBus-with-MCUXpresso-Config-Tools/m-p/797810#M671</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-12-18T23:27:35Z</dc:date>
    </item>
  </channel>
</rss>