<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 Using Segger J-link plus with FRDM-KV31F. Target machine actively refused it.</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Using-Segger-J-link-plus-with-FRDM-KV31F-Target-machine-actively/m-p/791663#M604</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I try to use the Segger J-Link plus with an FRDM-KV31F I get the following message.&lt;/P&gt;&lt;P&gt;"localhost:2336: No connection could be made because the target machine actively refused it."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the console I get this, "Checking target voltage...&amp;nbsp; Connecting to target failed. Connected correctly?&lt;/P&gt;&lt;P&gt;GDB Server will be closed..."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attach a photo of my connection - Have I done it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I have, any clues as to what is going on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also am attaching the messages generated.&amp;nbsp; The first window message is also duplicated in the console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also attached the Configuration for the Segger probe in MCUXpresso.&amp;nbsp; If I change from SWD connection to JTAG the results are the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tim Boatman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Jun 2018 18:59:17 GMT</pubDate>
    <dc:creator>timboatman</dc:creator>
    <dc:date>2018-06-18T18:59:17Z</dc:date>
    <item>
      <title>Using Segger J-link plus with FRDM-KV31F. Target machine actively refused it.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Using-Segger-J-link-plus-with-FRDM-KV31F-Target-machine-actively/m-p/791663#M604</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When I try to use the Segger J-Link plus with an FRDM-KV31F I get the following message.&lt;/P&gt;&lt;P&gt;"localhost:2336: No connection could be made because the target machine actively refused it."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the console I get this, "Checking target voltage...&amp;nbsp; Connecting to target failed. Connected correctly?&lt;/P&gt;&lt;P&gt;GDB Server will be closed..."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attach a photo of my connection - Have I done it right?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I have, any clues as to what is going on?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also am attaching the messages generated.&amp;nbsp; The first window message is also duplicated in the console.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also attached the Configuration for the Segger probe in MCUXpresso.&amp;nbsp; If I change from SWD connection to JTAG the results are the same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Tim Boatman&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jun 2018 18:59:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Using-Segger-J-link-plus-with-FRDM-KV31F-Target-machine-actively/m-p/791663#M604</guid>
      <dc:creator>timboatman</dc:creator>
      <dc:date>2018-06-18T18:59:17Z</dc:date>
    </item>
    <item>
      <title>Re: Using Segger J-link plus with FRDM-KV31F. Target machine actively refused it.</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Using-Segger-J-link-plus-with-FRDM-KV31F-Target-machine-actively/m-p/791664#M605</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="318961" data-username="timboatman" href="https://community.nxp.com/people/timboatman"&gt;Tim Boatman&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Could you please usa a demo project to have a try ? I just test on my side , it can work well.&lt;/P&gt;&lt;P&gt;And use the Debug button in "Quickstart Panel"&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/61963iADEBBAEBCB1CBF85/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;About debug , you can also have a look at "Chapter&amp;nbsp;11.&amp;nbsp;Debugging a Project -&amp;gt; &lt;A name="DebuggingOverview"&gt;&lt;/A&gt;Debugging Overview"&lt;/P&gt;&lt;P&gt;of "MCUXpresso IDE User Guide".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jun 2018 04:14:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Using-Segger-J-link-plus-with-FRDM-KV31F-Target-machine-actively/m-p/791664#M605</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-06-19T04:14:55Z</dc:date>
    </item>
  </channel>
</rss>