<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: Debugging on OM13087</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-on-OM13087/m-p/788344#M595</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luke,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried using the Clean-Up Debug button? It will kill all debug processes associated with LinkServer, P&amp;amp;E and&lt;BR /&gt;SEGGER debug connections. This button can be used in the event of a debugging crash to remove any failed processes that remain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62073i6BDDACE806720D14/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 05 Nov 2018 21:24:44 GMT</pubDate>
    <dc:creator>Carlos_Mendoza</dc:creator>
    <dc:date>2018-11-05T21:24:44Z</dc:date>
    <item>
      <title>Debugging on OM13087</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-on-OM13087/m-p/788343#M594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I`m having an issue with regards to the OM13087 dev board containing the LPC 1115 - I am able to install the software and run the blink.c example code, however whenever I attempt to debug a second time after killing the first debug session, the IDE informs me it cannot locate any probes&lt;/P&gt;&lt;P&gt;"Linkserver is disconnected, not powered or in use"&lt;/P&gt;&lt;P&gt;I am attempted to debug using the CMSIS-dap debug probe. Upon removing and reinstalling the software, I encountered the same issue, any help would be appreciated.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Oct 2018 12:17:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-on-OM13087/m-p/788343#M594</guid>
      <dc:creator>luke_abela_16</dc:creator>
      <dc:date>2018-10-31T12:17:37Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging on OM13087</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-on-OM13087/m-p/788344#M595</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Luke,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you tried using the Clean-Up Debug button? It will kill all debug processes associated with LinkServer, P&amp;amp;E and&lt;BR /&gt;SEGGER debug connections. This button can be used in the event of a debugging crash to remove any failed processes that remain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/62073i6BDDACE806720D14/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope it helps!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Carlos Mendoza&lt;BR /&gt;Technical Support Engineer&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Nov 2018 21:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-on-OM13087/m-p/788344#M595</guid>
      <dc:creator>Carlos_Mendoza</dc:creator>
      <dc:date>2018-11-05T21:24:44Z</dc:date>
    </item>
  </channel>
</rss>