<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic frdmrw612_lpc_gpio_input_interrupt does not work in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/frdmrw612-lpc-gpio-input-interrupt-does-not-work/m-p/2389790#M5833</link>
    <description>&lt;P&gt;The sample project&amp;nbsp;lpc_gpio_input_interrupt comes with the RW612 does not work!&lt;/P&gt;&lt;P&gt;Any idea??&lt;/P&gt;&lt;P&gt;Wang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Jul 2026 13:08:27 GMT</pubDate>
    <dc:creator>hswang2222</dc:creator>
    <dc:date>2026-07-02T13:08:27Z</dc:date>
    <item>
      <title>frdmrw612_lpc_gpio_input_interrupt does not work</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/frdmrw612-lpc-gpio-input-interrupt-does-not-work/m-p/2389790#M5833</link>
      <description>&lt;P&gt;The sample project&amp;nbsp;lpc_gpio_input_interrupt comes with the RW612 does not work!&lt;/P&gt;&lt;P&gt;Any idea??&lt;/P&gt;&lt;P&gt;Wang&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jul 2026 13:08:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/frdmrw612-lpc-gpio-input-interrupt-does-not-work/m-p/2389790#M5833</guid>
      <dc:creator>hswang2222</dc:creator>
      <dc:date>2026-07-02T13:08:27Z</dc:date>
    </item>
    <item>
      <title>Re: frdmrw612_lpc_gpio_input_interrupt does not work</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/frdmrw612-lpc-gpio-input-interrupt-does-not-work/m-p/2389858#M5834</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;What SDK version are you using?&lt;/P&gt;
&lt;P&gt;I just tried with SDK 26.06 and the example is running successfully.&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;MCUX SDK version: 2026.06.00
GPIO Driver example.
SW2 is turned on.
SW2 is turned on.
SW2 is turned on.
SW2 is turned on.&lt;/LI-CODE&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Daniel.&lt;/P&gt;</description>
      <pubDate>Thu, 02 Jul 2026 17:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/frdmrw612-lpc-gpio-input-interrupt-does-not-work/m-p/2389858#M5834</guid>
      <dc:creator>DanielRuvalcaba</dc:creator>
      <dc:date>2026-07-02T17:07:12Z</dc:date>
    </item>
  </channel>
</rss>