<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GDB PEMicro interface debugging not showing up in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/GDB-PEMicro-interface-debugging-not-showing-up/m-p/786446#M580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently installed Kinetis Deign Studio 3.2.0 on Mac OSX High Sierra and am I trying to flash a FRDM-KL26Z (am studying this at the University and everybody use Windows, unfortunatly).&lt;/P&gt;&lt;P&gt;I installed the GDB PEMicro packs, but the problem is that the only configuration that shows up into the Flash Configurations is GDB Segger J-Link Debugging.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried to select and deselect several options from Launch Configurations, without succes; the only thing that changes is J-Link dissapearing from Flash Configurations.&lt;/P&gt;&lt;P&gt;Any help, or suggestions?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74546i29F4D122877DDE8A/image-size/large?v=v2&amp;amp;px=999" title="gdb.png" alt="gdb.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 13 Oct 2018 09:44:35 GMT</pubDate>
    <dc:creator>catalin_iordach</dc:creator>
    <dc:date>2018-10-13T09:44:35Z</dc:date>
    <item>
      <title>GDB PEMicro interface debugging not showing up</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/GDB-PEMicro-interface-debugging-not-showing-up/m-p/786446#M580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recently installed Kinetis Deign Studio 3.2.0 on Mac OSX High Sierra and am I trying to flash a FRDM-KL26Z (am studying this at the University and everybody use Windows, unfortunatly).&lt;/P&gt;&lt;P&gt;I installed the GDB PEMicro packs, but the problem is that the only configuration that shows up into the Flash Configurations is GDB Segger J-Link Debugging.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've tried to select and deselect several options from Launch Configurations, without succes; the only thing that changes is J-Link dissapearing from Flash Configurations.&lt;/P&gt;&lt;P&gt;Any help, or suggestions?&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/74546i29F4D122877DDE8A/image-size/large?v=v2&amp;amp;px=999" title="gdb.png" alt="gdb.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 13 Oct 2018 09:44:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/GDB-PEMicro-interface-debugging-not-showing-up/m-p/786446#M580</guid>
      <dc:creator>catalin_iordach</dc:creator>
      <dc:date>2018-10-13T09:44:35Z</dc:date>
    </item>
    <item>
      <title>Re: GDB PEMicro interface debugging not showing up</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/GDB-PEMicro-interface-debugging-not-showing-up/m-p/786447#M581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Catalin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the Release notes of the KDS 3.2 there is a note that mentioned:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/75984i7DC5D56D1DC74805/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, for MAC, you only have support for Segger interface. I would like to recommend you MCUXpresso IDE which has full support for LinkServer, P&amp;amp;E or SEGGER.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Jorge Alcala&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 19 Oct 2018 21:30:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/GDB-PEMicro-interface-debugging-not-showing-up/m-p/786447#M581</guid>
      <dc:creator>jorge_a_vazquez</dc:creator>
      <dc:date>2018-10-19T21:30:12Z</dc:date>
    </item>
  </channel>
</rss>