<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPCXpresso824-MAX Board doesn't connect in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2178508#M5713</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just got a brand new&amp;nbsp;&lt;SPAN class=""&gt;LPCXpresso824-MAX Board,&lt;/SPAN&gt;&amp;nbsp;plugged it in and, apart from the 5V LED, nothing, no sign of life. (I thought that maybe the blinky program was pre loaded, but maybe not)&lt;/P&gt;&lt;P&gt;Anyway that's not the problem, MCUXpresso will not connect (see screen shot).&lt;/P&gt;&lt;P&gt;There is no UART connection for the board in the Device manager either.&lt;/P&gt;&lt;P&gt;I did install the 11U35 driver then realised that I have Win10 and didn't need to, but had the problem before I installed that.&lt;/P&gt;&lt;P&gt;I have rebooted the IDE and the computer. Still nothing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Wed, 01 Oct 2025 00:59:43 GMT</pubDate>
    <dc:creator>graynomad</dc:creator>
    <dc:date>2025-10-01T00:59:43Z</dc:date>
    <item>
      <title>LPCXpresso824-MAX Board doesn't connect</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2178508#M5713</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I just got a brand new&amp;nbsp;&lt;SPAN class=""&gt;LPCXpresso824-MAX Board,&lt;/SPAN&gt;&amp;nbsp;plugged it in and, apart from the 5V LED, nothing, no sign of life. (I thought that maybe the blinky program was pre loaded, but maybe not)&lt;/P&gt;&lt;P&gt;Anyway that's not the problem, MCUXpresso will not connect (see screen shot).&lt;/P&gt;&lt;P&gt;There is no UART connection for the board in the Device manager either.&lt;/P&gt;&lt;P&gt;I did install the 11U35 driver then realised that I have Win10 and didn't need to, but had the problem before I installed that.&lt;/P&gt;&lt;P&gt;I have rebooted the IDE and the computer. Still nothing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 01 Oct 2025 00:59:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2178508#M5713</guid>
      <dc:creator>graynomad</dc:creator>
      <dc:date>2025-10-01T00:59:43Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso824-MAX Board doesn't connect</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2180076#M5714</link>
      <description>&lt;P&gt;Hello&amp;nbsp;graynomad,&lt;/P&gt;
&lt;P&gt;Have you tried reinstalling the DAPLink firmware?&lt;/P&gt;
&lt;P&gt;The procedure is here:&lt;BR /&gt;&lt;A href="https://os.mbed.com/handbook/Firmware-LPCXpresso824-MAX" target="_blank"&gt;https://os.mbed.com/handbook/Firmware-LPCXpresso824-MAX&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Although the firmware is available here because it's deprecated.&lt;BR /&gt;&lt;A href="https://os.mbed.com/questions/74818/After-firmware-update-mbed-does-not-star/" target="_blank"&gt;https://os.mbed.com/questions/74818/After-firmware-update-mbed-does-not-star/&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Regards,&lt;BR /&gt;Gustavo&lt;/P&gt;</description>
      <pubDate>Fri, 03 Oct 2025 20:32:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2180076#M5714</guid>
      <dc:creator>gusarambula</dc:creator>
      <dc:date>2025-10-03T20:32:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso824-MAX Board doesn't connect</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2182867#M5718</link>
      <description>&lt;P&gt;I've updated the firmware, no difference.&lt;/P&gt;</description>
      <pubDate>Thu, 09 Oct 2025 08:43:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2182867#M5718</guid>
      <dc:creator>graynomad</dc:creator>
      <dc:date>2025-10-09T08:43:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso824-MAX Board doesn't connect</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2184110#M5719</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/154766"&gt;@graynomad&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please make sure that the JP1 jumper is open when using the onboard debugger.&lt;/P&gt;
&lt;P&gt;Have you tried using an external debugger? In that case, the JP1 jumper has to be closed.&lt;/P&gt;
&lt;P&gt;Please also try using a different SW tool, like&amp;nbsp;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING" target="_self"&gt;Secure Provisioning Tool&lt;/A&gt;&amp;nbsp;or &lt;A href="https://www.flashmagictool.com/" target="_self"&gt;Flash Magic&lt;/A&gt;&amp;nbsp;to establish communication with the debugger.&lt;/P&gt;</description>
      <pubDate>Fri, 10 Oct 2025 22:02:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2184110#M5719</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-10-10T22:02:13Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso824-MAX Board doesn't connect</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2184201#M5720</link>
      <description>&lt;P&gt;Jumper open. Flashmagic can't find anything either (see screen shot).&lt;/P&gt;</description>
      <pubDate>Sat, 11 Oct 2025 04:01:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2184201#M5720</guid>
      <dc:creator>graynomad</dc:creator>
      <dc:date>2025-10-11T04:01:35Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso824-MAX Board doesn't connect</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2185088#M5721</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/154766"&gt;@graynomad&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;Please try the following two scenarios:&lt;/P&gt;
&lt;P&gt;1. Try establishing connections with your board using the on-board debugger and Secure Provisioning Tool, with JP1 open.&lt;/P&gt;
&lt;P&gt;2. Try using an external debugger with any of the aforementioned tools while making sure to set&amp;nbsp;&lt;SPAN&gt;JP1 jumper closed.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 13 Oct 2025 19:20:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2185088#M5721</guid>
      <dc:creator>EdwinHz</dc:creator>
      <dc:date>2025-10-13T19:20:23Z</dc:date>
    </item>
    <item>
      <title>Re: LPCXpresso824-MAX Board doesn't connect</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2215106#M5748</link>
      <description>&lt;P&gt;Sorry, it's been a while. I actually gave up.&lt;/P&gt;&lt;P&gt;I've used a few of these Xpresso boards in the past with no issues, this one flashes the "USB disk" LED on power up and windows pops up an explorer window with two files.&amp;nbsp; Details,txt has this content&lt;/P&gt;&lt;P&gt;Version: 0221&lt;BR /&gt;Build: Mar 3 2015 15:06:30&lt;BR /&gt;Git Commit SHA: 23fa06dd2fcfee6aff77f6cd8175adecb11fd1fd&lt;BR /&gt;Git Local mods: Yes&lt;/P&gt;&lt;P&gt;So the board is not bricked, but the IDE just refuses to see it.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Nov 2025 20:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCXpresso824-MAX-Board-doesn-t-connect/m-p/2215106#M5748</guid>
      <dc:creator>graynomad</dc:creator>
      <dc:date>2025-11-19T20:05:02Z</dc:date>
    </item>
  </channel>
</rss>