<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic KMS - MCUXPRESSO PINS and Timer Tools in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/KMS-MCUXPRESSO-PINS-and-Timer-Tools/m-p/784832#M569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anybody tell me if the KMS environment for BLDC motor control can use the PINS and CLOCK tools of MCUXpresso?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, is there any app note / video that explains the process of using PINS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I open the PINS tool i get a number of errors in the Config Tools Overview as shown in the attachment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jul 2018 18:08:00 GMT</pubDate>
    <dc:creator>gianveglio</dc:creator>
    <dc:date>2018-07-25T18:08:00Z</dc:date>
    <item>
      <title>KMS - MCUXPRESSO PINS and Timer Tools</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/KMS-MCUXPRESSO-PINS-and-Timer-Tools/m-p/784832#M569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can anybody tell me if the KMS environment for BLDC motor control can use the PINS and CLOCK tools of MCUXpresso?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If so, is there any app note / video that explains the process of using PINS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I open the PINS tool i get a number of errors in the Config Tools Overview as shown in the attachment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jul 2018 18:08:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/KMS-MCUXPRESSO-PINS-and-Timer-Tools/m-p/784832#M569</guid>
      <dc:creator>gianveglio</dc:creator>
      <dc:date>2018-07-25T18:08:00Z</dc:date>
    </item>
    <item>
      <title>Re: KMS - MCUXPRESSO PINS and Timer Tools</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/KMS-MCUXPRESSO-PINS-and-Timer-Tools/m-p/784833#M570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="303164" data-username="gianveglio" href="https://community.nxp.com/people/gianveglio"&gt;gian veglio&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;- Which project you import into MCUXpresso IDE ？&lt;/P&gt;&lt;P&gt;&amp;nbsp;And show error message from "Problems" view by double click error flag.&lt;/P&gt;&lt;P&gt;- There is BLDC demo under SDK, you can open and configure pins :&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/66493i6ADB94DACD8785AE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;- About the usage of Pins configure tool , please take a look at &amp;lt;MCUXpresso_IDE_ConfigTools_User_Manual.pdf&amp;gt;&lt;/P&gt;&lt;P&gt;(I also attached it for you .)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 04:16:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/KMS-MCUXPRESSO-PINS-and-Timer-Tools/m-p/784833#M570</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2018-07-26T04:16:18Z</dc:date>
    </item>
  </channel>
</rss>