<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: LinkServer installation on Ubuntu via command line</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115112#M5683</link>
    <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;,&lt;BR /&gt;I have recently seen your blog post about &lt;STRONG&gt;devcontainers&lt;/STRONG&gt; and it's exactly what I wanted to set up in my team as well - although it's still on my TODO list &lt;LI-EMOJI id="lia_grinning-face-with-smiling-eyes" title=":grinning_face_with_smiling_eyes:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;However, I was wondering about something more official that would be on &lt;STRONG&gt;dockerhub&lt;/STRONG&gt; or some other registry with full documentation and official NXP branding. Since it's becoming more and more popular for some solutions I was just curious if that is something NXP considers.&lt;BR /&gt;&lt;BR /&gt;I'm fairly confident that what you proposed works, however it does not answer the main question (even though it provides a viable solution in a form of an alternative installation method which I like very much).&lt;BR /&gt;The question was whether there is some misuse in my command line or there is something wrong with the binary itself.&lt;BR /&gt;As a matter of fact, I recently found some such inconsistency in the &lt;STRONG&gt;LinkServer flash dump&lt;/STRONG&gt; command and I've been told it will be relayed up the chain to fix, so I believe it's possible and I would only want to make it clear in case anyone else stumbles upon the same issue.&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;I love your blogs, it's a great jobs you are doing out there, keep it up!&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 12 Jun 2025 07:22:21 GMT</pubDate>
    <dc:creator>mimlo</dc:creator>
    <dc:date>2025-06-12T07:22:21Z</dc:date>
    <item>
      <title>LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2114634#M5679</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;I'd like to ask a question regarding installation of LinkServer (assuming one already has a .bin file downloaded) in an automated way - no human intervention needed.&lt;BR /&gt;&lt;BR /&gt;I'm executing the following command:&lt;BR /&gt;&lt;STRONG&gt;./LinkServer_25.3.31.x86_64.deb.bin --accept&lt;/STRONG&gt;&lt;BR /&gt;, but I'm still prompted with license agreement window.&lt;BR /&gt;&lt;BR /&gt;From the --help it seems like it should be enough to make it accept the agreement. Below you will find output from &lt;STRONG&gt;./LinkServer_25.3.31.x86_64.deb.bin&amp;nbsp; --help&lt;/STRONG&gt; command:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Makeself version 2.4.0
 1) Getting help or info about ./LinkServer_25.3.31.x86_64.deb.bin :
  ./LinkServer_25.3.31.x86_64.deb.bin --help   Print this message
  ./LinkServer_25.3.31.x86_64.deb.bin --info   Print embedded info : title, default target directory, embedded script ...
  ./LinkServer_25.3.31.x86_64.deb.bin --lsm    Print embedded lsm entry (or no LSM)
  ./LinkServer_25.3.31.x86_64.deb.bin --list   Print the list of files in the archive
  ./LinkServer_25.3.31.x86_64.deb.bin --check  Checks integrity of the archive

 2) Running ./LinkServer_25.3.31.x86_64.deb.bin :
  ./LinkServer_25.3.31.x86_64.deb.bin [options] [--] [additional arguments to embedded script]
  with following options (in that order)
  --confirm             Ask before running embedded script
  --quiet               Do not print anything except error messages
  --accept              Accept the license
  --noexec              Do not run embedded script
  --keep                Do not erase target directory after running
                        the embedded script
  --noprogress          Do not show the progress during the decompression
  --nox11               Do not spawn an xterm
  --nochown             Do not give the extracted files to the current user
  --nodiskspace         Do not check for available disk space
  --target dir          Extract directly to a target directory (absolute or relative)
                        This directory may undergo recursive chown (see --nochown).
  --tar arg1 [arg2 ...] Access the contents of the archive through the tar command
  --                    Following arguments will be passed to the embedded script&lt;/LI-CODE&gt;&lt;P&gt;I'm wondering if I'm doing something wrong or the LinkServer CLI is faulty.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;While I'm at the topic of tools and automation, are you planning on adding a docker image for LinkServer tool or similar?&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Michael&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 17:11:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2114634#M5679</guid>
      <dc:creator>mimlo</dc:creator>
      <dc:date>2025-06-11T17:11:43Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2114660#M5680</link>
      <description>&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;you can see how I'm doing this (in my case in a Ubunto docker image):&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2025/02/18/remote-debugging-with-devcontainer-and-vs-code/" target="_blank"&gt;https://mcuoneclipse.com/2025/02/18/remote-debugging-with-devcontainer-and-vs-code/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The code and scripts are here:&lt;/P&gt;&lt;P&gt;&lt;A href="https://github.com/ErichStyger/MCUXpresso_LPC55S16_CI_CD" target="_blank"&gt;https://github.com/ErichStyger/MCUXpresso_LPC55S16_CI_CD&lt;/A&gt;&lt;/P&gt;&lt;P&gt;The file is here:&amp;nbsp;&lt;A href="https://github.com/ErichStyger/MCUXpresso_LPC55S16_CI_CD/blob/main/.docker/Dockerfile" target="_blank"&gt;https://github.com/ErichStyger/MCUXpresso_LPC55S16_CI_CD/blob/main/.docker/Dockerfile&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 17:53:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2114660#M5680</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2025-06-11T17:53:48Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2114663#M5681</link>
      <description>&lt;P&gt;On the topic of automation (say: CI/CD), I recommend to have a look at a series of articles on my blog, starting with&amp;nbsp;&lt;A href="https://github.com/ErichStyger/MCUXpresso_LPC55S16_CI_CD/blob/main/README.md" target="_blank"&gt;https://github.com/ErichStyger/MCUXpresso_LPC55S16_CI_CD/blob/main/README.md&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Or simply use:&amp;nbsp;&lt;A href="https://mcuoneclipse.com/category/ci-cd/" target="_blank"&gt;https://mcuoneclipse.com/category/ci-cd/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Wed, 11 Jun 2025 17:56:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2114663#M5681</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2025-06-11T17:56:37Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115112#M5683</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;,&lt;BR /&gt;I have recently seen your blog post about &lt;STRONG&gt;devcontainers&lt;/STRONG&gt; and it's exactly what I wanted to set up in my team as well - although it's still on my TODO list &lt;LI-EMOJI id="lia_grinning-face-with-smiling-eyes" title=":grinning_face_with_smiling_eyes:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;However, I was wondering about something more official that would be on &lt;STRONG&gt;dockerhub&lt;/STRONG&gt; or some other registry with full documentation and official NXP branding. Since it's becoming more and more popular for some solutions I was just curious if that is something NXP considers.&lt;BR /&gt;&lt;BR /&gt;I'm fairly confident that what you proposed works, however it does not answer the main question (even though it provides a viable solution in a form of an alternative installation method which I like very much).&lt;BR /&gt;The question was whether there is some misuse in my command line or there is something wrong with the binary itself.&lt;BR /&gt;As a matter of fact, I recently found some such inconsistency in the &lt;STRONG&gt;LinkServer flash dump&lt;/STRONG&gt; command and I've been told it will be relayed up the chain to fix, so I believe it's possible and I would only want to make it clear in case anyone else stumbles upon the same issue.&lt;BR /&gt;&lt;BR /&gt;&lt;EM&gt;&lt;STRONG&gt;I love your blogs, it's a great jobs you are doing out there, keep it up!&lt;/STRONG&gt;&lt;/EM&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 07:22:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115112#M5683</guid>
      <dc:creator>mimlo</dc:creator>
      <dc:date>2025-06-12T07:22:21Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115154#M5684</link>
      <description>&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;thank you very much for your kind words!&lt;/P&gt;&lt;P&gt;On the --accept option, I believe this is on the debian side (not an expert on debian installation scripts), and possibly the LinkServer installation sub-part does not honor that somehow. I have pinged a contact I have so he might chime in.&lt;/P&gt;&lt;P&gt;About the LinkServer flash dump: if you don't mind, can you share it here or the link to that discussion?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 07:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115154#M5684</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2025-06-12T07:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115263#M5685</link>
      <description>&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;can you try this:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;sudo&lt;/STRONG&gt; ./LinkServer_25.3.31.x86_64.deb.bin &lt;STRONG&gt;acceptLicense skipIdeSelect&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Erich&lt;/STRONG&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 09:14:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115263#M5685</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2025-06-12T09:14:18Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115299#M5686</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/17173"&gt;@ErichStyger&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;It works like a charm thank you.&lt;BR /&gt;&lt;BR /&gt;Looking at this command you provided and at the &lt;STRONG&gt;--help&lt;/STRONG&gt; print, it looks like there is something missing (for example the &lt;STRONG&gt;skipIdeSelect&lt;/STRONG&gt; option).&lt;BR /&gt;Unless of course I'm missing something and it's documented somewhere else.&lt;BR /&gt;&lt;BR /&gt;Thank you once more.&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Michael&lt;/P&gt;</description>
      <pubDate>Thu, 12 Jun 2025 09:49:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2115299#M5686</guid>
      <dc:creator>mimlo</dc:creator>
      <dc:date>2025-06-12T09:49:25Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2150215#M5698</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/220472"&gt;@mimlo&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;&lt;P&gt;FYI, I wrote an article about it here on my blog:&amp;nbsp;&lt;A href="https://mcuoneclipse.com/2025/08/11/streamlining-linkserver-installation-for-ci-cd/" target="_blank"&gt;https://mcuoneclipse.com/2025/08/11/streamlining-linkserver-installation-for-ci-cd/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Mon, 11 Aug 2025 16:15:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2150215#M5698</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2025-08-11T16:15:51Z</dc:date>
    </item>
    <item>
      <title>Re: LinkServer installation on Ubuntu via command line</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2150220#M5699</link>
      <description>Impeccable timing &lt;LI-EMOJI id="lia_winking-face" title=":winking_face:"&gt;&lt;/LI-EMOJI&gt;&lt;BR /&gt;I'll read it tomorrow and comment there.&lt;BR /&gt;&lt;BR /&gt;I see we're after a similar thing here, so combined effort might actually bring great benefits to the community.&lt;BR /&gt;Thanks for that!</description>
      <pubDate>Mon, 11 Aug 2025 16:24:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LinkServer-installation-on-Ubuntu-via-command-line/m-p/2150220#M5699</guid>
      <dc:creator>mimlo</dc:creator>
      <dc:date>2025-08-11T16:24:29Z</dc:date>
    </item>
  </channel>
</rss>