<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MC9S12XDP512 Secure Mode Issue in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/MC9S12XDP512-Secure-Mode-Issue/m-p/2037596#M5573</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use MC9S12XDP512 microcontroller in secure mode. The application code runs without any issues in unsecure mode, but when secure mode is enabled, I encounter a problem.&lt;/P&gt;&lt;P&gt;Based on my observations, the issue occurs when accessing variables in the SRAM region. These variables are located in the 0x20_0000–0x3F_FFFF (CS1) area. When secure mode is active, the program unexpectedly stops running.&lt;/P&gt;&lt;P&gt;Is there any special configuration required for SRAM access in secure mode?&lt;BR /&gt;Do you have any suggestions?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
    <pubDate>Tue, 04 Feb 2025 08:52:05 GMT</pubDate>
    <dc:creator>okan_saglam</dc:creator>
    <dc:date>2025-02-04T08:52:05Z</dc:date>
    <item>
      <title>MC9S12XDP512 Secure Mode Issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MC9S12XDP512-Secure-Mode-Issue/m-p/2037596#M5573</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I am trying to use MC9S12XDP512 microcontroller in secure mode. The application code runs without any issues in unsecure mode, but when secure mode is enabled, I encounter a problem.&lt;/P&gt;&lt;P&gt;Based on my observations, the issue occurs when accessing variables in the SRAM region. These variables are located in the 0x20_0000–0x3F_FFFF (CS1) area. When secure mode is active, the program unexpectedly stops running.&lt;/P&gt;&lt;P&gt;Is there any special configuration required for SRAM access in secure mode?&lt;BR /&gt;Do you have any suggestions?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 08:52:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MC9S12XDP512-Secure-Mode-Issue/m-p/2037596#M5573</guid>
      <dc:creator>okan_saglam</dc:creator>
      <dc:date>2025-02-04T08:52:05Z</dc:date>
    </item>
    <item>
      <title>Re: MC9S12XDP512 Secure Mode Issue</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MC9S12XDP512-Secure-Mode-Issue/m-p/2037663#M5574</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;It does not smell me like security issue but something between debug and normal mode together with writing mode register twice (it is write once only in the normal mode).&lt;/P&gt;
&lt;P&gt;BTW, do not you mix security and protection?&lt;/P&gt;
&lt;P&gt;&lt;A href="https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-S12XE-External-BUS-design-Addendum-To-AN2708/ta-p/1118041" target="_blank"&gt;https://community.nxp.com/t5/S12-MagniV-Microcontrollers/S12XD-S12XE-External-BUS-design-Addendum-To-AN2708/ta-p/1118041&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please read &lt;SPAN&gt;AN-ExBUS-AddendumToAN2708-v.0.2.zip&lt;/SPAN&gt; chapter 5.2 SW Solution from the page and compare design.&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;I believe you will find the source of the issue because I do not see into your HW and SW design.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;/P&gt;
&lt;P&gt;Ladislav&lt;/P&gt;</description>
      <pubDate>Tue, 04 Feb 2025 11:13:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MC9S12XDP512-Secure-Mode-Issue/m-p/2037663#M5574</guid>
      <dc:creator>lama</dc:creator>
      <dc:date>2025-02-04T11:13:08Z</dc:date>
    </item>
  </channel>
</rss>