<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Problems with MCU Link and IMX RT1176 in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2008601#M5540</link>
    <description>&lt;P&gt;Hello, thanks for your information, could you test a simple blinking led to test if the flash could be done.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
    <pubDate>Fri, 06 Dec 2024 00:18:54 GMT</pubDate>
    <dc:creator>Pavel_Hernandez</dc:creator>
    <dc:date>2024-12-06T00:18:54Z</dc:date>
    <item>
      <title>Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2006889#M5529</link>
      <description>&lt;P&gt;I've been using JLink to debug a custom 1176 board with no problems.&lt;BR /&gt;Now I'm trying the same with MCU-Link and LinkServer and I'm facing problems related to flash driver configuration:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;$ /usr/local/LinkServer/LinkServer flash MIMXRT1176xxxxx:MIMXRT1170-EVK verify build.elf
INFO: Exact match for MIMXRT1176xxxxx:MIMXRT1170-EVK found
INFO: Selected device MIMXRT1176xxxxx:MIMXRT1170-EVK
INFO: Getting available probes
INFO: Selected probe #1 RCBNN1BAEWWXT (MCU-LINK (r0FF) CMSIS-DAP V3.148)
INFO: MCU-Link firmware update `check`: local firmware [3.148] is the same as the version running on the selected probe ([RCBNN1BAEWWXT] [MCU-LINK (r0FF) CMSIS-DAP V3.148])
Firmware update `check`: not required - the update can be performed using `forced` mode
Ns: MCUXpresso IDE RedlinkMulti Driver v24.9 (Sep 19 2024 19:39:44 - crt_emu_cm_redlink build 802)
Pc: (  0) Reading remote configuration
Wc(03). No cache support.
Nc: Found generic directory XML file in /tmp/tmp99jx1dxz/crt_directory.xml
Pc: (  5) Remote configuration complete
Nc: Reconnected to existing LinkServer process.
Wc: ============= SCRIPT: RT1170_connect_M7_wake_M4.scp =============
Wc: RT1170 Connect M7 and Wake M4 Script
Wc: DpID = 6BA02477
Wc: APID = 0x84770001
Wc: Setting M4 spin code
Wc: Setting M4 clock
Wc: Resetting M4 core
Wc: View cores on the DAP AP
Wc: DpID = 6BA02477
Wc: TAP 0: 6BA02477 Core 0: M7  APID: 84770001 ROM Table: E00FD003*
Wc: TAP 0: 6BA02477 Core 1: M4  APID: 24770011 ROM Table: E00FF003
Wc: ============= END SCRIPT ========================================
Nc: Probe Firmware: MCU-LINK (r0FF) CMSIS-DAP V3.148 (NXP Semiconductors)
Nc: Serial Number:  RCBNN1BAEWWXT
Nc: VID:PID:  1FC9:0143
Nc: USB Path: 0001:0012:00
Nc: Using memory from core 0 after searching for a good core
Pc: ( 30) Emulator Connected
Pc: ( 40) Debug Halt
Pc: ( 50) CPU ID
Nc: debug interface type      = CoreSight DP (DAP DP ID 6BA02477) over SWD TAP 0
Nc: processor type            = Cortex-M7 (CPU ID 00000C27) on DAP AP 0
Nc: number of h/w breakpoints = 8
Nc: number of flash patches   = 0
Nc: number of h/w watchpoints = 4
Nc: Probe(0): Connected&amp;amp;Reset. DpID: 6BA02477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;
Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Ns: Content of CoreSight Debug ROM(s):
Nc: RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)
Nc: ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)
Nc: ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)
Nc: ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)
Nc: ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)
Nc: ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)
Nc: ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)
Nc: ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core
Nc: ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT
Nc: ROM 1 E0043000: CID B105900D PID 04001BB908 CSt CSTF type 0x12 Trace Link - Trace funnel/router
Nc: NXP: MIMXRT1176xxxxx
Nc: DAP stride is 1024 bytes (256 words)
Nc: Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1170_SFDP_QSPI.cfx
Nc: Image 'iMXRT1170_SFDP_FlexSPI1_A_QSPI Sep 19 2024 18:31:37'
Nc: Opening flash driver MIMXRT1170_SFDP_QSPI.cfx
Nc: Sending VECTRESET to run flash driver
Ec: Flash Driver V.2 dynamic startup failed - driver Init provided no flash parameters

Nc: Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.
Ec: op Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPIJ driver rc 20107 (0x4E8B)

Ec: vendor chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.
Wc: failed to initialize flash driver MIMXRT1170_SFDP_QSPI.cfx
Pc: ( 65) Chip Setup Complete
Pc: (100) Target Operation Failed
CRITICAL: Critical error
ERRMSG: Exception: Flash operation exited with code 1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Dec 2024 09:54:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2006889#M5529</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-04T09:54:57Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007620#M5531</link>
      <description>&lt;P&gt;Hello, my name is Pavel, and I will be supporting your case, I need more information about the hardware, did you use the same interface as the J-Link?&amp;nbsp;&lt;/P&gt;
&lt;PRE class="lia-code-sample  language-markup"&gt;&lt;CODE&gt;Nc: Image 'iMXRT1170_SFDP_FlexSPI1_A_QSPI Sep 19 2024 18:31:37'
&lt;/CODE&gt;&lt;/PRE&gt;
&lt;P&gt;Do you have the QSPI on a FlexSPI &lt;STRONG&gt;1 &lt;/STRONG&gt;port?&lt;/P&gt;
&lt;P&gt;could you try to use blhost?&lt;/P&gt;
&lt;P&gt;blhost&amp;nbsp; -p COMxx get-property 1&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 00:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007620#M5531</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-05T00:39:16Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007883#M5533</link>
      <description>&lt;P&gt;&amp;gt; Hello, my name is Pavel, and I will be supporting your case, I need more information about the &amp;gt; hardware, did you use the same interface as the J-Link?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, SWD.&lt;/P&gt;&lt;P&gt;&amp;gt; Do you have the QSPI on a FlexSPI&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;STRONG&gt;1&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/STRONG&gt;port?&lt;/P&gt;&lt;P&gt;Yes&lt;/P&gt;&lt;P&gt;&amp;gt; could you try to use blhost?&lt;/P&gt;&lt;P&gt;&amp;gt; blhost&amp;nbsp; -p COMxx get-property 1&amp;nbsp;&lt;/P&gt;&lt;P&gt;What serial port should I connect to? the one opened by MCU-Link (ttyACM0)?&lt;BR /&gt;I'm getting "Error: Initial ping failure: No response received for ping command."&lt;BR /&gt;&lt;BR /&gt;My board does not open any tty ports over USB (other than the two handling shell/console in our application but there are not relevant, obviously) and it's not connected via serial.&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 07:34:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007883#M5533</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-05T07:34:36Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007924#M5534</link>
      <description>&lt;P&gt;Ok, I figured I need to enable recovery mode to force-load rom bootloader. I was able to connect with blhost (using usb connection) and got:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;$ sudo ./blhost -u /dev/hidraw5 get-property 1
Inject command 'get-property'
Response status = 0 (0x0) Success.
Response word 1 = 1258487809 (0x4b030001)
Current Version = K3.0.1&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 05 Dec 2024 08:11:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007924#M5534</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-05T08:11:42Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007932#M5535</link>
      <description>&lt;P&gt;Also:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;$ sudo ./blhost -u /dev/hidraw5 get-property 18
Inject command 'get-property'
Response status = 0 (0x0) Success.
Response word 1 = 2190645060 (0x82929744)
Response word 2 = 421359630 (0x191d700e)
Unique Device ID = 44 97 92 82 0E 70 1D 19&lt;/LI-CODE&gt;</description>
      <pubDate>Thu, 05 Dec 2024 08:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2007932#M5535</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-05T08:18:03Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2008601#M5540</link>
      <description>&lt;P&gt;Hello, thanks for your information, could you test a simple blinking led to test if the flash could be done.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 06 Dec 2024 00:18:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2008601#M5540</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-06T00:18:54Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2008892#M5541</link>
      <description>&lt;P&gt;I neither can verify nor flash any image.&lt;/P&gt;</description>
      <pubDate>Fri, 06 Dec 2024 07:13:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2008892#M5541</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-06T07:13:54Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2009388#M5543</link>
      <description>&lt;P&gt;Hello, what kind of distro of ubuntu you have?&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1733520221038.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/314623iA0E0C5DEBFE99468/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1733520221038.png" alt="Pavel_Hernandez_0-1733520221038.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Maybe will could try as same that the IDE support.&lt;/P&gt;
&lt;UL class="boxes"&gt;
&lt;LI&gt;Ubuntu 20.04.2 LTS / 22.04 LTS.&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;Could you try to flash using blhost?&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 06 Dec 2024 21:33:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2009388#M5543</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-06T21:33:43Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2009854#M5545</link>
      <description>&lt;P&gt;My&amp;nbsp;Ubuntu is 22.04.5 LTS&lt;/P&gt;</description>
      <pubDate>Mon, 09 Dec 2024 08:36:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2009854#M5545</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-09T08:36:37Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2015332#M5552</link>
      <description>&lt;P&gt;Is there anything else that could be done? Or MCU Link just does not support iMX RT1176?&lt;/P&gt;</description>
      <pubDate>Tue, 17 Dec 2024 13:16:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2015332#M5552</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-17T13:16:11Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2015642#M5554</link>
      <description>&lt;P&gt;Hello, I'm afraid that the configuration on the MCU-Link is not the problem this has support for your EVK. I reviewed again your LOG and seems there is a problem with the driver SFDP QSPI.&lt;/P&gt;
&lt;P&gt;Would you let me know more about your board...&lt;/P&gt;
&lt;P&gt;What kind of memory QSPI do you have?&lt;BR /&gt;What kind of version of Jlink driver have?&lt;BR /&gt;Is the Jlink version "plus", "edu" or "normal"?&lt;BR /&gt;What was the difference when you change the debugger? did you modify the code or the board?&lt;BR /&gt;Could you install SPT to confirm there is a communication with the QSPI?&lt;BR /&gt;&lt;A href="https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-secure-provisioning-tool:MCUXPRESSO-SECURE-PROVISIONING" target="_blank"&gt;MCUXpresso Secure Provisioning Tool | NXP Semiconductors&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;In some cases, doing a mass erase the board come back to normally check the&amp;nbsp;2.2 SPT Mass Erase.&lt;BR /&gt;&lt;A href="https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs-Knowledge/RT-board-recovery-for-debugger-connect-issues/ta-p/1635260" target="_blank"&gt;RT board recovery for debugger connect issues - NXP Community&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 01:22:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2015642#M5554</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-18T01:22:22Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016014#M5555</link>
      <description>&lt;P&gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;What kind of memory QSPI do you have?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;NOR Flash W25Q128FWPIG&lt;/SPAN&gt;&lt;SPAN class=""&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;&amp;gt; What kind of version of Jlink driver have?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;gt; Is the Jlink version "plus", "edu" or "normal"?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;&lt;SPAN&gt;The problem is about MCU Link, standard version.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;What was the difference when you change the debugger? did you modify the code or the board?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;No, it's the same configuration&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;nbsp;&lt;SPAN&gt;Could you install SPT to confirm there is a communication with the QSPI?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I have installed it and run a flash test there, output is:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;### Check presence of FlashLoader ###
### Select FlexSPI NOR memory instance #1 using option on address 0x2000 ###
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- fill-memory 0x2000 4 0xCF900001 word
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "fill-memory",
   "response": [],
   "status": {
      "description": "0 (0x0) Success.",
      "value": 0
   }
}
blhost succeeded
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- configure-memory 9 0x2000
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "configure-memory",
   "response": [],
   "status": {
      "description": "0 (0x0) Success.",
      "value": 0
   }
}
blhost succeeded
### Configure FlexSPI NOR memory using options on address 0x2000 ###
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- fill-memory 0x2000 4 0xC0000007 word
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "fill-memory",
   "response": [],
   "status": {
      "description": "0 (0x0) Success.",
      "value": 0
   }
}
blhost succeeded
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- configure-memory 9 0x2000
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "configure-memory",
   "response": [],
   "status": {
      "description": "20107 (0x4e8b) FlexSPINOR: SFDP Not Found.",
      "value": 20107
   }
}
blhost failed&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jakobczyk_woj_0-1734522291592.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/316468iAADE55079E26BE44/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jakobczyk_woj_0-1734522291592.png" alt="jakobczyk_woj_0-1734522291592.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 11:46:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016014#M5555</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-18T11:46:12Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016019#M5556</link>
      <description>&lt;P&gt;Mass erase in SPT is not possible because it can't pass memory configuration with the same output as above.&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 11:53:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016019#M5556</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-18T11:53:03Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016585#M5557</link>
      <description>&lt;P&gt;Hello, thanks for the information, I recommend open the example, modify the LUT for your memory and check the Quad mode to activate this register.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Pavel_Hernandez_0-1734562221418.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/316571iD5E95E27A1ADACA1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Pavel_Hernandez_0-1734562221418.png" alt="Pavel_Hernandez_0-1734562221418.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Wed, 18 Dec 2024 22:58:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016585#M5557</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-18T22:58:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016986#M5558</link>
      <description>&lt;P&gt;I don't see this example in SPT.&lt;BR /&gt;Also not sure what you mean regarding LUT and Quad mode.&lt;BR /&gt;I have tried with supplied binary&amp;nbsp;bootable_images/evkmimxrt1170_iled_blinky_cm7_QSPI_FLASH.bin but with the same result:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;### Parse input arguments ###
### Check presence of FlashLoader ###
### Select FlexSPI NOR memory instance #1 using option on address 0x2000 ###
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- fill-memory 0x2000 4 0xCF900001 word
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "fill-memory",
   "response": [],
   "status": {
      "description": "0 (0x0) Success.",
      "value": 0
   }
}
blhost succeeded
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- configure-memory 9 0x2000
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "configure-memory",
   "response": [],
   "status": {
      "description": "0 (0x0) Success.",
      "value": 0
   }
}
blhost succeeded
### Configure FlexSPI NOR memory using options on address 0x2000 ###
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- fill-memory 0x2000 4 0xC0000007 word
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "fill-memory",
   "response": [],
   "status": {
      "description": "0 (0x0) Success.",
      "value": 0
   }
}
blhost succeeded
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk /opt/nxp/MCUX_Provi_v10/bin
/opt/nxp/MCUX_Provi_v10/bin/_internal/tools/spsdk/blhost -t 5000 -u 0x15A2,0x0073 -j -- configure-memory 9 0x2000
/opt/nxp/MCUX_Provi_v10/bin
{
   "command": "configure-memory",
   "response": [],
   "status": {
      "description": "20107 (0x4e8b) FlexSPINOR: SFDP Not Found.",
      "value": 20107
   }
}
blhost failed&lt;/LI-CODE&gt;</description>
      <pubDate>Thu, 19 Dec 2024 07:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016986#M5558</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-19T07:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016992#M5559</link>
      <description>I have tried all the options in "Quad mode setting" in "Boot Memory Configuration" but none helped.</description>
      <pubDate>Thu, 19 Dec 2024 07:53:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2016992#M5559</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2024-12-19T07:53:58Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2018104#M5562</link>
      <description>&lt;P&gt;Hello, I recommend use a logic analyzer to see if the driver is working well, this seems could be a hardware issue, let me know about your test.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Fri, 20 Dec 2024 23:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2018104#M5562</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2024-12-20T23:31:56Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2023066#M5565</link>
      <description>&lt;P&gt;&amp;gt; Hello, I recommend use a logic analyzer to see if the driver is working well, this seems could be a hardware issue, let me know about your test.&lt;/P&gt;&lt;P&gt;Could you please provide more information what should check with a logic analyzer?&lt;/P&gt;</description>
      <pubDate>Tue, 07 Jan 2025 07:29:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2023066#M5565</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2025-01-07T07:29:21Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2025173#M5568</link>
      <description>&lt;P&gt;Hello, if the communication between the MCU and the QSPI is correct on the flexspi.&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Pavel&lt;/P&gt;</description>
      <pubDate>Thu, 09 Jan 2025 22:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2025173#M5568</guid>
      <dc:creator>Pavel_Hernandez</dc:creator>
      <dc:date>2025-01-09T22:21:00Z</dc:date>
    </item>
    <item>
      <title>Re: Problems with MCU Link and IMX RT1176</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2026678#M5571</link>
      <description>&lt;P&gt;The communication is correct. The board can be flashed with another debug probe (as I mentioned) and the flashed firmware is working fine.&lt;/P&gt;</description>
      <pubDate>Mon, 13 Jan 2025 10:50:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Problems-with-MCU-Link-and-IMX-RT1176/m-p/2026678#M5571</guid>
      <dc:creator>jakobczyk_woj</dc:creator>
      <dc:date>2025-01-13T10:50:29Z</dc:date>
    </item>
  </channel>
</rss>