<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCUXpresso LPC824 initialization order when using PINT in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-LPC824-initialization-order-when-using-PINT/m-p/1731482#M5118</link>
    <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223652"&gt;@dropTarget&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Which SDK and MCUXpresso IDE version are you using? Could you please try it with the newest versions (v2.14.0 and v11.8.0 respectively) for the LPC824?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;The example &lt;EM&gt;pint_pin_interrupt&lt;/EM&gt;&amp;nbsp;uses the ConfigTools' functions as PINT_Init() and PINT_PinInterruptConfig() after BOARD_InitBootPins(). Could you please take a look at?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
    <pubDate>Thu, 28 Sep 2023 19:52:19 GMT</pubDate>
    <dc:creator>RaRo</dc:creator>
    <dc:date>2023-09-28T19:52:19Z</dc:date>
    <item>
      <title>MCUXpresso LPC824 initialization order when using PINT</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-LPC824-initialization-order-when-using-PINT/m-p/1730805#M5116</link>
      <description>&lt;P&gt;LPC824/MCUXpresso:&lt;/P&gt;&lt;P&gt;After configuring an input pin to trigger an interrupt using the PINT config tool, GPIO outputs don't work properly.&amp;nbsp; I have found that if the order of initialization in main() is modified such that BOARD_InitBootPins() is called after BOARD_InitBootPeripherals(), the problem is resolved.&lt;/P&gt;&lt;P&gt;Apparently, PINT configuration is altering the GPIO pins configuration setup in BOARD_InitBootPins() such that outputs no longer function properly.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 27 Sep 2023 22:47:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-LPC824-initialization-order-when-using-PINT/m-p/1730805#M5116</guid>
      <dc:creator>dropTarget</dc:creator>
      <dc:date>2023-09-27T22:47:18Z</dc:date>
    </item>
    <item>
      <title>Re: MCUXpresso LPC824 initialization order when using PINT</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-LPC824-initialization-order-when-using-PINT/m-p/1731482#M5118</link>
      <description>&lt;P class="lia-align-justify"&gt;Hello &lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/223652"&gt;@dropTarget&lt;/a&gt;,&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Which SDK and MCUXpresso IDE version are you using? Could you please try it with the newest versions (v2.14.0 and v11.8.0 respectively) for the LPC824?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;The example &lt;EM&gt;pint_pin_interrupt&lt;/EM&gt;&amp;nbsp;uses the ConfigTools' functions as PINT_Init() and PINT_PinInterruptConfig() after BOARD_InitBootPins(). Could you please take a look at?&lt;/P&gt;
&lt;P class="lia-align-justify"&gt;Best regards, Raul.&lt;/P&gt;</description>
      <pubDate>Thu, 28 Sep 2023 19:52:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUXpresso-LPC824-initialization-order-when-using-PINT/m-p/1731482#M5118</guid>
      <dc:creator>RaRo</dc:creator>
      <dc:date>2023-09-28T19:52:19Z</dc:date>
    </item>
  </channel>
</rss>