<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic No reference for LPC55s16 in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608231#M4877</link>
    <description>&lt;P&gt;Why no one worked with LPC55s16 board&amp;nbsp; &amp;nbsp;no refreence could be found on the internet or youtube ,I just want to interface LPC55s16 board with MLX90640 Thermal camera and need complete code for it. Inbuilt sdk examples haven't worked out&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Thu, 02 Mar 2023 08:49:51 GMT</pubDate>
    <dc:creator>Vijay222</dc:creator>
    <dc:date>2023-03-02T08:49:51Z</dc:date>
    <item>
      <title>No reference for LPC55s16</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608231#M4877</link>
      <description>&lt;P&gt;Why no one worked with LPC55s16 board&amp;nbsp; &amp;nbsp;no refreence could be found on the internet or youtube ,I just want to interface LPC55s16 board with MLX90640 Thermal camera and need complete code for it. Inbuilt sdk examples haven't worked out&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Mar 2023 08:49:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608231#M4877</guid>
      <dc:creator>Vijay222</dc:creator>
      <dc:date>2023-03-02T08:49:51Z</dc:date>
    </item>
    <item>
      <title>Re: No reference for LPC55s16</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608264#M4878</link>
      <description>&lt;P&gt;Not sure how you searched the internet, but I'm using the LPC55S16, for example&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2021/12/30/lorawan-with-nxp-lpc55s16-and-arm-cortex-m33/" target="_blank"&gt;https://mcuoneclipse.com/2021/12/30/lorawan-with-nxp-lpc55s16-and-arm-cortex-m33/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://mcuoneclipse.com/2021/05/15/using-fatfs-and-minini-with-the-nxp-lpc55s16-evk/" target="_blank"&gt;https://mcuoneclipse.com/2021/05/15/using-fatfs-and-minini-with-the-nxp-lpc55s16-evk/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;But I have not used it with the MLX90640, but that sensor has an I2C interface and should be straight forward to use. If you are looking for the I2C part, the NXP SDK has drivers/examples, so does the two above project include I2C in the McuLib.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 02 Mar 2023 09:31:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608264#M4878</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-03-02T09:31:46Z</dc:date>
    </item>
    <item>
      <title>Re: No reference for LPC55s16</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608911#M4881</link>
      <description>&lt;P&gt;Thanks for idea ,The thing is i just wana to build an poultry robot using LPC55s16 board. Since iam new to the board i don't know hot to interface LPC55s16 board With Mlx90640 and&amp;nbsp; motors for the base of the robot connected with tyre. So would you&amp;nbsp; able to help me out i just tried to find&amp;nbsp; out simple sensor interface with the board but there was no basic full explanation with the code for the board as like as Arduino so kindly help me out.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 05:45:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608911#M4881</guid>
      <dc:creator>Vijay222</dc:creator>
      <dc:date>2023-03-03T05:45:35Z</dc:date>
    </item>
    <item>
      <title>Re: No reference for LPC55s16</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608960#M4882</link>
      <description>&lt;P&gt;I recommend that you check out the examples of the NXP MCUXpresso SDK for it.&lt;/P&gt;</description>
      <pubDate>Fri, 03 Mar 2023 06:44:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/No-reference-for-LPC55s16/m-p/1608960#M4882</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2023-03-03T06:44:15Z</dc:date>
    </item>
  </channel>
</rss>