<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: Debugging issue with LPC11C24 and MCUXpresso</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-issue-with-LPC11C24-and-MCUXpresso/m-p/1587486#M4839</link>
    <description>&lt;P&gt;So as said above, the cause for this strange behavior was MCU resetting. After searching in the code I've found that watchdog resets the MCU if I stop on a breakpoint. Unfortunately&amp;nbsp;the only sign of a reset was jumping to an incorrect address. After changing from LPC-Link 2 to Segger J-link&amp;nbsp;I get a message that my MCU is reset, and only after that I discovered the watchdog issue.&lt;/P&gt;</description>
    <pubDate>Wed, 25 Jan 2023 07:23:12 GMT</pubDate>
    <dc:creator>ruslan1</dc:creator>
    <dc:date>2023-01-25T07:23:12Z</dc:date>
    <item>
      <title>Debugging issue with LPC11C24 and MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-issue-with-LPC11C24-and-MCUXpresso/m-p/1583927#M4832</link>
      <description>&lt;P&gt;I have an application that should run on out board. I have some strange issue that I can't debug the application. I use LPC-LInk2 that connected to the board, the application compiled in Debug mode. I can set a breakpoint and IDE stops on it without problem. But when I press F6 to step over it just jumps to some wrong address&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Untitled.png" style="width: 530px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/206053i105AD5279F3D7393/image-size/large?v=v2&amp;amp;px=999" role="button" title="Untitled.png" alt="Untitled.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;and so it fails with message:&lt;/P&gt;&lt;LI-CODE lang="markup"&gt;Failed to execute MI command:
-exec-next 1
Error message from debugger back end:
Cannot find bounds of current function&lt;/LI-CODE&gt;&lt;P&gt;&amp;nbsp;and I can't continue to debug the application. If I put a breakpoint on the next line it stops but pressing F6 again fails.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've checked the forum but cant' find any solution for that.&lt;/P&gt;</description>
      <pubDate>Tue, 17 Jan 2023 10:58:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-issue-with-LPC11C24-and-MCUXpresso/m-p/1583927#M4832</guid>
      <dc:creator>ruslan1</dc:creator>
      <dc:date>2023-01-17T10:58:11Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging issue with LPC11C24 and MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-issue-with-LPC11C24-and-MCUXpresso/m-p/1584923#M4835</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Thank you so much for your interest in our products and for using our community.&lt;/P&gt;
&lt;P&gt;Your micro is resetting, you must have moved something and it is difficult to deduce the cause. I recommend you try again an example of those that are available to see if the same thing continues to happen.&lt;/P&gt;
&lt;P&gt;Hope it helps you.&lt;/P&gt;
&lt;P&gt;Have a nice day!&lt;/P&gt;</description>
      <pubDate>Wed, 18 Jan 2023 19:02:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-issue-with-LPC11C24-and-MCUXpresso/m-p/1584923#M4835</guid>
      <dc:creator>_Leo_</dc:creator>
      <dc:date>2023-01-18T19:02:00Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging issue with LPC11C24 and MCUXpresso</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-issue-with-LPC11C24-and-MCUXpresso/m-p/1587486#M4839</link>
      <description>&lt;P&gt;So as said above, the cause for this strange behavior was MCU resetting. After searching in the code I've found that watchdog resets the MCU if I stop on a breakpoint. Unfortunately&amp;nbsp;the only sign of a reset was jumping to an incorrect address. After changing from LPC-Link 2 to Segger J-link&amp;nbsp;I get a message that my MCU is reset, and only after that I discovered the watchdog issue.&lt;/P&gt;</description>
      <pubDate>Wed, 25 Jan 2023 07:23:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-issue-with-LPC11C24-and-MCUXpresso/m-p/1587486#M4839</guid>
      <dc:creator>ruslan1</dc:creator>
      <dc:date>2023-01-25T07:23:12Z</dc:date>
    </item>
  </channel>
</rss>