<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debugging Bootloader and Application in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1563632#M4787</link>
    <description>&lt;P&gt;Great, thank you for the help. I'll see if switching up the debug probe helps with the issue.&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Fri, 02 Dec 2022 16:50:58 GMT</pubDate>
    <dc:creator>rnicolls</dc:creator>
    <dc:date>2022-12-02T16:50:58Z</dc:date>
    <item>
      <title>Debugging Bootloader and Application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1562424#M4783</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm running a bootloader in a debug session and jumping to an application. I'd like to load symbols for the application so that I can step through the application's code. Is there a way that I can do this?&lt;/P&gt;&lt;P&gt;The application and the bootloader are two separate projects.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm using the LinkServer debugger&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 01:08:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1562424#M4783</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2022-12-01T01:08:41Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Bootloader and Application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1562528#M4784</link>
      <description>&lt;P&gt;See an article I wrote here: &lt;A href="https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/" target="_blank"&gt;https://mcuoneclipse.com/2020/11/03/debugging-bootloader-and-application-with-one-debug-session/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Same principle works with LinkServer connection.&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;</description>
      <pubDate>Thu, 01 Dec 2022 04:46:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1562528#M4784</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-12-01T04:46:23Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Bootloader and Application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1563204#M4785</link>
      <description>&lt;P&gt;Hi Erich,&lt;/P&gt;&lt;P&gt;Thank you for the article, it was helpful. I have the bootloader running on the target and was able to connect with the application's debug configuration and see the bootloader code. It worked well a couple of times but now I'm consistently getting the attached error. Is this something you've experienced before?&lt;/P&gt;</description>
      <pubDate>Fri, 02 Dec 2022 05:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1563204#M4785</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2022-12-02T05:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Bootloader and Application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1563414#M4786</link>
      <description>&lt;P&gt;Yes, I have seen these in other contexts. To my understanding, it indicates a problem between the debug probe and the target. It could be the cable or some noise on the connection line.&lt;/P&gt;&lt;P&gt;What helped on my case was using a different debug probe, e.g. J-Link or P&amp;amp;E.&lt;/P&gt;</description>
      <pubDate>Fri, 02 Dec 2022 09:53:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1563414#M4786</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2022-12-02T09:53:07Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging Bootloader and Application</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1563632#M4787</link>
      <description>&lt;P&gt;Great, thank you for the help. I'll see if switching up the debug probe helps with the issue.&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 02 Dec 2022 16:50:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-Bootloader-and-Application/m-p/1563632#M4787</guid>
      <dc:creator>rnicolls</dc:creator>
      <dc:date>2022-12-02T16:50:58Z</dc:date>
    </item>
  </channel>
</rss>