<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error when flashing to MIMXRT1050-EVKB - &amp;quot;Wire ACK Wait in DAP access&amp;quot; in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1313544#M4259</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Maybe there is error code in flash which can cause download fail. Please try to use NXP_MCUBootUtility tool to erase flash. Before connect to the tool, set the SW7 to serial download mode first.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/JayHeng/NXP-MCUBootUtility" target="_blank"&gt;https://github.com/JayHeng/NXP-MCUBootUtility&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
    <pubDate>Tue, 27 Jul 2021 04:10:50 GMT</pubDate>
    <dc:creator>jingpan</dc:creator>
    <dc:date>2021-07-27T04:10:50Z</dc:date>
    <item>
      <title>Error when flashing to MIMXRT1050-EVKB - "Wire ACK Wait in DAP access"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1308627#M4235</link>
      <description>&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm getting a "Wire ACK Wait in DAP access" error when trying to flash to my MIMXRT1050-EVKB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;Ns: MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 17:55:57 - crt_emu_cm_redlink build 18)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Pc: ( 0) Reading remote configuration&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc(03). No cache support.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Found chip XML file in ./mimxrt1050-evk-common/cmake/MIMXRT1052xxxxB.xml&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Pc: ( 5) Remote configuration complete&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Restarted LinkServer process (PID 499706).&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: ============= SCRIPT: RT1050_connect.scp =============&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: RT1050 Connect Script&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: DpID = 0BD11477&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Error: Wire Ack Wait Fault&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Error: Wire Ack Wait Fault&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Disabling MPU&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Error: Wire Ack Wait Fault&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Error: Wire Ack Wait Fault&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Configure FlexRAM for 256KB OC RAM, 128KB I-TCM, 128KB D-TCM&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Error: Wire Ack Wait Fault&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Error: Wire Ack Wait Fault&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Error: Wire Ack Wait Fault&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: Finished&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Wc: ============= END SCRIPT =============================&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Probe Firmware: DAPLink CMSIS-DAP (ARM)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Serial Number: 0227000047784e4500299003d917004ce561000097969900&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: VID:PID: 0D28:0204&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: USB Path: /dev/hidraw5&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Using memory from core 0 after searching for a good core&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: connection failed - Nn(05). Wire ACK Wait in DAP access.. Retrying&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Ed:02: Failed on connect: Em(01). Cannot find MEM-AP selected by core index (check target power)&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Et: Probe(0): Connected&amp;amp;Reset. Was: NotConnected. DpID: 0BD11477. CpuID: 00000000. Info: &amp;lt;None&amp;gt;&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Last stub error 0: OK&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Last sticky error: 0x0 AIndex: 0&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: No debug bus (MemAp) selected&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: DAP Speed test unexecuted or failed&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;/FONT&gt;&lt;BR /&gt;&lt;FONT size="3"&gt;Pc: (100) Target Connection Failed&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;-------------------------&lt;/P&gt;&lt;P&gt;I tried using both firmware (QSPI and Hyperflash) and to flash both from the GUI Flash Tool and the cmd line.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Any solution?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I'm on Ubuntu 20.04.2 LTS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;</description>
      <pubDate>Thu, 15 Jul 2021 20:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1308627#M4235</guid>
      <dc:creator>dabortol</dc:creator>
      <dc:date>2021-07-15T20:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: Error when flashing to MIMXRT1050-EVKB - "Wire ACK Wait in DAP access"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1308775#M4237</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/189147"&gt;@dabortol&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;I guess the RT1050 chip is not power on. Please check J1. You should connect the jumper to 5-6.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jul 2021 03:27:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1308775#M4237</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-07-16T03:27:00Z</dc:date>
    </item>
    <item>
      <title>Re: Error when flashing to MIMXRT1050-EVKB - "Wire ACK Wait in DAP access"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1312618#M4250</link>
      <description>&lt;P&gt;J1 is connected to 5-6.&lt;/P&gt;&lt;P&gt;I get a slightly different error at times.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------&lt;/P&gt;&lt;P&gt;Ns: MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 17:55:57 - crt_emu_cm_redlink build 18)&lt;BR /&gt;Pc: ( 0) Reading remote configuration&lt;BR /&gt;Wc(03). No cache support.&lt;BR /&gt;Nc: Found chip XML file in ./mimxrt1050-evk-common/cmake/MIMXRT1052xxxxB.xml&lt;BR /&gt;Pc: ( 5) Remote configuration complete&lt;BR /&gt;Nc: Restarted LinkServer process (PID 159613).&lt;BR /&gt;Wc: ============= SCRIPT: RT1050_connect.scp =============&lt;BR /&gt;Wc: RT1050 Connect Script&lt;BR /&gt;Wc: DpID = 0BD11477&lt;BR /&gt;Wc: APID = 0x04770041&lt;BR /&gt;Wc: Disabling MPU&lt;BR /&gt;Wc: Configure FlexRAM for 256KB OC RAM, 128KB I-TCM, 128KB D-TCM&lt;BR /&gt;Wc: Finished&lt;BR /&gt;Wc: ============= END SCRIPT =============================&lt;BR /&gt;Nc: Probe Firmware: DAPLink CMSIS-DAP (ARM)&lt;BR /&gt;Nc: Serial Number: 0227000047784e4500299003d917004ce561000097969900&lt;BR /&gt;Nc: VID:PID: 0D28:0204&lt;BR /&gt;Nc: USB Path: /dev/hidraw5&lt;BR /&gt;Nc: Using memory from core 0 after searching for a good core&lt;BR /&gt;Pc: ( 30) Emulator Connected&lt;BR /&gt;Pc: ( 40) Debug Halt&lt;BR /&gt;Pc: ( 50) CPU ID&lt;BR /&gt;Nc: debug interface type = CoreSight DP (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;Nc: processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;Nc: number of h/w breakpoints = 8&lt;BR /&gt;Nc: number of flash patches = 0&lt;BR /&gt;Nc: number of h/w watchpoints = 4&lt;BR /&gt;Nc: Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Nc: Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Ns: Content of CoreSight Debug ROM(s):&lt;BR /&gt;Nc: RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;Nc: ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;Nc: ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;Nc: ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;Nc: ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;Nc: ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;Nc: ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;Nc: ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;Nc: ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;Nc: ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU&lt;BR /&gt;Nc: ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)&lt;BR /&gt;Nc: NXP: MIMXRT1052xxxxB&lt;BR /&gt;Nc: DAP stride is 1024 bytes (256 words)&lt;BR /&gt;Wc: XML Error - no license-type XML file 'crt_common.xme' on path.&lt;BR /&gt;Nc: note - part information contained no product license-type data&lt;BR /&gt;Nc: Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1050_SFDP_HYPERFLASH.cfx&lt;BR /&gt;Nc: Image 'iMXRT1050_SFDP_HYPERFLASH Mar 22 2021 08:16:02'&lt;BR /&gt;Nc: Opening flash driver MIMXRT1050_SFDP_HYPERFLASH.cfx&lt;BR /&gt;Nc: Sending VECTRESET to run flash driver&lt;BR /&gt;Nc: state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;Xw:&lt;BR /&gt;Nc: state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;Xw:&lt;BR /&gt;Wc: Warning - processor did not halt - gave up waiting&lt;BR /&gt;Nc: target failed to halt after flash driver reset - (null)&lt;BR /&gt;Nc: After error Nn(05). Wire ACK Wait in DAP access -&lt;BR /&gt;Nc: Failed to read address register in DAP - Nn(05). Wire ACK Wait in DAP access&lt;BR /&gt;Nc: Driver memory check after reset - mem not working after mailbox read - Em(17). Debug port inaccessible after access at location 0x2000D908&lt;BR /&gt;Nc: flash start - disabling IRQs failed - rc Ep(08). Cannot access core regs when target running.&lt;BR /&gt;Ec: vendor chip initialization failed - Ep(08). Cannot access core regs when target running.&lt;BR /&gt;Wc: failed to initialize flash driver MIMXRT1050_SFDP_HYPERFLASH.cfx&lt;BR /&gt;Pc: ( 65) Chip Setup Complete&lt;BR /&gt;Pc: (100) Target Connection Failed&lt;BR /&gt;Nc: error closing down debug session - Nn(05). Wire ACK Wait in DAP access&lt;/P&gt;</description>
      <pubDate>Fri, 23 Jul 2021 11:59:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1312618#M4250</guid>
      <dc:creator>dabortol</dc:creator>
      <dc:date>2021-07-23T11:59:48Z</dc:date>
    </item>
    <item>
      <title>Re: Error when flashing to MIMXRT1050-EVKB - "Wire ACK Wait in DAP access"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1312924#M4254</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;The RT1050 has powered on now. But it seems the code can't download to Hyperflash. Please check SW7. It should be 0110. You can refer to AN12107 Figure 8.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 02:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1312924#M4254</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-07-26T02:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: Error when flashing to MIMXRT1050-EVKB - "Wire ACK Wait in DAP access"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1313222#M4255</link>
      <description>&lt;P&gt;Hi, SW7 is set to 0110. Same as in Figure 8.&lt;/P&gt;</description>
      <pubDate>Mon, 26 Jul 2021 13:20:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1313222#M4255</guid>
      <dc:creator>dabortol</dc:creator>
      <dc:date>2021-07-26T13:20:42Z</dc:date>
    </item>
    <item>
      <title>Re: Error when flashing to MIMXRT1050-EVKB - "Wire ACK Wait in DAP access"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1313544#M4259</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;Maybe there is error code in flash which can cause download fail. Please try to use NXP_MCUBootUtility tool to erase flash. Before connect to the tool, set the SW7 to serial download mode first.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://github.com/JayHeng/NXP-MCUBootUtility" target="_blank"&gt;https://github.com/JayHeng/NXP-MCUBootUtility&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Tue, 27 Jul 2021 04:10:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1313544#M4259</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-07-27T04:10:50Z</dc:date>
    </item>
    <item>
      <title>Re: Error when flashing to MIMXRT1050-EVKB - "Wire ACK Wait in DAP access"</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1315345#M4267</link>
      <description>&lt;P&gt;Hi, after a few attempts I am now able to flash the device.&lt;/P&gt;&lt;P&gt;What worked for me was to :&lt;/P&gt;&lt;P&gt;- power off -&amp;gt; configure the board to serial downloader mode SW7 (0001)&lt;/P&gt;&lt;P&gt;- power on -&amp;gt; flash the device (MCUXpresso GUI Flash tool)&lt;/P&gt;&lt;P&gt;- power off -&amp;gt; set back SW7 to Hyper Flash Boot Mode (0110) -&amp;gt; power on&lt;/P&gt;&lt;P&gt;Reference &lt;A href="https://www.nxp.com/docs/en/application-note/AN12107.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN12107.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an unrelated issue (?) which is the LCD screen being black.&lt;/P&gt;&lt;P&gt;Thanks for your help&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Jul 2021 14:22:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK-Wait-in-DAP/m-p/1315345#M4267</guid>
      <dc:creator>dabortol</dc:creator>
      <dc:date>2021-07-29T14:22:37Z</dc:date>
    </item>
  </channel>
</rss>