<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックLPC54018 driver Init provided no flash parameters</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1308211#M4232</link>
    <description>&lt;P&gt;Hallo everyone,&lt;/P&gt;&lt;P&gt;I recently created a new project in MCUXpresso to work with FreeRTOS on my LPC54018 on the OM40003 Bord. Sadly, every attempt to start a debugging session ends in an “Driver V.2 dynamic startup failed - driver Init provided no flash parameters” &lt;SPAN&gt;Error. (detail below)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Even with the example Projects / clean FreeRTOS I encounter the same problem. As an older example Project worked on my Controller, I started to test different SDK versions. In version 2.8.2 and 2.6.0 neither new Projects nor examples worked. On the 2.3.0 Version only example Projects could run.&lt;/P&gt;&lt;P&gt;I also noticed the default SPIFI driver was changing from LPC540xx_SPIFI_GENERIC.cfx to LPC540xx_SPIFI_SFDP.cfx. sadly, I found no further information about those.&lt;/P&gt;&lt;P&gt;As I tried to flash the controller directly with the MCUExpresso flashing tool and the good version from the 2.3.0 SDK, I got another error: “File 'lpcxpresso54018v2.3_shell.axf' load failure: Ef(11). No flash configured.” Flash attempts with the other non debugable version got me back to the old error. But this time with a minor variation. “Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPI driver rc 15 (0xF)” instead of the former “Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPI driver rc 13 - No supported SPIFI device found”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It’s probably also worth mentioning, that I have to boot the controller into a non-default boot state (ISP-Mode) or end up with an “Cannot halt processor” error.&lt;/P&gt;&lt;P&gt;Also, I tried vector catch as mentioned in the various other posts with a similar problem.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Karl&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v11.3.1 [Build 5262] [2021-04-02]&lt;/P&gt;&lt;P&gt;SDK: LPCXpresso54018 version 2.8.2/ 2.6.0 / 2.3.0&lt;/P&gt;&lt;P&gt;Board: OM430003 with LPC54018 Rev E&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 16:50:12 - crt_emu_cm_redlink build 18)&lt;/P&gt;&lt;P&gt;Found chip XML file in C:/dev/MCUXpressoIDE_11.3.1_5262/Workspace/bare metal_v2.3/Debug\LPC54018.xml&lt;/P&gt;&lt;P&gt;(&amp;nbsp; 5) Remote configuration complete&lt;/P&gt;&lt;P&gt;Reconnected to existing LinkServer process.&lt;/P&gt;&lt;P&gt;Probe Firmware: LPC-LINK2 CMSIS-DAP V5.361 (NXP Semiconductors)&lt;/P&gt;&lt;P&gt;Serial Number:&amp;nbsp; LSAUAQBQ&lt;/P&gt;&lt;P&gt;VID:PID:&amp;nbsp; 1FC9:0090&lt;/P&gt;&lt;P&gt;USB Path: \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#8&amp;amp;13ccc672&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;/P&gt;&lt;P&gt;Using memory from core 0 after searching for a good core&lt;/P&gt;&lt;P&gt;debug interface type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = CoreSight DP (DAP DP ID 2BA01477) over SWD TAP 0&lt;/P&gt;&lt;P&gt;processor type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = Cortex-M4 (CPU ID 00000C24) on DAP AP 0&lt;/P&gt;&lt;P&gt;number of h/w breakpoints = 6&lt;/P&gt;&lt;P&gt;number of flash patches&amp;nbsp;&amp;nbsp; = 2&lt;/P&gt;&lt;P&gt;number of h/w watchpoints = 4&lt;/P&gt;&lt;P&gt;Probe(0): Connected&amp;amp;Reset. DpID: 2BA01477. CpuID: 00000C24. Info: &amp;lt;None&amp;gt;&lt;/P&gt;&lt;P&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;/P&gt;&lt;P&gt;Content of CoreSight Debug ROM(s):&lt;/P&gt;&lt;P&gt;RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)&lt;/P&gt;&lt;P&gt;ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU&lt;/P&gt;&lt;P&gt;ROM 1 E0041000: CID B105900D PID 04000BB925 CSt ETM type 0x13 Trace Source - Core&lt;/P&gt;&lt;P&gt;NXP: LPC54018&lt;/P&gt;&lt;P&gt;DAP stride is 4096 bytes (1024 words)&lt;/P&gt;&lt;P&gt;XML Error - no license-type XML file 'crt_common.xme' on path.&lt;/P&gt;&lt;P&gt;note - part information contained no product license-type data&lt;/P&gt;&lt;P&gt;Inspected v.2 External Flash Device on SPI LPC540xx_SPIFI_GENERIC.cfx&lt;/P&gt;&lt;P&gt;Image 'LPC5460x Generic SPIFI Mar 22 2021 08:18:07'&lt;/P&gt;&lt;P&gt;Opening flash driver LPC540xx_SPIFI_GENERIC.cfx&lt;/P&gt;&lt;P&gt;Sending VECTRESET to run flash driver&lt;/P&gt;&lt;P&gt;Driver V.2 dynamic startup failed - driver Init provided no flash parameters&lt;/P&gt;&lt;P&gt;Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;/P&gt;&lt;P&gt;Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPI driver rc 13 - No supported SPIFI device found&lt;/P&gt;&lt;P&gt;chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;/P&gt;&lt;P&gt;failed to initialize flash driver LPC540xx_SPIFI_GENERIC.cfx&lt;/P&gt;&lt;/LI-SPOILER&gt;</description>
    <pubDate>Thu, 15 Jul 2021 08:57:18 GMT</pubDate>
    <dc:creator>KTech</dc:creator>
    <dc:date>2021-07-15T08:57:18Z</dc:date>
    <item>
      <title>LPC54018 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1308211#M4232</link>
      <description>&lt;P&gt;Hallo everyone,&lt;/P&gt;&lt;P&gt;I recently created a new project in MCUXpresso to work with FreeRTOS on my LPC54018 on the OM40003 Bord. Sadly, every attempt to start a debugging session ends in an “Driver V.2 dynamic startup failed - driver Init provided no flash parameters” &lt;SPAN&gt;Error. (detail below)&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Even with the example Projects / clean FreeRTOS I encounter the same problem. As an older example Project worked on my Controller, I started to test different SDK versions. In version 2.8.2 and 2.6.0 neither new Projects nor examples worked. On the 2.3.0 Version only example Projects could run.&lt;/P&gt;&lt;P&gt;I also noticed the default SPIFI driver was changing from LPC540xx_SPIFI_GENERIC.cfx to LPC540xx_SPIFI_SFDP.cfx. sadly, I found no further information about those.&lt;/P&gt;&lt;P&gt;As I tried to flash the controller directly with the MCUExpresso flashing tool and the good version from the 2.3.0 SDK, I got another error: “File 'lpcxpresso54018v2.3_shell.axf' load failure: Ef(11). No flash configured.” Flash attempts with the other non debugable version got me back to the old error. But this time with a minor variation. “Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPI driver rc 15 (0xF)” instead of the former “Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPI driver rc 13 - No supported SPIFI device found”&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It’s probably also worth mentioning, that I have to boot the controller into a non-default boot state (ISP-Mode) or end up with an “Cannot halt processor” error.&lt;/P&gt;&lt;P&gt;Also, I tried vector catch as mentioned in the various other posts with a similar problem.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Karl&lt;/P&gt;&lt;P&gt;MCUXpresso IDE v11.3.1 [Build 5262] [2021-04-02]&lt;/P&gt;&lt;P&gt;SDK: LPCXpresso54018 version 2.8.2/ 2.6.0 / 2.3.0&lt;/P&gt;&lt;P&gt;Board: OM430003 with LPC54018 Rev E&lt;/P&gt;&lt;LI-SPOILER&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 16:50:12 - crt_emu_cm_redlink build 18)&lt;/P&gt;&lt;P&gt;Found chip XML file in C:/dev/MCUXpressoIDE_11.3.1_5262/Workspace/bare metal_v2.3/Debug\LPC54018.xml&lt;/P&gt;&lt;P&gt;(&amp;nbsp; 5) Remote configuration complete&lt;/P&gt;&lt;P&gt;Reconnected to existing LinkServer process.&lt;/P&gt;&lt;P&gt;Probe Firmware: LPC-LINK2 CMSIS-DAP V5.361 (NXP Semiconductors)&lt;/P&gt;&lt;P&gt;Serial Number:&amp;nbsp; LSAUAQBQ&lt;/P&gt;&lt;P&gt;VID:PID:&amp;nbsp; 1FC9:0090&lt;/P&gt;&lt;P&gt;USB Path: \\?\hid#vid_1fc9&amp;amp;pid_0090&amp;amp;mi_00#8&amp;amp;13ccc672&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;/P&gt;&lt;P&gt;Using memory from core 0 after searching for a good core&lt;/P&gt;&lt;P&gt;debug interface type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = CoreSight DP (DAP DP ID 2BA01477) over SWD TAP 0&lt;/P&gt;&lt;P&gt;processor type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = Cortex-M4 (CPU ID 00000C24) on DAP AP 0&lt;/P&gt;&lt;P&gt;number of h/w breakpoints = 6&lt;/P&gt;&lt;P&gt;number of flash patches&amp;nbsp;&amp;nbsp; = 2&lt;/P&gt;&lt;P&gt;number of h/w watchpoints = 4&lt;/P&gt;&lt;P&gt;Probe(0): Connected&amp;amp;Reset. DpID: 2BA01477. CpuID: 00000C24. Info: &amp;lt;None&amp;gt;&lt;/P&gt;&lt;P&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;/P&gt;&lt;P&gt;Content of CoreSight Debug ROM(s):&lt;/P&gt;&lt;P&gt;RBASE E00FF000: CID B105100D PID 04000BB4C4 ROM (type 0x1)&lt;/P&gt;&lt;P&gt;ROM 1 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0001000: CID B105E00D PID 04003BB002 Gen DWT (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0002000: CID B105E00D PID 04002BB003 Gen FPB (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0000000: CID B105E00D PID 04003BB001 Gen ITM (type 0x0)&lt;/P&gt;&lt;P&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A1 CSt TPIU type 0x11 Trace Sink - TPIU&lt;/P&gt;&lt;P&gt;ROM 1 E0041000: CID B105900D PID 04000BB925 CSt ETM type 0x13 Trace Source - Core&lt;/P&gt;&lt;P&gt;NXP: LPC54018&lt;/P&gt;&lt;P&gt;DAP stride is 4096 bytes (1024 words)&lt;/P&gt;&lt;P&gt;XML Error - no license-type XML file 'crt_common.xme' on path.&lt;/P&gt;&lt;P&gt;note - part information contained no product license-type data&lt;/P&gt;&lt;P&gt;Inspected v.2 External Flash Device on SPI LPC540xx_SPIFI_GENERIC.cfx&lt;/P&gt;&lt;P&gt;Image 'LPC5460x Generic SPIFI Mar 22 2021 08:18:07'&lt;/P&gt;&lt;P&gt;Opening flash driver LPC540xx_SPIFI_GENERIC.cfx&lt;/P&gt;&lt;P&gt;Sending VECTRESET to run flash driver&lt;/P&gt;&lt;P&gt;Driver V.2 dynamic startup failed - driver Init provided no flash parameters&lt;/P&gt;&lt;P&gt;Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;/P&gt;&lt;P&gt;Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPI driver rc 13 - No supported SPIFI device found&lt;/P&gt;&lt;P&gt;chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;/P&gt;&lt;P&gt;failed to initialize flash driver LPC540xx_SPIFI_GENERIC.cfx&lt;/P&gt;&lt;/LI-SPOILER&gt;</description>
      <pubDate>Thu, 15 Jul 2021 08:57:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1308211#M4232</guid>
      <dc:creator>KTech</dc:creator>
      <dc:date>2021-07-15T08:57:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1308763#M4236</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;Please first use a simple demo project LED to test.&lt;/P&gt;
&lt;P&gt;If still can't work, please take a video or screenshots show your steps.&lt;/P&gt;
&lt;P&gt;Does your board can work well before?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Fri, 16 Jul 2021 03:04:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1308763#M4236</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-07-16T03:04:46Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1309567#M4240</link>
      <description>&lt;P&gt;Hallo Alice,&lt;/P&gt;&lt;P&gt;yes my board worked well bevor, using mainly test projects from the 2.3.0 SDK Version.&lt;/P&gt;&lt;P&gt;Now I cannot get anything to work being created from the newer SDK versions, while the old 2.3 examples are still running fine.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;U&gt;Gpio_led_out&lt;/U&gt;&lt;/STRONG&gt; SDK version 2.8.2&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;I click import SDK example.&lt;/LI&gt;&lt;LI&gt;I select the LPC54018 Board.&lt;/LI&gt;&lt;LI&gt;I select the LED-project. (See image)&lt;/LI&gt;&lt;LI&gt;I reset the LPC-Bord by pressing reset and Button 1 for SPI Boot mode. Otherwise, I get the cannot hold processor error&lt;/LI&gt;&lt;LI&gt;I start Debugging.&lt;/LI&gt;&lt;LI&gt;I confirm the Probe selection.&lt;/LI&gt;&lt;LI&gt;Error (See images)&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;This very exact process works fine with v2.3.0 examples but fails as soon as I try the same with a new project.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Karl&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="project selection.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150156i179266C7E4C3555E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="project selection.bmp" alt="project selection.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="error1.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150152iCE83951643D7A9D5/image-size/medium?v=v2&amp;amp;px=400" role="button" title="error1.bmp" alt="error1.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="error2.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150153i9FC38D7314485D74/image-size/medium?v=v2&amp;amp;px=400" role="button" title="error2.bmp" alt="error2.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="error3.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150154i1C4C31F8AF1A75BC/image-size/medium?v=v2&amp;amp;px=400" role="button" title="error3.bmp" alt="error3.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="SDK.bmp" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150155iB4B0069B777BD63D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="SDK.bmp" alt="SDK.bmp" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;     &lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 07:32:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1309567#M4240</guid>
      <dc:creator>KTech</dc:creator>
      <dc:date>2021-07-19T07:32:25Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1309776#M4245</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello &lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;A id="link_22" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/185875" target="_self" aria-label="View Profile of KTech"&gt;&lt;SPAN class=""&gt;KTech&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;Try to erase chip based on ISP mode:&lt;/P&gt;
&lt;P&gt;pressing ISP button and do not release,&amp;nbsp; and click erase button as below: &lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Alice_Yang_0-1626690735766.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/150204i3CABA06B2525476D/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Alice_Yang_0-1626690735766.png" alt="Alice_Yang_0-1626690735766.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Pay attention, open a new workspace and import new led project to try.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 10:32:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1309776#M4245</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-07-19T10:32:56Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54018 driver Init provided no flash parameters</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1309820#M4246</link>
      <description>&lt;P&gt;Hallo Alice&lt;/P&gt;&lt;P&gt;thank you very much, after the Mass erase I can now debug again. Pressing the ISP buttons for the entire time when using the chip tool was the solution.&lt;/P&gt;&lt;P&gt;PS: for everyone with the same problem ISP button 0 was the one to press. &amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Karl&lt;/P&gt;</description>
      <pubDate>Mon, 19 Jul 2021 11:19:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC54018-driver-Init-provided-no-flash-parameters/m-p/1309820#M4246</guid>
      <dc:creator>KTech</dc:creator>
      <dc:date>2021-07-19T11:19:04Z</dc:date>
    </item>
  </channel>
</rss>