<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: RT1060-EVK Unable to program</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/RT1060-EVK-Unable-to-program/m-p/1297169#M4194</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/101064"&gt;@chadgraham&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;As I saw that you use the MCUBootUtility, I think you already try the serial downloader but could you confirm if the method in the following &lt;A href="read://https_mcuoneclipse.com/?url=https%3A%2F%2Fmcuoneclipse.com%2F2019%2F01%2F02%2Fregaining-debug-access-of-nxp-i-mx-rt1064-evk-executing-wfi%2F" target="_self"&gt;post&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
    <pubDate>Wed, 23 Jun 2021 22:10:39 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2021-06-23T22:10:39Z</dc:date>
    <item>
      <title>RT1060-EVK Unable to program</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/RT1060-EVK-Unable-to-program/m-p/1294267#M4191</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I have a RT1060-EVK that I cannot connect to with the CMSIS-DAP.&amp;nbsp; I have tried new workspaces, new examples, different QSPI configuration files, external tools (blhost), and even the Boot utility... all without success.&lt;/P&gt;&lt;P&gt;Looking on the forums, this appears to be a common problem, but none of the suggestions have corrected the issue.&amp;nbsp; Does anyone have a method to correct this?&amp;nbsp; The error log is listed below.&lt;/P&gt;&lt;P&gt;MCUXpresso IDE RedlinkMulti Driver v11.3 (Mar 30 2021 16:50:12 - crt_emu_cm_redlink build 18)&lt;BR /&gt;Found chip XML file in C:/Work/Designs/TempWorkspace/evkmimxrt1060_iled_blinky/Debug\MIMXRT1062xxxxA.xml&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;============= SCRIPT: RT1060_connect.scp =============&lt;BR /&gt;RT1060 Connect Script&lt;BR /&gt;DpID = 0BD11477&lt;BR /&gt;APID = 0x04770041&lt;BR /&gt;Disabling MPU&lt;BR /&gt;Configure FlexRAM for 768KB OC RAM, 128KB I-TCM, 128KB D-TCM&lt;BR /&gt;Finished&lt;BR /&gt;============= END SCRIPT =============================&lt;BR /&gt;Probe Firmware: CMSIS-DAP (ARM)&lt;BR /&gt;Serial Number: 02290000060a94aa00000000000000000000000097969905&lt;BR /&gt;VID:PID: 0D28:0204&lt;BR /&gt;USB Path: \\?\hid#vid_0d28&amp;amp;pid_0204&amp;amp;mi_03#a&amp;amp;1e662134&amp;amp;0&amp;amp;0000#{4d1e55b2-f16f-11cf-88cb-001111000030}&lt;BR /&gt;Using memory from core 0 after searching for a good core&lt;BR /&gt;debug interface type = CoreSight DP (DAP DP ID 0BD11477) over SWD TAP 0&lt;BR /&gt;processor type = Cortex-M7 (CPU ID 00000C27) on DAP AP 0&lt;BR /&gt;number of h/w breakpoints = 8&lt;BR /&gt;number of flash patches = 0&lt;BR /&gt;number of h/w watchpoints = 4&lt;BR /&gt;Probe(0): Connected&amp;amp;Reset. DpID: 0BD11477. CpuID: 00000C27. Info: &amp;lt;None&amp;gt;&lt;BR /&gt;Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.&lt;BR /&gt;Content of CoreSight Debug ROM(s):&lt;BR /&gt;RBASE E00FD000: CID B105100D PID 000008E88C ROM (type 0x1)&lt;BR /&gt;ROM 1 E00FE000: CID B105100D PID 04000BB4C8 ROM (type 0x1)&lt;BR /&gt;ROM 2 E00FF000: CID B105100D PID 04000BB4C7 ROM (type 0x1)&lt;BR /&gt;ROM 3 E000E000: CID B105E00D PID 04000BB00C Gen SCS (type 0x0)&lt;BR /&gt;ROM 3 E0001000: CID B105E00D PID 04000BB002 Gen DWT (type 0x0)&lt;BR /&gt;ROM 3 E0002000: CID B105E00D PID 04000BB00E Gen (type 0x0)&lt;BR /&gt;ROM 3 E0000000: CID B105E00D PID 04000BB001 Gen ITM (type 0x0)&lt;BR /&gt;ROM 2 E0041000: CID B105900D PID 04001BB975 CSt ARM ETMv4.0 type 0x13 Trace Source - Core&lt;BR /&gt;ROM 2 E0042000: CID B105900D PID 04004BB906 CSt type 0x14 Debug Control - Trigger, e.g. ECT&lt;BR /&gt;ROM 1 E0040000: CID B105900D PID 04000BB9A9 CSt type 0x11 Trace Sink - TPIU&lt;BR /&gt;ROM 1 E0043000: CID B105F00D PID 04001BB101 Sys (type 0x0)&lt;BR /&gt;NXP: MIMXRT1062xxxxA&lt;BR /&gt;DAP stride is 1024 bytes (256 words)&lt;BR /&gt;XML Error - no license-type XML file 'crt_common.xme' on path.&lt;BR /&gt;note - part information contained no product license-type data&lt;BR /&gt;Inspected v.2 External Flash Device on SPI using SFDP JEDEC ID MIMXRT1060_SFDP_QSPI.cfx&lt;BR /&gt;Image 'iMXRT1060_SFDP_QSPI Mar 22 2021 08:15:58'&lt;BR /&gt;Opening flash driver MIMXRT1060_SFDP_QSPI.cfx&lt;BR /&gt;Sending VECTRESET to run flash driver&lt;BR /&gt;Driver V.2 dynamic startup failed - driver Init provided no flash parameters&lt;BR /&gt;Flash Driver V.2 startup failed - rc Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;BR /&gt;Terminate (0x0, 0x0, 0x0) status 0x40 - driver reports init failure - EXTSPIJ driver rc 20107 (0x4E8B)&lt;BR /&gt;chip initialization failed - Ef(55): Dynamic flash driver startup failed to provide flash parameters.&lt;BR /&gt;failed to initialize flash driver MIMXRT1060_SFDP_QSPI.cfx&lt;/P&gt;</description>
      <pubDate>Thu, 17 Jun 2021 18:56:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/RT1060-EVK-Unable-to-program/m-p/1294267#M4191</guid>
      <dc:creator>chadgraham</dc:creator>
      <dc:date>2021-06-17T18:56:02Z</dc:date>
    </item>
    <item>
      <title>Re: RT1060-EVK Unable to program</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/RT1060-EVK-Unable-to-program/m-p/1297169#M4194</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/101064"&gt;@chadgraham&lt;/a&gt;,&lt;/P&gt;
&lt;P&gt;As I saw that you use the MCUBootUtility, I think you already try the serial downloader but could you confirm if the method in the following &lt;A href="read://https_mcuoneclipse.com/?url=https%3A%2F%2Fmcuoneclipse.com%2F2019%2F01%2F02%2Fregaining-debug-access-of-nxp-i-mx-rt1064-evk-executing-wfi%2F" target="_self"&gt;post&lt;/A&gt;.&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Alexis Andalon&lt;/P&gt;</description>
      <pubDate>Wed, 23 Jun 2021 22:10:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/RT1060-EVK-Unable-to-program/m-p/1297169#M4194</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2021-06-23T22:10:39Z</dc:date>
    </item>
  </channel>
</rss>