<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: How to increase RPMsg buffer size?</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/How-to-increase-RPMsg-buffer-size/m-p/1286362#M4179</link>
    <description>&lt;P&gt;Hello, &lt;BR /&gt;&lt;BR /&gt;For the master side one should look in the Linux side RPMSG driver, it is located at drivers/rpmsg/imx_rpmsg.c&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
    <pubDate>Wed, 02 Jun 2021 22:05:48 GMT</pubDate>
    <dc:creator>AldoG</dc:creator>
    <dc:date>2021-06-02T22:05:48Z</dc:date>
    <item>
      <title>How to increase RPMsg buffer size?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/How-to-increase-RPMsg-buffer-size/m-p/1278386#M4164</link>
      <description>&lt;P&gt;For our product testing we need to determine what the transfer time to send data to and from the core complex's on a i.MX8M Nano. We have the VAR-SOM-MX8M-NANO development boards.&lt;BR /&gt;&lt;BR /&gt;I have changed RL_BUFFER_PAYLOAD_SIZE in rpmsg_config.h to 2032&lt;/P&gt;&lt;P&gt;However I cannot find "SH_MEM_TOTAL_SIZE in any file and also I cannot find main_master.c and main_remote_master.c in the build.&lt;/P&gt;&lt;P&gt;I am using mcuxpresso_sdk_2.9.x-var01 (at &lt;A href="https://github.com/varigit/freertos-variscite" target="_blank"&gt;https://github.com/varigit/freertos-variscite&lt;/A&gt;) on a VAR-SOM-MX8M-NANO which is a Cortex A53 running Linux and a Cortex M7 running FreeRTOS&lt;/P&gt;&lt;P&gt;Are these definitions in different files than listed here which may be specific to setting the Master?&lt;/P&gt;&lt;P&gt;Thank you much for your help.&lt;/P&gt;&lt;P&gt;Brian&lt;/P&gt;&lt;P&gt;0Comments&lt;/P&gt;</description>
      <pubDate>Tue, 18 May 2021 16:50:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/How-to-increase-RPMsg-buffer-size/m-p/1278386#M4164</guid>
      <dc:creator>btclark1</dc:creator>
      <dc:date>2021-05-18T16:50:34Z</dc:date>
    </item>
    <item>
      <title>Re: How to increase RPMsg buffer size?</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/How-to-increase-RPMsg-buffer-size/m-p/1286362#M4179</link>
      <description>&lt;P&gt;Hello, &lt;BR /&gt;&lt;BR /&gt;For the master side one should look in the Linux side RPMSG driver, it is located at drivers/rpmsg/imx_rpmsg.c&lt;BR /&gt;&lt;BR /&gt;Best regards,&lt;BR /&gt;Aldo.&lt;/P&gt;</description>
      <pubDate>Wed, 02 Jun 2021 22:05:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/How-to-increase-RPMsg-buffer-size/m-p/1286362#M4179</guid>
      <dc:creator>AldoG</dc:creator>
      <dc:date>2021-06-02T22:05:48Z</dc:date>
    </item>
  </channel>
</rss>