<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCU-Link debug probe messing up variables in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1259012#M4140</link>
    <description>&lt;P&gt;Just to clear up some comments on this thread:&lt;/P&gt;
&lt;P&gt;MCUXpresso supports PE Micro and SEGGER probes via their respective GDB servers, while the other probe types (basically CMSIS-DAP protocol probes from NXP) are serviced via an equivalent server called Linkserver. The issue reported in this thread was down to a bug in Linkserver which was fully scoped and fixed in release 11.3.1.&lt;/P&gt;</description>
    <pubDate>Thu, 08 Apr 2021 16:03:12 GMT</pubDate>
    <dc:creator>brendonslade</dc:creator>
    <dc:date>2021-04-08T16:03:12Z</dc:date>
    <item>
      <title>MCU-Link debug probe messing up variables</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1250652#M4133</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I've recently received a new MCU-Link debug probe and wanted to use it for my new projects, as it offers an amazing speed improvement compared to the LPC-Link or LPC-Link2.&lt;/P&gt;&lt;P&gt;But during one of my last debug sessions I've encountered a strange behaviour with the MCU-Link.&lt;/P&gt;&lt;P&gt;If I create an array with unsigned chars and change the first byte, then everything is ok. But as soon as I modify the second byte, then the third and fourth byte are also changed to a seemingly random value. If the third Byte is changed, then only the fourth byte is changed.&lt;/P&gt;&lt;P&gt;Thats not very nice, but I could live with that for now. But whats really bad in my oppinion is, if I create an array with, for example, 14 bytes and change the last one, then there are two bytes changed outside of the array.&lt;/P&gt;&lt;P&gt;I've tested that with two custom boards with a MIMXRT1011 and MIMXRT1024 and also with a LPCXPRESSO1769 board. Also when I use the LPC-Link2 (with Segger J-Link Firmware), then everything is normal.&lt;/P&gt;&lt;P&gt;The test projects for the RT1011 and for the LPC1769 are attached, and also a screen capture of MCUXpresso showing the problem.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Mar 2021 18:00:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1250652#M4133</guid>
      <dc:creator>PWaas</dc:creator>
      <dc:date>2021-03-23T18:00:03Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-Link debug probe messing up variables</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1251009#M4135</link>
      <description>&lt;P&gt;Hello &lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160422" target="_self"&gt;&lt;SPAN class=""&gt;PWaas,&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;SPAN class=""&gt;I use LPC-link2 test LPC1769 refer to&amp;nbsp; your video, the same.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;SPAN class=""&gt;And why do you need add data through this way?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;SPAN class=""&gt;BR&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;SPAN class=""&gt;Alice&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 08:08:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1251009#M4135</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-03-24T08:08:52Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-Link debug probe messing up variables</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1251099#M4136</link>
      <description>&lt;P&gt;Hello Alice,&lt;/P&gt;&lt;P&gt;I've never really used the LPC-Link2 with the CMSIS DAP firmware. I switched to the Segger J-Link firmware right after I got it, as it was faster and more relieable in some situations.&lt;/P&gt;&lt;P&gt;You are right, the LPC-Link and the LPC-Link2 with CMSIS DAP Firmware show the same behaviour, but the LPC-Link2 with J-Link firmware does not, so it seems like a general problem with the implementation.&lt;/P&gt;&lt;P&gt;But nevertheless, I think that modifying variables at runtime is a very basic function of any debugger and should not change values that haven't been touched.&lt;/P&gt;&lt;P&gt;For example when you want to test some functions with different values without recompiling the whole project every time, or maybe you want to modify the raturn value of a function. The easiest way I found of doing that, is to use the Expressions, as the context menu already offers a shortcut to that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 24 Mar 2021 09:39:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1251099#M4136</guid>
      <dc:creator>PWaas</dc:creator>
      <dc:date>2021-03-24T09:39:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-Link debug probe messing up variables</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1251996#M4137</link>
      <description>&lt;P&gt;Hello &lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160422" target="_self"&gt;&lt;SPAN class=""&gt;PWaas&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;Thanks for your sharing, I know your meaning now, I have submit a ticket about this feature to development team, and keep you informed after get any update.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 25 Mar 2021 09:11:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1251996#M4137</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-03-25T09:11:48Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-Link debug probe messing up variables</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1256915#M4138</link>
      <description>&lt;P&gt;Hello &lt;SPAN class="UserName lia-user-name lia-user-rank-Contributor-I lia-component-message-view-widget-author-username"&gt;&lt;A id="link_12" class="lia-link-navigation lia-page-link lia-user-name-link" style="color: #333f48;" href="https://community.nxp.com/t5/user/viewprofilepage/user-id/160422" target="_self"&gt;&lt;SPAN class=""&gt;PWaas&lt;/SPAN&gt;&lt;/A&gt;&lt;/SPAN&gt;,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Please use the production of &amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;A href="https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-integrated-development-environment-ide:MCUXpresso-IDE?tab=Design_Tools_Tab#nogo" target="_blank"&gt;IDE 11.3.1 is now available&lt;/A&gt; .&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;To be clear to everyone, the issue wasn't MCU-Link specific, but also impacts other debug probes that connect using LinkServer (previously known as redline), so that includes LPC-Link, LPC-Link2 and the LPC11U35 based CMSIS-DAP debug probes.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;Thanks.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;BR&lt;/P&gt;
&lt;P&gt;Alice&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 02:59:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1256915#M4138</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2021-04-08T02:59:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-Link debug probe messing up variables</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1258192#M4139</link>
      <description>&lt;P&gt;&amp;lt;post removed as Alice updated her post with same info&amp;gt;&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 15:54:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1258192#M4139</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2021-04-08T15:54:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCU-Link debug probe messing up variables</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1259012#M4140</link>
      <description>&lt;P&gt;Just to clear up some comments on this thread:&lt;/P&gt;
&lt;P&gt;MCUXpresso supports PE Micro and SEGGER probes via their respective GDB servers, while the other probe types (basically CMSIS-DAP protocol probes from NXP) are serviced via an equivalent server called Linkserver. The issue reported in this thread was down to a bug in Linkserver which was fully scoped and fixed in release 11.3.1.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Apr 2021 16:03:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCU-Link-debug-probe-messing-up-variables/m-p/1259012#M4140</guid>
      <dc:creator>brendonslade</dc:creator>
      <dc:date>2021-04-08T16:03:12Z</dc:date>
    </item>
  </channel>
</rss>