<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PORT_SetPinInterruptConfig() mixing GPIO &amp;amp; PORT in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/PORT-SetPinInterruptConfig-mixing-GPIO-amp-PORT/m-p/1236288#M4108</link>
    <description>&lt;P&gt;Hi Jing,&lt;/P&gt;&lt;P&gt;Thank you very much for putting a fine point on that for me. I appreciate your help!&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Andre.&lt;/P&gt;</description>
    <pubDate>Thu, 25 Feb 2021 04:44:17 GMT</pubDate>
    <dc:creator>Frotz</dc:creator>
    <dc:date>2021-02-25T04:44:17Z</dc:date>
    <item>
      <title>PORT_SetPinInterruptConfig() mixing GPIO &amp; PORT</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/PORT-SetPinInterruptConfig-mixing-GPIO-amp-PORT/m-p/1234747#M4105</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;In the gpio_input_interrupt example for the FRDM-KE15Z, the interrupt is configured using&amp;nbsp;PORT_SetPinInterruptConfig(). The pin for SW2 is on GPIOB and the port used in the example is PORTB. Is there any value in using a different port when calling this function. Is it always necessary to match the GPIO module and the port? Can they be mixed?&lt;/P&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;&lt;P&gt;Andre.&lt;/P&gt;</description>
      <pubDate>Tue, 23 Feb 2021 05:50:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/PORT-SetPinInterruptConfig-mixing-GPIO-amp-PORT/m-p/1234747#M4105</guid>
      <dc:creator>Frotz</dc:creator>
      <dc:date>2021-02-23T05:50:05Z</dc:date>
    </item>
    <item>
      <title>Re: PORT_SetPinInterruptConfig() mixing GPIO &amp; PORT</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/PORT-SetPinInterruptConfig-mixing-GPIO-amp-PORT/m-p/1236270#M4107</link>
      <description>&lt;P&gt;Hi Frotz,&lt;/P&gt;
&lt;P&gt;Yes, the io interrupt control register is in PORT group, not in gpio group. GPIOA is corresponding to PORTA and&amp;nbsp;GPIOB is corresponding to PORTB. This is fixed.&lt;/P&gt;
&lt;P&gt;Once&amp;nbsp;PORT_SetPinInterruptConfig() is called, it only can enable one interrupt from a certain group pins.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Regards,&lt;/P&gt;
&lt;P&gt;Jing&lt;/P&gt;</description>
      <pubDate>Thu, 25 Feb 2021 03:26:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/PORT-SetPinInterruptConfig-mixing-GPIO-amp-PORT/m-p/1236270#M4107</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2021-02-25T03:26:38Z</dc:date>
    </item>
    <item>
      <title>Re: PORT_SetPinInterruptConfig() mixing GPIO &amp; PORT</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/PORT-SetPinInterruptConfig-mixing-GPIO-amp-PORT/m-p/1236288#M4108</link>
      <description>&lt;P&gt;Hi Jing,&lt;/P&gt;&lt;P&gt;Thank you very much for putting a fine point on that for me. I appreciate your help!&lt;/P&gt;&lt;P&gt;Best,&lt;/P&gt;&lt;P&gt;Andre.&lt;/P&gt;</description>
      <pubDate>Thu, 25 Feb 2021 04:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/PORT-SetPinInterruptConfig-mixing-GPIO-amp-PORT/m-p/1236288#M4108</guid>
      <dc:creator>Frotz</dc:creator>
      <dc:date>2021-02-25T04:44:17Z</dc:date>
    </item>
  </channel>
</rss>