<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 Re: Python 3.8.1 installed, but IDE remind that 'Requested Python version (3) not installed'</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1209587#M4075</link>
    <description>&lt;P&gt;I used python 2.7 at first time.&lt;/P&gt;&lt;P&gt;And I generated a firmware successfully, it can not boot up. I found that the&amp;nbsp;dk6_image_tool.py script should work with python(3).&lt;/P&gt;&lt;P&gt;As I changed a computer to install the same IDE, SDK and python 3.8.1, everything works well.&lt;/P&gt;</description>
    <pubDate>Mon, 11 Jan 2021 10:04:26 GMT</pubDate>
    <dc:creator>zengfs</dc:creator>
    <dc:date>2021-01-11T10:04:26Z</dc:date>
    <item>
      <title>Python 3.8.1 installed, but IDE remind that 'Requested Python version (3) not installed'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1206653#M4064</link>
      <description>&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="zengfs_0-1609833560605.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/133959iCAE882A7B476411E/image-size/medium?v=v2&amp;amp;px=400" role="button" title="zengfs_0-1609833560605.png" alt="zengfs_0-1609833560605.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I can check the python version in cmd, but IDE still remind me that the python3 was not installed.&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 08:00:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1206653#M4064</guid>
      <dc:creator>zengfs</dc:creator>
      <dc:date>2021-01-05T08:00:17Z</dc:date>
    </item>
    <item>
      <title>Re: Python 3.8.1 installed, but IDE remind that 'Requested Python version (3) not installed'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1206746#M4065</link>
      <description>&lt;P&gt;The script is running something called "py" not "python".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 05 Jan 2021 09:18:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1206746#M4065</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2021-01-05T09:18:13Z</dc:date>
    </item>
    <item>
      <title>Re: Python 3.8.1 installed, but IDE remind that 'Requested Python version (3) not installed'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1207168#M4066</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt; You should use python2.7. The syntax is little different.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="2.PNG" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/134065i80B725A7D708BBB1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="2.PNG" alt="2.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;
&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;
&lt;P&gt;- We are following threads for 7 days after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;</description>
      <pubDate>Wed, 06 Jan 2021 01:46:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1207168#M4066</guid>
      <dc:creator>nxf56274</dc:creator>
      <dc:date>2021-01-06T01:46:29Z</dc:date>
    </item>
    <item>
      <title>Re: Python 3.8.1 installed, but IDE remind that 'Requested Python version (3) not installed'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1209587#M4075</link>
      <description>&lt;P&gt;I used python 2.7 at first time.&lt;/P&gt;&lt;P&gt;And I generated a firmware successfully, it can not boot up. I found that the&amp;nbsp;dk6_image_tool.py script should work with python(3).&lt;/P&gt;&lt;P&gt;As I changed a computer to install the same IDE, SDK and python 3.8.1, everything works well.&lt;/P&gt;</description>
      <pubDate>Mon, 11 Jan 2021 10:04:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1209587#M4075</guid>
      <dc:creator>zengfs</dc:creator>
      <dc:date>2021-01-11T10:04:26Z</dc:date>
    </item>
    <item>
      <title>Re: Python 3.8.1 installed, but IDE remind that 'Requested Python version (3) not installed'</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1221212#M4097</link>
      <description>&lt;P&gt;From the project setting, there is a post compiling command:&lt;/P&gt;
&lt;P&gt;echo "${OsType}" | grep -q win* &amp;amp;&amp;amp; py -3 "../scripts/dk6_image_tool.py" -s 294912 ${ENV_IMAGE_TOOL_OPTS} ${BuildArtifactFileName} || python3 "../scripts/dk6_image_tool.py" -s 294912 ${ENV_IMAGE_TOOL_OPTS} ${BuildArtifactFileName}&lt;/P&gt;
&lt;P&gt;So clearly it asks for Python 3. Not Python 2.7. This is a good thing I think because python 2.x is phasing out.&lt;/P&gt;
&lt;P&gt;I guess the documentation is not up-to-date because it still asks us to install 2.7.&lt;/P&gt;
&lt;P&gt;As for you issue I have no clue too. The command asks for either "py" or "python3". But in your screenshot you only showed "python -v" Could that be somehow you only have python.exe but not python3.exe available in your environment?&lt;/P&gt;</description>
      <pubDate>Tue, 26 Jan 2021 11:14:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Python-3-8-1-installed-but-IDE-remind-that-Requested-Python/m-p/1221212#M4097</guid>
      <dc:creator>Xiang_Li</dc:creator>
      <dc:date>2021-01-26T11:14:16Z</dc:date>
    </item>
  </channel>
</rss>