<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: redlink server not starting in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1163917#M3959</link>
    <description>&lt;P&gt;The firewall is off. It seems to me that the debugger can't connect to the server because the server is not running!&lt;/P&gt;&lt;P&gt;I expected "r&lt;SPAN&gt;edlinkserv -commandline" to manually start the server and give me a command prompt. It doesn't. It starts and then shuts down immediately.&lt;/SPAN&gt;&lt;/P&gt;</description>
    <pubDate>Wed, 07 Oct 2020 12:54:28 GMT</pubDate>
    <dc:creator>pnw4</dc:creator>
    <dc:date>2020-10-07T12:54:28Z</dc:date>
    <item>
      <title>redlink server not starting</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1163837#M3957</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using MCUXpresso v11.2.0.build 4120 on Windows 10 with an LPC-Link2 board.&lt;/P&gt;&lt;P&gt;The problem is that the "Probe discovering operation for IDE LinkServer probes" never completes. The error is: "RedlinkServerException Cannot write to server: not open". The RedlinkServer log just shows:&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Closed]&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Closed]&lt;/P&gt;&lt;P&gt;...&lt;/P&gt;&lt;P&gt;I have re-flashed the LPC_Link2 board and it shows up in device manager as "LPC-LinkII UCom Port (COM4)"&lt;/P&gt;&lt;P&gt;Starting redlinkserv from the command line shows the following and exits to the command prompt:&lt;/P&gt;&lt;P&gt;C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\binaries&amp;gt;redlinkserv -commandline&lt;BR /&gt;redlink&amp;gt;telnet server: bind to port 3025 - No error (rc 0)&lt;/P&gt;&lt;P&gt;C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\binaries&amp;gt;&lt;/P&gt;&lt;P&gt;No redlinkserv process is running.&lt;/P&gt;&lt;P&gt;Can you suggest what to try next?&lt;/P&gt;&lt;P&gt;Cheers - Paul&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 10:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1163837#M3957</guid>
      <dc:creator>pnw4</dc:creator>
      <dc:date>2020-10-07T10:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: redlink server not starting</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1163850#M3958</link>
      <description>&lt;P&gt;Check your firewall. It looks like it is preventing the debugger from connecting to the server.&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 10:39:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1163850#M3958</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-10-07T10:39:44Z</dc:date>
    </item>
    <item>
      <title>Re: redlink server not starting</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1163917#M3959</link>
      <description>&lt;P&gt;The firewall is off. It seems to me that the debugger can't connect to the server because the server is not running!&lt;/P&gt;&lt;P&gt;I expected "r&lt;SPAN&gt;edlinkserv -commandline" to manually start the server and give me a command prompt. It doesn't. It starts and then shuts down immediately.&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 07 Oct 2020 12:54:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1163917#M3959</guid>
      <dc:creator>pnw4</dc:creator>
      <dc:date>2020-10-07T12:54:28Z</dc:date>
    </item>
    <item>
      <title>Re: redlink server not starting</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1164358#M3960</link>
      <description>&lt;P&gt;That definitely implies that the firewall (or something) is blocking the server. Double check firewalls, antivirus, anti malware etc.&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 08:04:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/redlink-server-not-starting/m-p/1164358#M3960</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-10-08T08:04:19Z</dc:date>
    </item>
  </channel>
</rss>