<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックUSB not connecting from VCOM CDC example</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/USB-not-connecting-from-VCOM-CDC-example/m-p/1159514#M3950</link>
    <description>&lt;P&gt;Using an LPC55S16 dev board and wanting to talk CDC VCOM out on the USB FS port.&lt;/P&gt;&lt;P&gt;Using MXCUexpresso 11.2 and SDK 2.8.2&lt;/P&gt;&lt;P&gt;Pulled in the lpcxresso55s16_dev_cdc_vcom_bm and the lite version of this, compiled (without problems) and ran it out onto the board. Board is being powered by the debug interface so is providing a vcom for that (LPC-Link II UCom Port) just fine, it looks like.&lt;/P&gt;&lt;P&gt;The problem is that neither of these stock, out of the box things will connect on either of the USB ports.&amp;nbsp; Windows (10) shows an error of Unkown USB Device (Device Descriptor Request Failed) which tells me it doesn't get real far here...&lt;/P&gt;&lt;P&gt;Any ideas?&amp;nbsp; Neither of these stock projects works out of the box....&lt;/P&gt;</description>
    <pubDate>Fri, 25 Sep 2020 20:01:04 GMT</pubDate>
    <dc:creator>randylee</dc:creator>
    <dc:date>2020-09-25T20:01:04Z</dc:date>
    <item>
      <title>USB not connecting from VCOM CDC example</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/USB-not-connecting-from-VCOM-CDC-example/m-p/1159514#M3950</link>
      <description>&lt;P&gt;Using an LPC55S16 dev board and wanting to talk CDC VCOM out on the USB FS port.&lt;/P&gt;&lt;P&gt;Using MXCUexpresso 11.2 and SDK 2.8.2&lt;/P&gt;&lt;P&gt;Pulled in the lpcxresso55s16_dev_cdc_vcom_bm and the lite version of this, compiled (without problems) and ran it out onto the board. Board is being powered by the debug interface so is providing a vcom for that (LPC-Link II UCom Port) just fine, it looks like.&lt;/P&gt;&lt;P&gt;The problem is that neither of these stock, out of the box things will connect on either of the USB ports.&amp;nbsp; Windows (10) shows an error of Unkown USB Device (Device Descriptor Request Failed) which tells me it doesn't get real far here...&lt;/P&gt;&lt;P&gt;Any ideas?&amp;nbsp; Neither of these stock projects works out of the box....&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 20:01:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/USB-not-connecting-from-VCOM-CDC-example/m-p/1159514#M3950</guid>
      <dc:creator>randylee</dc:creator>
      <dc:date>2020-09-25T20:01:04Z</dc:date>
    </item>
    <item>
      <title>Re: USB not connecting from VCOM CDC example</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/USB-not-connecting-from-VCOM-CDC-example/m-p/1159516#M3951</link>
      <description>&lt;P&gt;Ah, found it! I had this plugged into a hub and that was causing problems apparently. Plugging it directly into my machine and it enumerates correctly!&lt;/P&gt;&lt;P&gt;Why that would be is a mystery that I'd like to know about at some point tho...&lt;/P&gt;</description>
      <pubDate>Fri, 25 Sep 2020 20:13:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/USB-not-connecting-from-VCOM-CDC-example/m-p/1159516#M3951</guid>
      <dc:creator>randylee</dc:creator>
      <dc:date>2020-09-25T20:13:00Z</dc:date>
    </item>
  </channel>
</rss>