<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: LPC-Link2 flasher</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1135177#M3930</link>
    <description>&lt;P&gt;I understand that these flash tools, e.g. "crt_emu_cm_redlink", are included in the MCUXpresso installation. Are they also available as a standalone download?&lt;/P&gt;&lt;P&gt;I just want to flash our custom board and not debug it. Therefore our "programming station" does not need a full installation of MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;Is there an installation package available that has a smaller footprint than the full MCUXpresso installation? I guess I can not just copy the "crt_emu_cm_redlink" and "boot_link2" executables as drivers would be missing.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
    <pubDate>Thu, 03 Sep 2020 10:56:08 GMT</pubDate>
    <dc:creator>danielholala</dc:creator>
    <dc:date>2020-09-03T10:56:08Z</dc:date>
    <item>
      <title>LPC-Link2 flasher</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1080423#M3712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I'm using&amp;nbsp;OM13054:LPC-Link2.&lt;/P&gt;&lt;P&gt;I need not to debug, but just to upload a file, which is in bin or hex format to mcu MK20dn512xxx.&amp;nbsp;&lt;/P&gt;&lt;P&gt;What PC flasher to use?&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 11:56:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1080423#M3712</guid>
      <dc:creator>peterkostadinov</dc:creator>
      <dc:date>2020-06-10T11:56:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link2 flasher</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1080424#M3713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are using MCUXPRESSO, then see&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389128"&gt;Using the GUI flash programming tool&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/389139"&gt;https://community.nxp.com/thread/389139&lt;/A&gt;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;for more details, see chapter 14 of the MCUXpresso user guide&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 12:33:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1080424#M3713</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2020-06-10T12:33:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link2 flasher</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1080425#M3714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;Con Verse,&lt;/P&gt;&lt;P&gt;Thank you very much!!!&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jun 2020 16:17:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1080425#M3714</guid>
      <dc:creator>peterkostadinov</dc:creator>
      <dc:date>2020-06-10T16:17:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link2 flasher</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1135177#M3930</link>
      <description>&lt;P&gt;I understand that these flash tools, e.g. "crt_emu_cm_redlink", are included in the MCUXpresso installation. Are they also available as a standalone download?&lt;/P&gt;&lt;P&gt;I just want to flash our custom board and not debug it. Therefore our "programming station" does not need a full installation of MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;Is there an installation package available that has a smaller footprint than the full MCUXpresso installation? I guess I can not just copy the "crt_emu_cm_redlink" and "boot_link2" executables as drivers would be missing.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2020 10:56:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1135177#M3930</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2020-09-03T10:56:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC-Link2 flasher</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1423263#M4523</link>
      <description>&lt;BLOCKQUOTE&gt;&lt;P&gt;I understand that these flash tools, e.g. "crt_emu_cm_redlink", are included in the MCUXpresso installation. Are they also available as a standalone download?&lt;/P&gt;&lt;P&gt;I just want to flash our custom board and not debug it. Therefore our "programming station" does not need a full installation of MCUXpresso IDE.&lt;/P&gt;&lt;P&gt;Is there an installation package available that has a smaller footprint than the full MCUXpresso installation? I guess I can not just copy the "crt_emu_cm_redlink" and "boot_link2" executables as drivers would be missing.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I'd like to raise this question again: Is "crt_emu_cm_redlink" available standalone? I've yet to find a standalone download. For now, I'm resorting to the full installation of MCUXpresso IDE.&lt;/P&gt;</description>
      <pubDate>Fri, 04 Mar 2022 11:21:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC-Link2-flasher/m-p/1423263#M4523</guid>
      <dc:creator>danielholala</dc:creator>
      <dc:date>2022-03-04T11:21:10Z</dc:date>
    </item>
  </channel>
</rss>