<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC2148 SD Card Driver in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/LPC2148-SD-Card-Driver/m-p/742081#M342</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sam,&lt;/P&gt;&lt;P&gt;When using legacy SD card drivers, it is common that they will have some issues when trying to communicate with newer SD cards, like SDHC.&lt;/P&gt;&lt;P&gt;In this case, you could try using the driver as is with Standard Capacity cards (2GB or less), or applying some modifications to the driver to be able to communicate with High Capacity cards (4 to 32 GB), as the mentioned on the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/8080718/sdhc-microsd-card-and-spi-initialization"&gt;https://stackoverflow.com/questions/8080718/sdhc-microsd-card-and-spi-initialization&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This is more common with SPI-based drivers rather than SD Host Controller drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Feb 2018 22:46:26 GMT</pubDate>
    <dc:creator>CarlosCasillas</dc:creator>
    <dc:date>2018-02-15T22:46:26Z</dc:date>
    <item>
      <title>LPC2148 SD Card Driver</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC2148-SD-Card-Driver/m-p/742080#M341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I am trying to get SD Card working on my LPC2148 Board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;I came across this link&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/application-note/AN10406.pdf" title="https://www.nxp.com/docs/en/application-note/AN10406.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN10406.pdf&lt;/A&gt;&amp;nbsp; (which is pretty old). I compiled it but I dont see any file creation or LED blinking&amp;nbsp; to indicate anything is hapenning.&amp;nbsp;&lt;/P&gt;&lt;P&gt;My SD Card is connected on the SPI1 interface.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an updated Driver ?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;Sam&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Feb 2018 05:32:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC2148-SD-Card-Driver/m-p/742080#M341</guid>
      <dc:creator>sambha</dc:creator>
      <dc:date>2018-02-14T05:32:42Z</dc:date>
    </item>
    <item>
      <title>Re: LPC2148 SD Card Driver</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPC2148-SD-Card-Driver/m-p/742081#M342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sam,&lt;/P&gt;&lt;P&gt;When using legacy SD card drivers, it is common that they will have some issues when trying to communicate with newer SD cards, like SDHC.&lt;/P&gt;&lt;P&gt;In this case, you could try using the driver as is with Standard Capacity cards (2GB or less), or applying some modifications to the driver to be able to communicate with High Capacity cards (4 to 32 GB), as the mentioned on the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://stackoverflow.com/questions/8080718/sdhc-microsd-card-and-spi-initialization"&gt;https://stackoverflow.com/questions/8080718/sdhc-microsd-card-and-spi-initialization&lt;/A&gt;&lt;/P&gt;&lt;P&gt;This is more common with SPI-based drivers rather than SD Host Controller drivers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this will be useful for you.&lt;/P&gt;&lt;P&gt;Best regards!&lt;/P&gt;&lt;P&gt;/Carlos&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Feb 2018 22:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPC2148-SD-Card-Driver/m-p/742081#M342</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2018-02-15T22:46:26Z</dc:date>
    </item>
  </channel>
</rss>