<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Generalのトピックprobably a BUG found in Serial Manager</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/probably-a-BUG-found-in-Serial-Manager/m-p/1048488#M3412</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using MUCXpresso IDE with SDK version of 2.8.0 of chip KV58F1M0VLL24. I'm using C++, and both my C &amp;amp; C++ compiler is set to arm-none-eabi-c++ with -std=c++17. When compiling "serial_manager.c", it reported an linking error of cannot find function "Serial_SwoWrite(...)". I found that it is because in file "serial_port_internal.h", the definitions are guarded with " extern "C"' ", but in file "serial_port_swo.c", they are not. The same happens to other files such as "serial_port_uart.c",etc. adding back the " extern "C" " solves the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 31 Jul 2020 04:54:53 GMT</pubDate>
    <dc:creator>ChekhovMark</dc:creator>
    <dc:date>2020-07-31T04:54:53Z</dc:date>
    <item>
      <title>probably a BUG found in Serial Manager</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/probably-a-BUG-found-in-Serial-Manager/m-p/1048488#M3412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using MUCXpresso IDE with SDK version of 2.8.0 of chip KV58F1M0VLL24. I'm using C++, and both my C &amp;amp; C++ compiler is set to arm-none-eabi-c++ with -std=c++17. When compiling "serial_manager.c", it reported an linking error of cannot find function "Serial_SwoWrite(...)". I found that it is because in file "serial_port_internal.h", the definitions are guarded with " extern "C"' ", but in file "serial_port_swo.c", they are not. The same happens to other files such as "serial_port_uart.c",etc. adding back the " extern "C" " solves the problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2020 04:54:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/probably-a-BUG-found-in-Serial-Manager/m-p/1048488#M3412</guid>
      <dc:creator>ChekhovMark</dc:creator>
      <dc:date>2020-07-31T04:54:53Z</dc:date>
    </item>
    <item>
      <title>Re: probably a BUG found in Serial Manager</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/probably-a-BUG-found-in-Serial-Manager/m-p/1048489#M3413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Chekhov,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot for your comments, I will report this issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 31 Jul 2020 21:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/probably-a-BUG-found-in-Serial-Manager/m-p/1048489#M3413</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2020-07-31T21:13:50Z</dc:date>
    </item>
  </channel>
</rss>