<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic  LPCX 4367 SPI problem in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/LPCX-4367-SPI-problem/m-p/1045603#M3377</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In LPCX 4367 board use the example code periph_ssp&lt;BR /&gt;1.I can use SPI1 to communicate with my device(In J1 pin PF4,P1_3,P1_4,P1_5) ,but if change to SPI0(in J3 pin SSEL,MOSI,MISO,SCK) can not get any data.&lt;BR /&gt;2.Are there any other document about LPCX 4367 pin definetion and example code?&lt;BR /&gt;3.This board can connect two spi device?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 May 2020 09:01:33 GMT</pubDate>
    <dc:creator>davechiu</dc:creator>
    <dc:date>2020-05-05T09:01:33Z</dc:date>
    <item>
      <title>LPCX 4367 SPI problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCX-4367-SPI-problem/m-p/1045603#M3377</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In LPCX 4367 board use the example code periph_ssp&lt;BR /&gt;1.I can use SPI1 to communicate with my device(In J1 pin PF4,P1_3,P1_4,P1_5) ,but if change to SPI0(in J3 pin SSEL,MOSI,MISO,SCK) can not get any data.&lt;BR /&gt;2.Are there any other document about LPCX 4367 pin definetion and example code?&lt;BR /&gt;3.This board can connect two spi device?&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2020 09:01:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCX-4367-SPI-problem/m-p/1045603#M3377</guid>
      <dc:creator>davechiu</dc:creator>
      <dc:date>2020-05-05T09:01:33Z</dc:date>
    </item>
    <item>
      <title>Re:  LPCX 4367 SPI problem</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/LPCX-4367-SPI-problem/m-p/1045604#M3378</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chiu Dave,&lt;/P&gt;&lt;P&gt;You can also refer LPC43S67 SPI demo from this site. it's same for LPC4367.&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/thread/470943#comment-1006933" title="https://community.nxp.com/thread/470943#comment-1006933"&gt;https://community.nxp.com/thread/470943#comment-1006933&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 May 2020 02:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/LPCX-4367-SPI-problem/m-p/1045604#M3378</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-05-07T02:59:47Z</dc:date>
    </item>
  </channel>
</rss>