<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: EEPROM Binary file generation in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/EEPROM-Binary-file-generation/m-p/1025337#M3167</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version of the reader library are you working with ? When you run the script, do you get some errors regarding some missing files? Could you please help me with the log you get when you run the script?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards ,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 Nov 2019 21:15:20 GMT</pubDate>
    <dc:creator>stephanie_m</dc:creator>
    <dc:date>2019-11-22T21:15:20Z</dc:date>
    <item>
      <title>EEPROM Binary file generation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/EEPROM-Binary-file-generation/m-p/1025336#M3166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on the PN7462AU kit for the card reader application.&lt;/P&gt;&lt;P&gt;I need to update the EEPROM binary file as mentioned in the EEPROM Management Application Note.&lt;/P&gt;&lt;P&gt;After following its instruction for installing python 2.7 and making the required changes in the "user_ee.xml" as per the user settings and then running "user_ee.bat" file. It was unable to create the new user_ee.bin with user defined settings into it. I have tried it many times it it was not updating.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Even I was looking for the Code Read Protection by adding the custom parameter as suggested in the EEPROM management file for the product and release versions, I have added (custom structure and filed for the code read protection levels-&lt;STRONG&gt;CRP&lt;/STRONG&gt;) that file too in the mentioned user.xml file it doesn't change or update any values into file, as we can check or get confirmed through "_output_xml_sizes".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, Please let me know the that how do I proceed for updating user_ee.bin file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looking forward the support and response.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks &amp;amp; Regards&lt;/P&gt;&lt;P&gt;SR&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 20:09:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/EEPROM-Binary-file-generation/m-p/1025336#M3166</guid>
      <dc:creator>sachin_singh</dc:creator>
      <dc:date>2019-11-21T20:09:41Z</dc:date>
    </item>
    <item>
      <title>Re: EEPROM Binary file generation</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/EEPROM-Binary-file-generation/m-p/1025337#M3167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which version of the reader library are you working with ? When you run the script, do you get some errors regarding some missing files? Could you please help me with the log you get when you run the script?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards ,&lt;/P&gt;&lt;P&gt;Estephania&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 Nov 2019 21:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/EEPROM-Binary-file-generation/m-p/1025337#M3167</guid>
      <dc:creator>stephanie_m</dc:creator>
      <dc:date>2019-11-22T21:15:20Z</dc:date>
    </item>
  </channel>
</rss>