<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックNXP flash is write-protected</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/NXP-flash-is-write-protected/m-p/1002003#M2921</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="微信截图_20200323183746.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103864iF04671B8DDE8CA52/image-size/large?v=v2&amp;amp;px=999" role="button" title="微信截图_20200323183746.png" alt="微信截图_20200323183746.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Device "MKW41Z512XXX4" selected.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Found SWD-DP with ID 0x0BC11477&lt;BR /&gt;Found SWD-DP with ID 0x0BC11477&lt;BR /&gt;AP-IDR: 0x04770031, Type: AHB-AP&lt;BR /&gt;AHB-AP ROM: 0xF0002000 (Base addr. of first ROM table)&lt;BR /&gt;Found Cortex-M0 r0p1, Little endian.&lt;BR /&gt;FPUnit: 2 code (BP) slots and 0 literal slots&lt;BR /&gt;CoreSight components:&lt;BR /&gt;ROMTbl 0 @ F0002000&lt;BR /&gt;ROMTbl 0 [0]: FFFFE000, CID: B105900D, PID: 001BB932 MTB-M0+&lt;BR /&gt;ROMTbl 0 [1]: FFFFF000, CID: B105900D, PID: 0008E000 MTBDWT&lt;BR /&gt;ROMTbl 0 [2]: F00FD000, CID: B105100D, PID: 000BB4C0 ROM Table&lt;BR /&gt;ROMTbl 1 @ E00FF000&lt;BR /&gt;ROMTbl 1 [0]: FFF0F000, CID: B105E00D, PID: 000BB008 SCS&lt;BR /&gt;ROMTbl 1 [1]: FFF02000, CID: B105E00D, PID: 000BB00A DWT&lt;BR /&gt;ROMTbl 1 [2]: FFF03000, CID: B105E00D, PID: 000BB00B FPB&lt;/P&gt;&lt;P&gt;****** Error: Kinetis (connect): Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set and mass erase is disabled. J-Link cannot unprotect the device.&lt;BR /&gt;Cortex-M0 identified.&lt;/P&gt;&lt;P&gt;Above is a screenshot and log of the problem I encountered.&lt;/P&gt;&lt;P&gt;In addition, I found relevant blog on the official website of NXP, but it seems to be of no use, it still shows flash write protection (1. I used unlock kinetis in jlink commander, 2. I also used mass erase, but I didn't find it in j-flash, only a erase chips was found).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Mar 2020 10:49:37 GMT</pubDate>
    <dc:creator>bs16935531041</dc:creator>
    <dc:date>2020-03-23T10:49:37Z</dc:date>
    <item>
      <title>NXP flash is write-protected</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/NXP-flash-is-write-protected/m-p/1002003#M2921</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="微信截图_20200323183746.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103864iF04671B8DDE8CA52/image-size/large?v=v2&amp;amp;px=999" role="button" title="微信截图_20200323183746.png" alt="微信截图_20200323183746.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Device "MKW41Z512XXX4" selected.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Found SWD-DP with ID 0x0BC11477&lt;BR /&gt;Found SWD-DP with ID 0x0BC11477&lt;BR /&gt;AP-IDR: 0x04770031, Type: AHB-AP&lt;BR /&gt;AHB-AP ROM: 0xF0002000 (Base addr. of first ROM table)&lt;BR /&gt;Found Cortex-M0 r0p1, Little endian.&lt;BR /&gt;FPUnit: 2 code (BP) slots and 0 literal slots&lt;BR /&gt;CoreSight components:&lt;BR /&gt;ROMTbl 0 @ F0002000&lt;BR /&gt;ROMTbl 0 [0]: FFFFE000, CID: B105900D, PID: 001BB932 MTB-M0+&lt;BR /&gt;ROMTbl 0 [1]: FFFFF000, CID: B105900D, PID: 0008E000 MTBDWT&lt;BR /&gt;ROMTbl 0 [2]: F00FD000, CID: B105100D, PID: 000BB4C0 ROM Table&lt;BR /&gt;ROMTbl 1 @ E00FF000&lt;BR /&gt;ROMTbl 1 [0]: FFF0F000, CID: B105E00D, PID: 000BB008 SCS&lt;BR /&gt;ROMTbl 1 [1]: FFF02000, CID: B105E00D, PID: 000BB00A DWT&lt;BR /&gt;ROMTbl 1 [2]: FFF03000, CID: B105E00D, PID: 000BB00B FPB&lt;/P&gt;&lt;P&gt;****** Error: Kinetis (connect): Protection bytes in flash at addr. 0x400 - 0x40F indicate that readout protection is set and mass erase is disabled. J-Link cannot unprotect the device.&lt;BR /&gt;Cortex-M0 identified.&lt;/P&gt;&lt;P&gt;Above is a screenshot and log of the problem I encountered.&lt;/P&gt;&lt;P&gt;In addition, I found relevant blog on the official website of NXP, but it seems to be of no use, it still shows flash write protection (1. I used unlock kinetis in jlink commander, 2. I also used mass erase, but I didn't find it in j-flash, only a erase chips was found).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 10:49:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/NXP-flash-is-write-protected/m-p/1002003#M2921</guid>
      <dc:creator>bs16935531041</dc:creator>
      <dc:date>2020-03-23T10:49:37Z</dc:date>
    </item>
    <item>
      <title>Re: NXP flash is write-protected</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/NXP-flash-is-write-protected/m-p/1002004#M2922</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="357046" data-username="bs16935531041@163.com" href="https://community.nxp.com/people/bs16935531041@163.com"&gt;shuai bai&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Unfortunately, there is no way to recover the mcu. If you are using a board you can replace the damaged mcu for a new one.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I apologize for the inconvenience this may cause you.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2020 18:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/NXP-flash-is-write-protected/m-p/1002004#M2922</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2020-03-25T18:58:53Z</dc:date>
    </item>
  </channel>
</rss>