<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 fatfs with ramdisk and dataflash</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/fatfs-with-ramdisk-and-dataflash/m-p/724404#M274</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm developing an application using a custom board based on MK66, MCUXpresso 10.1.1 and SDK 2.3.&lt;/P&gt;&lt;P&gt;On the board there is external battery backed up RAM,&amp;nbsp;used for a ramdisk, and a 8 MB dataflash device (AT45DB321E), where I need to implement 2 different disk.&lt;/P&gt;&lt;P&gt;I've read the FatFs docs and it seems that I can&amp;nbsp;handle only 1 disk of the same type (ramdisk, SD disk, MMC disk).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did I misunderstand something?&lt;/P&gt;&lt;P&gt;How can I handle my devices?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Mar 2018 10:39:38 GMT</pubDate>
    <dc:creator>biafra</dc:creator>
    <dc:date>2018-03-02T10:39:38Z</dc:date>
    <item>
      <title>fatfs with ramdisk and dataflash</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/fatfs-with-ramdisk-and-dataflash/m-p/724404#M274</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm developing an application using a custom board based on MK66, MCUXpresso 10.1.1 and SDK 2.3.&lt;/P&gt;&lt;P&gt;On the board there is external battery backed up RAM,&amp;nbsp;used for a ramdisk, and a 8 MB dataflash device (AT45DB321E), where I need to implement 2 different disk.&lt;/P&gt;&lt;P&gt;I've read the FatFs docs and it seems that I can&amp;nbsp;handle only 1 disk of the same type (ramdisk, SD disk, MMC disk).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did I misunderstand something?&lt;/P&gt;&lt;P&gt;How can I handle my devices?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks&lt;/P&gt;&lt;P&gt;Biafra&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Mar 2018 10:39:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/fatfs-with-ramdisk-and-dataflash/m-p/724404#M274</guid>
      <dc:creator>biafra</dc:creator>
      <dc:date>2018-03-02T10:39:38Z</dc:date>
    </item>
    <item>
      <title>Re: fatfs with ramdisk and dataflash</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/fatfs-with-ramdisk-and-dataflash/m-p/724405#M275</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Biafra:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In theory it is possible to write into several different physical discs, but I have never tried it in practice.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Mar 2018 03:09:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/fatfs-with-ramdisk-and-dataflash/m-p/724405#M275</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2018-03-20T03:09:09Z</dc:date>
    </item>
  </channel>
</rss>