<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Communicating between 2 NHS3100 in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Communicating-between-2-NHS3100/m-p/971762#M2674</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NHS3100 is a passive element. This means that the NFC qualities it has is essentially a tag.&amp;nbsp;Unfortunately you will not be able to communicate between two of these. You need an active element in order to properly communicate with the NHS3100.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you can provide the minimum requirements of your application, such as other peripherals, power, security, etc. I can point you in the right direction so you can compliment the NHS3100 correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or if you have any other questions regarding the NHS3100, do let me know as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Aug 2019 21:52:36 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2019-08-27T21:52:36Z</dc:date>
    <item>
      <title>Communicating between 2 NHS3100</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Communicating-between-2-NHS3100/m-p/971761#M2673</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I was wondering if I could use the NFC module to communicate between 2 NHS3100 chips. I would like to have my two devices communicate which each other when they are brought in close proximity.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Aug 2019 18:36:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Communicating-between-2-NHS3100/m-p/971761#M2673</guid>
      <dc:creator>michael_sprauve</dc:creator>
      <dc:date>2019-08-26T18:36:25Z</dc:date>
    </item>
    <item>
      <title>Re: Communicating between 2 NHS3100</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Communicating-between-2-NHS3100/m-p/971762#M2674</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NHS3100 is a passive element. This means that the NFC qualities it has is essentially a tag.&amp;nbsp;Unfortunately you will not be able to communicate between two of these. You need an active element in order to properly communicate with the NHS3100.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you can provide the minimum requirements of your application, such as other peripherals, power, security, etc. I can point you in the right direction so you can compliment the NHS3100 correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Or if you have any other questions regarding the NHS3100, do let me know as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Aug 2019 21:52:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Communicating-between-2-NHS3100/m-p/971762#M2674</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-08-27T21:52:36Z</dc:date>
    </item>
  </channel>
</rss>