<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso Generalのトピックthe variable define by FLEXIO_UART_Type unwork</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/the-variable-define-by-FLEXIO-UART-Type-unwork/m-p/960360#M2557</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i build a new project to test flexio function,and i copy the code from the example project (flexio_uart_interrupt_transfer). but when i start debug,i find that the variable define by&amp;nbsp;FLEXIO_UART_Type is null, the function cant get in when it use the pointer of the variable.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 24 Jul 2019 05:25:59 GMT</pubDate>
    <dc:creator>wuyunfeng</dc:creator>
    <dc:date>2019-07-24T05:25:59Z</dc:date>
    <item>
      <title>the variable define by FLEXIO_UART_Type unwork</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/the-variable-define-by-FLEXIO-UART-Type-unwork/m-p/960360#M2557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i build a new project to test flexio function,and i copy the code from the example project (flexio_uart_interrupt_transfer). but when i start debug,i find that the variable define by&amp;nbsp;FLEXIO_UART_Type is null, the function cant get in when it use the pointer of the variable.&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jul 2019 05:25:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/the-variable-define-by-FLEXIO-UART-Type-unwork/m-p/960360#M2557</guid>
      <dc:creator>wuyunfeng</dc:creator>
      <dc:date>2019-07-24T05:25:59Z</dc:date>
    </item>
    <item>
      <title>Re: the variable define by FLEXIO_UART_Type unwork</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/the-variable-define-by-FLEXIO-UART-Type-unwork/m-p/960361#M2558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Can you give more detail about your problem? Are you using KL28?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Jing&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Jul 2019 03:26:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/the-variable-define-by-FLEXIO-UART-Type-unwork/m-p/960361#M2558</guid>
      <dc:creator>jingpan</dc:creator>
      <dc:date>2019-07-26T03:26:44Z</dc:date>
    </item>
  </channel>
</rss>