<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso General中的主题 MCUxpresso debugger failing to connect to RT 1062 (MIMXRT1060-EVK) - Probe Index 1</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/MCUxpresso-debugger-failing-to-connect-to-RT-1062-MIMXRT1060-EVK/m-p/953704#M2486</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Error: Unable to configure core for probe index 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested this with a number of sample / experimental projects and they all exhibit the same issues. I need a reliable / repeatable method to recover from this. I am using the MIMXRT1060-EVK with External PSU 5V and the USB cable connected from PC to J41. I am running version DAP 0244.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Daplink Mode: Interface&lt;BR /&gt;Interface Version: 0246&lt;BR /&gt;Bootloader Version: 0244&lt;BR /&gt;Git SHA: 51140ef2aa7be53bca9e15ca7ef7acef05ff6527&lt;BR /&gt;Local Mods: 1&lt;BR /&gt;USB Interfaces: MSD, CDC, HID, WebUSB&lt;BR /&gt;Bootloader CRC: 0xe493996b&lt;BR /&gt;Interface CRC: 0xf7f2f5dd&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I have followed:&amp;nbsp;&lt;A class="link-titled" href="https://freescale.jiveon.com/thread/505973" title="https://freescale.jiveon.com/thread/505973"&gt;MCUxpresso debugger failing to connect to RT 10... | NXP Community&lt;/A&gt;&amp;nbsp;as closely as possible.&lt;/P&gt;&lt;P&gt;Trying to debug through DAP I get:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Error in final launch sequence&lt;/P&gt;&lt;P&gt;Error: Unable to configure core for probe index 1.&lt;BR /&gt;Wire not connected&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Setting SW7 to 0000 and using GUI flash tool mass erase, gave:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;BR /&gt;(100) Target Connection Failed&lt;BR /&gt;Unable to perform operation!&lt;BR /&gt;Command failed with exit code 1&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Tried using J-Link. Removed J47 and J48&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Error in final launch sequence&lt;BR /&gt;Failed to execute MI command:&lt;BR /&gt;-target-select remote localhost:2331&lt;/P&gt;&lt;P&gt;Error message from debugger back end:&lt;BR /&gt;localhost:2331: No connection could be made because the target machine actively refused it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could not connect to target.&lt;BR /&gt; SEGGER J-Link GDB Server V6.44a Command Line Version&lt;BR /&gt; JLinkARM.dll V6.44a (DLL compiled Mar 8 2019 17:31:48)&lt;BR /&gt; Command line: -nosilent -swoport 2332 -select USB=59304533 -telnetport 2333 -singlerun -endian little -noir -speed auto -port 2331 -vd -device MIMXRT1062xxx6A -if SWD -halt -reportuseraction&lt;BR /&gt; -----GDB Server start settings-----&lt;BR /&gt; GDBInit file: none&lt;BR /&gt; GDB Server Listening port: 2331&lt;BR /&gt; SWO raw output listening port: 2332&lt;BR /&gt; Terminal I/O port: 2333&lt;BR /&gt; Accept remote connection: localhost only&lt;BR /&gt; Generate logfile: off&lt;BR /&gt; Verify download: on&lt;BR /&gt; Init regs on start: off&lt;BR /&gt; Silent mode: off&lt;BR /&gt; Single run mode: on&lt;BR /&gt; Target connection timeout: 0 ms&lt;BR /&gt; ------J-Link related settings------&lt;BR /&gt; J-Link Host interface: USB&lt;BR /&gt; J-Link script: none&lt;BR /&gt; J-Link settings file: none&lt;BR /&gt; ------Target related settings------&lt;BR /&gt; Target device: MIMXRT1062xxx6A&lt;BR /&gt; Target interface: SWD&lt;BR /&gt; Target interface speed: auto&lt;BR /&gt; Target endian: little&lt;BR /&gt; Connecting to J-Link...&lt;BR /&gt; J-Link is connected.&lt;BR /&gt; Device "MIMXRT1062XXX6A" selected.&lt;BR /&gt; Firmware: J-Link V9 compiled Oct 25 2018 11:46:07&lt;BR /&gt; Hardware: V9.30&lt;BR /&gt;Feature(s): GDB&lt;BR /&gt; Checking target voltage...&lt;BR /&gt; Connecting to target failed. Connected correctly?&lt;BR /&gt; GDB Server will be closed...&lt;BR /&gt; Shutting down...&lt;BR /&gt; Could not connect to target.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Also tried going into different flash modes: SW7-0001 serial download; SW7-0000 and SW7-0010 internal flash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Oct 2019 22:03:47 GMT</pubDate>
    <dc:creator>graham_taylor-j</dc:creator>
    <dc:date>2019-10-07T22:03:47Z</dc:date>
    <item>
      <title>MCUxpresso debugger failing to connect to RT 1062 (MIMXRT1060-EVK) - Probe Index 1</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUxpresso-debugger-failing-to-connect-to-RT-1062-MIMXRT1060-EVK/m-p/953704#M2486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN&gt;Error: Unable to configure core for probe index 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tested this with a number of sample / experimental projects and they all exhibit the same issues. I need a reliable / repeatable method to recover from this. I am using the MIMXRT1060-EVK with External PSU 5V and the USB cable connected from PC to J41. I am running version DAP 0244.&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Daplink Mode: Interface&lt;BR /&gt;Interface Version: 0246&lt;BR /&gt;Bootloader Version: 0244&lt;BR /&gt;Git SHA: 51140ef2aa7be53bca9e15ca7ef7acef05ff6527&lt;BR /&gt;Local Mods: 1&lt;BR /&gt;USB Interfaces: MSD, CDC, HID, WebUSB&lt;BR /&gt;Bootloader CRC: 0xe493996b&lt;BR /&gt;Interface CRC: 0xf7f2f5dd&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;I have followed:&amp;nbsp;&lt;A class="link-titled" href="https://freescale.jiveon.com/thread/505973" title="https://freescale.jiveon.com/thread/505973"&gt;MCUxpresso debugger failing to connect to RT 10... | NXP Community&lt;/A&gt;&amp;nbsp;as closely as possible.&lt;/P&gt;&lt;P&gt;Trying to debug through DAP I get:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Error in final launch sequence&lt;/P&gt;&lt;P&gt;Error: Unable to configure core for probe index 1.&lt;BR /&gt;Wire not connected&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Setting SW7 to 0000 and using GUI flash tool mass erase, gave:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Connecting to probe 1 core 0 (using server started externally) gave 'Ee(42). Could not connect to core.'&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port&lt;BR /&gt;(100) Target Connection Failed&lt;BR /&gt;Unable to perform operation!&lt;BR /&gt;Command failed with exit code 1&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Tried using J-Link. Removed J47 and J48&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Error in final launch sequence&lt;BR /&gt;Failed to execute MI command:&lt;BR /&gt;-target-select remote localhost:2331&lt;/P&gt;&lt;P&gt;Error message from debugger back end:&lt;BR /&gt;localhost:2331: No connection could be made because the target machine actively refused it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could not connect to target.&lt;BR /&gt; SEGGER J-Link GDB Server V6.44a Command Line Version&lt;BR /&gt; JLinkARM.dll V6.44a (DLL compiled Mar 8 2019 17:31:48)&lt;BR /&gt; Command line: -nosilent -swoport 2332 -select USB=59304533 -telnetport 2333 -singlerun -endian little -noir -speed auto -port 2331 -vd -device MIMXRT1062xxx6A -if SWD -halt -reportuseraction&lt;BR /&gt; -----GDB Server start settings-----&lt;BR /&gt; GDBInit file: none&lt;BR /&gt; GDB Server Listening port: 2331&lt;BR /&gt; SWO raw output listening port: 2332&lt;BR /&gt; Terminal I/O port: 2333&lt;BR /&gt; Accept remote connection: localhost only&lt;BR /&gt; Generate logfile: off&lt;BR /&gt; Verify download: on&lt;BR /&gt; Init regs on start: off&lt;BR /&gt; Silent mode: off&lt;BR /&gt; Single run mode: on&lt;BR /&gt; Target connection timeout: 0 ms&lt;BR /&gt; ------J-Link related settings------&lt;BR /&gt; J-Link Host interface: USB&lt;BR /&gt; J-Link script: none&lt;BR /&gt; J-Link settings file: none&lt;BR /&gt; ------Target related settings------&lt;BR /&gt; Target device: MIMXRT1062xxx6A&lt;BR /&gt; Target interface: SWD&lt;BR /&gt; Target interface speed: auto&lt;BR /&gt; Target endian: little&lt;BR /&gt; Connecting to J-Link...&lt;BR /&gt; J-Link is connected.&lt;BR /&gt; Device "MIMXRT1062XXX6A" selected.&lt;BR /&gt; Firmware: J-Link V9 compiled Oct 25 2018 11:46:07&lt;BR /&gt; Hardware: V9.30&lt;BR /&gt;Feature(s): GDB&lt;BR /&gt; Checking target voltage...&lt;BR /&gt; Connecting to target failed. Connected correctly?&lt;BR /&gt; GDB Server will be closed...&lt;BR /&gt; Shutting down...&lt;BR /&gt; Could not connect to target.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;Also tried going into different flash modes: SW7-0001 serial download; SW7-0000 and SW7-0010 internal flash&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 22:03:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUxpresso-debugger-failing-to-connect-to-RT-1062-MIMXRT1060-EVK/m-p/953704#M2486</guid>
      <dc:creator>graham_taylor-j</dc:creator>
      <dc:date>2019-10-07T22:03:47Z</dc:date>
    </item>
    <item>
      <title>Re: MCUxpresso debugger failing to connect to RT 1062 (MIMXRT1060-EVK) - Probe Index 1</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUxpresso-debugger-failing-to-connect-to-RT-1062-MIMXRT1060-EVK/m-p/953705#M2487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The message&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;Checking target voltage...&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;Connecting to target failed. Connected correctly?&lt;/P&gt;&lt;P&gt;indicates that there might be a problem with the power supply. The J-Link senses the target voltage using pin 1 (VTRef):&lt;/P&gt;&lt;P&gt;&lt;IMG alt="Image result for jtag pinout segger" class="" height="420" src="https://www.segger.com/fileadmin/images/products/J-Link/Interface_Description/181129_JTAG.svg" width="330" /&gt;&lt;/P&gt;&lt;P&gt;Can you check that this pin really has 3V?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for the external power supply: that supply needs to be *very* stable and able to provide the needed current. I had problem with a bad/cheap one. Using a very good lab/desk power supply solved that problem for me. Additionally I had to have the power supply grounded.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 05:36:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUxpresso-debugger-failing-to-connect-to-RT-1062-MIMXRT1060-EVK/m-p/953705#M2487</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2019-10-08T05:36:39Z</dc:date>
    </item>
    <item>
      <title>Re: MCUxpresso debugger failing to connect to RT 1062 (MIMXRT1060-EVK) - Probe Index 1</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/MCUxpresso-debugger-failing-to-connect-to-RT-1062-MIMXRT1060-EVK/m-p/953706#M2488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;SOLVED: Touch Controller on attached LCD was dragging supply. Remove / replace LCD.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="display: inline !important; float: none; background-color: #ffffff; color: #3d3d3d; font-family: Helvetica Neue,Helvetica,Arial,Lucida Grande,sans-serif; font-size: 15px; font-style: normal; font-variant: normal; font-weight: 400; letter-spacing: normal; orphans: 2; overflow-wrap: break-word; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;Thanks&lt;/SPAN&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/ErichS"&gt;ErichS&lt;/A&gt;&lt;SPAN style="display: inline !important; float: none; background-color: #ffffff; color: #3d3d3d; font-family: Helvetica Neue,Helvetica,Arial,Lucida Grande,sans-serif; font-size: 15px; font-style: normal; font-variant: normal; font-weight: 400; letter-spacing: normal; orphans: 2; overflow-wrap: break-word; text-align: left; text-decoration: none; text-indent: 0px; text-transform: none; -webkit-text-stroke-width: 0px; white-space: normal; word-spacing: 0px;"&gt;‌&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Checked the 3.3v reference to JTAG. This was overloaded resulting in 0.8v to pin even when J-Link removed. Also listen closely for switched mode regulators working too hard. Buzzing / whining sound.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 15:49:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/MCUxpresso-debugger-failing-to-connect-to-RT-1062-MIMXRT1060-EVK/m-p/953706#M2488</guid>
      <dc:creator>graham_taylor-j</dc:creator>
      <dc:date>2019-10-08T15:49:08Z</dc:date>
    </item>
  </channel>
</rss>