<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB CCID Class - Interface configuring  in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/USB-CCID-Class-Interface-configuring/m-p/942548#M2319</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PNEV7462C card reader and need to add two interface in CCID class(which can be seen under device manager with SMART_CARD_READERs CLASS with Two interface).&lt;/P&gt;&lt;P&gt;In "phExCcid" example, it shows only single "interface" in SMART_CARD_READERs class. And I need to add one more interface into it.&lt;/P&gt;&lt;P&gt;So, How can I made changes into the Use usb descriptor files to add one more "interface in same SMART_CARD_READERs class.&lt;/P&gt;&lt;P&gt;Looking forward for the response for adding one more "interface" in SMART_CARD_READERs CCID USB Class.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your all the support and response are highly appreciative.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 19 Oct 2019 09:52:09 GMT</pubDate>
    <dc:creator>sachin_singh</dc:creator>
    <dc:date>2019-10-19T09:52:09Z</dc:date>
    <item>
      <title>USB CCID Class - Interface configuring</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/USB-CCID-Class-Interface-configuring/m-p/942548#M2319</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using PNEV7462C card reader and need to add two interface in CCID class(which can be seen under device manager with SMART_CARD_READERs CLASS with Two interface).&lt;/P&gt;&lt;P&gt;In "phExCcid" example, it shows only single "interface" in SMART_CARD_READERs class. And I need to add one more interface into it.&lt;/P&gt;&lt;P&gt;So, How can I made changes into the Use usb descriptor files to add one more "interface in same SMART_CARD_READERs class.&lt;/P&gt;&lt;P&gt;Looking forward for the response for adding one more "interface" in SMART_CARD_READERs CCID USB Class.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Your all the support and response are highly appreciative.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 19 Oct 2019 09:52:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/USB-CCID-Class-Interface-configuring/m-p/942548#M2319</guid>
      <dc:creator>sachin_singh</dc:creator>
      <dc:date>2019-10-19T09:52:09Z</dc:date>
    </item>
  </channel>
</rss>