<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Debugging unmanaed project in MCUXpresso General</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940626#M2301</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;if you want to create unmanaged/make file projects, you have to do it manually.&lt;/P&gt;&lt;P&gt;See &lt;A class="link-titled" href="https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/" title="https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/"&gt;Tutorial: Makefile Projects with Eclipse | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for the debugging parts: the 'blue' debug button creates the launch config setting based on the SDK/MCU used/assigned to the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 03 Oct 2019 17:48:42 GMT</pubDate>
    <dc:creator>ErichStyger</dc:creator>
    <dc:date>2019-10-03T17:48:42Z</dc:date>
    <item>
      <title>Debugging unmanaed project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940621#M2296</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I just got the LPC55s69 board and I was able to run the SDK projects on the current MCUexpresso IDE. Now, moving further, I tried to create a project and launch config for an unmanaged project (elf image built out side using the gcc tool chain included in the IDE). By launching it, I get errors, it Appears that the IDE does not recognize the elf images built outside. How to deal with this? Please point me literature for this.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Oct 2019 18:53:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940621#M2296</guid>
      <dc:creator>michaelanburaj</dc:creator>
      <dc:date>2019-10-02T18:53:30Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging unmanaed project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940622#M2297</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Could you post your image or at least the error messages?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 03:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940622#M2297</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2019-10-03T03:52:20Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging unmanaed project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940623#M2298</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is nothing special about an image built 'inside' or 'outside' of the IDE - provided they are using the same compiler/linker etc and have created a valid image, then it should work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Probably best if you report the exact error messages you see, and describe how you built your image (perhaps provide the .map files?)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 07:54:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940623#M2298</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2019-10-03T07:54:29Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging unmanaed project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940624#M2299</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Con Verse, Erich,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you both for responding quickly. Actually, after posting this, by comparing and matching settings from a sample project from SDK, I was able to run my elf image successfully. The problem was not with the image created outside, but rather the project &amp;amp; Linkserver.launch settings. I am able to manually copy the project settings.MCU settings on the&amp;nbsp; and also after the probe detection stage on the LinkServer.launch I manually match some of the settings.&lt;/P&gt;&lt;P&gt;Although this works, it is a bit ugly. I assume there should be a better or more cleaner approach to this. Like for instance if there is an option to attach the SDK.LPC55S69 (in my case) to the empty project "Makefile project" then I assume the settings into both project setting.MCU, LinkServer.launch-&amp;gt;Startup commands and all other relevant settings would then get automatically inherited from the SDK like it happens for the SDK_demo projects. I tried finding this path (customized eclipse has many ways, that it can get a bit confusing at times).&lt;/P&gt;&lt;P&gt;FYI:&lt;/P&gt;&lt;P&gt;1. I have the SDK already installed into MCUexpresso and when I import the SDK.example project, the settings on both project settings and Linkserver.Launch-&amp;gt;Startup seem to be populated with what is required automatically. Either these settings come from the attached SDK or is carried within these projects. Either case, if I can do a step that will allow inheriting all the correct settings automatically by pointing to the SDK for the Makefile project (which I have not figured yet) or my inheriting the settings from a SDK.demo project, that will be lot cleaner than me manually copying them over.&lt;/P&gt;&lt;P&gt;2. Even after manually choosing the right SDK, MCU under project setting.MCU (different compared to Attaching SDK with the board picture when importing SDK.demo project), the LinkServer.launch-&amp;gt;Startup commands come out differently, then I have to manually edit them (copy-paste) these commands from SDK.demo project for it to connect and run the image without errors.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Michael.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 16:26:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940624#M2299</guid>
      <dc:creator>michaelanburaj</dc:creator>
      <dc:date>2019-10-03T16:26:41Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging unmanaed project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940625#M2300</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Additional info: There is also the "New projects" option under the quickstart panel. This seems to do all that I want, but, then unfortunately it does not support a project option for Makefile project (or) unmaganged.&lt;/P&gt;&lt;P&gt;FYI: I am not stuck, as I have the workaround to manually copy/match stuff over to "Makefile project"&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;-Michael.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 16:45:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940625#M2300</guid>
      <dc:creator>michaelanburaj</dc:creator>
      <dc:date>2019-10-03T16:45:48Z</dc:date>
    </item>
    <item>
      <title>Re: Debugging unmanaed project</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940626#M2301</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michael,&lt;/P&gt;&lt;P&gt;if you want to create unmanaged/make file projects, you have to do it manually.&lt;/P&gt;&lt;P&gt;See &lt;A class="link-titled" href="https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/" title="https://mcuoneclipse.com/2017/07/22/tutorial-makefile-projects-with-eclipse/"&gt;Tutorial: Makefile Projects with Eclipse | MCU on Eclipse&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;As for the debugging parts: the 'blue' debug button creates the launch config setting based on the SDK/MCU used/assigned to the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this this helps,&lt;/P&gt;&lt;P&gt;Erich&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Oct 2019 17:48:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Debugging-unmanaed-project/m-p/940626#M2301</guid>
      <dc:creator>ErichStyger</dc:creator>
      <dc:date>2019-10-03T17:48:42Z</dc:date>
    </item>
  </channel>
</rss>