<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCUXpresso GeneralのトピックRe: Faster compile/flash than the GUI Flash Tool</title>
    <link>https://community.nxp.com/t5/MCUXpresso-General/Faster-compile-flash-than-the-GUI-Flash-Tool/m-p/937237#M2247</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition to the fully feature functionality of the GUI Flash Tool (which will always trigger a probe discovery), you can also use the "Program Flash action ..." option on the Debug shortcuts in the Quickstart Panel, as described in section 12.3.1, "Debug Quickstart Shortcuts".&amp;nbsp;For further&amp;nbsp;details also see&amp;nbsp;12.3.6, "Project Flash Programming" in the MCUXpresso IDE v11.0 User Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively, you can just launch a debug session - which will generally trigger and build then launch a debug session (including automatically programming flash as the debug session starts).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Sep 2019 21:07:09 GMT</pubDate>
    <dc:creator>lpcxpresso_supp</dc:creator>
    <dc:date>2019-09-02T21:07:09Z</dc:date>
    <item>
      <title>Faster compile/flash than the GUI Flash Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Faster-compile-flash-than-the-GUI-Flash-Tool/m-p/937236#M2246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I'm using the i.MX1060 EVK board and MCUExpresso.&lt;/P&gt;&lt;P&gt;I'm working on a hardware design that can't be simulated well on desktop, so I have to do a lot of compile/flash cycles to test on the evaluation board directly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So currently, after making any change, I have to:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;click&amp;nbsp;build on the toolbar&lt;/LI&gt;&lt;LI&gt;click the project name in my workspace so it is in focus (the GUI flash tool icon will not be active otherwise)&lt;/LI&gt;&lt;LI&gt;click&amp;nbsp;the GUI Flash Tool button on the toolbar and wait for probe discovery to happen&lt;/LI&gt;&lt;LI&gt;Click&amp;nbsp;OK on probe discovery&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Click Run on GUI Flash Tool dialog and wait for programming to happen&lt;/LI&gt;&lt;LI&gt;Click ok on "Operation Completed!"&amp;nbsp;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There has to be a faster way! Can you help me understand how to flash in one button or keyboard shortcut?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 13:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Faster-compile-flash-than-the-GUI-Flash-Tool/m-p/937236#M2246</guid>
      <dc:creator>brian2</dc:creator>
      <dc:date>2019-09-02T13:03:14Z</dc:date>
    </item>
    <item>
      <title>Re: Faster compile/flash than the GUI Flash Tool</title>
      <link>https://community.nxp.com/t5/MCUXpresso-General/Faster-compile-flash-than-the-GUI-Flash-Tool/m-p/937237#M2247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In addition to the fully feature functionality of the GUI Flash Tool (which will always trigger a probe discovery), you can also use the "Program Flash action ..." option on the Debug shortcuts in the Quickstart Panel, as described in section 12.3.1, "Debug Quickstart Shortcuts".&amp;nbsp;For further&amp;nbsp;details also see&amp;nbsp;12.3.6, "Project Flash Programming" in the MCUXpresso IDE v11.0 User Guide.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Alternatively, you can just launch a debug session - which will generally trigger and build then launch a debug session (including automatically programming flash as the debug session starts).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 21:07:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCUXpresso-General/Faster-compile-flash-than-the-GUI-Flash-Tool/m-p/937237#M2247</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2019-09-02T21:07:09Z</dc:date>
    </item>
  </channel>
</rss>